StrainGagePlacementType Enumeration

class NXOpen.CAE.ResponseSimulation.StrainGagePlacementType

Bases: object

Specifies the placement type of Strain Gage Enum Members

Enum Member Enum Member Description
Node
ElementFaceCenter
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.