StrainGageOrientationPlane Enumeration

class NXOpen.CAE.ResponseSimulation.StrainGageOrientationPlane

Bases: object

Specifies the orientation plane type of Strain Gage Enum Members

Enum Member Enum Member Description
FacePlane
Csys
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.