CombinationEvaluationOptions Class¶
-
class
NXOpen.CAE.ResponseSimulation.
CombinationEvaluationOptions
¶ Bases:
NXOpen.TaggedObject
Represents the setting for combination evaluation.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CombinationMethod | Returns or sets the combination method for multiple excitation combination |
EvaluationMethodOption | Returns or sets the calculation method |
NeighboringFactor | Returns or sets the neighboring factor. |
Tag | Returns the Tag for this object. |
TimeDuration | Returns or sets the time duration in second. |
Methods¶
Enumerations¶
CombinationEvaluationOptionsEvaluationMethod Enumeration | Specifies the calculation method of combination evaluation |
CombinationEvaluationOptionsMultipleExcitationCombinationMethod Enumeration | Specifies combination method for multiple excitation combination |
Property Detail¶
CombinationMethod¶
-
CombinationEvaluationOptions.
CombinationMethod
¶ Returns or sets the combination method for multiple excitation combination
-------------------------------------
Getter Method
Signature
CombinationMethod
Returns: Return type: NXOpen.CAE.ResponseSimulation.CombinationEvaluationOptionsMultipleExcitationCombinationMethod
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
CombinationMethod
Parameters: combinationMethod ( NXOpen.CAE.ResponseSimulation.CombinationEvaluationOptionsMultipleExcitationCombinationMethod
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
EvaluationMethodOption¶
-
CombinationEvaluationOptions.
EvaluationMethodOption
¶ Returns or sets the calculation method
-------------------------------------
Getter Method
Signature
EvaluationMethodOption
Returns: Return type: NXOpen.CAE.ResponseSimulation.CombinationEvaluationOptionsEvaluationMethod
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
EvaluationMethodOption
Parameters: method ( NXOpen.CAE.ResponseSimulation.CombinationEvaluationOptionsEvaluationMethod
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
NeighboringFactor¶
-
CombinationEvaluationOptions.
NeighboringFactor
¶ Returns or sets the neighboring factor.
Must be specified when calculation method is :py:class:` CAE.ResponseSimulation.CombinationEvaluationOptionsEvaluationMethod.Nrl < CAE.ResponseSimulation.CombinationEvaluationOptionsEvaluationMethod>`
-------------------------------------
Getter Method
Signature
NeighboringFactor
Returns: Return type: float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
NeighboringFactor
Parameters: neighboringFactor (float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
TimeDuration¶
-
CombinationEvaluationOptions.
TimeDuration
¶ Returns or sets the time duration in second.
Must be specified when calculation method is
CAE.ResponseSimulation.CombinationEvaluationOptionsEvaluationMethod.NqcDoubleSum
-------------------------------------
Getter Method
Signature
TimeDuration
Returns: Return type: float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
TimeDuration
Parameters: timeDuration (float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)