CombinationEvaluationOptionsEvaluationMethod Enumeration

NXOpen.CAE.ResponseSimulation.CombinationEvaluationOptions.EvaluationMethod is an alias for NXOpen.CAE.ResponseSimulation.CombinationEvaluationOptionsEvaluationMethod

class NXOpen.CAE.ResponseSimulation.CombinationEvaluationOptionsEvaluationMethod

Bases: object

Specifies the calculation method of combination evaluation

Enum Members

Enum Member Enum Member Description
Abs
Srss
Nrl
Cqc
NqcDoubleSum
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.