CombinationEvaluationOptionsMultipleExcitationCombinationMethod Enumeration

NXOpen.CAE.ResponseSimulation.CombinationEvaluationOptions.MultipleExcitationCombinationMethod is an alias for NXOpen.CAE.ResponseSimulation.CombinationEvaluationOptionsMultipleExcitationCombinationMethod

class NXOpen.CAE.ResponseSimulation.CombinationEvaluationOptionsMultipleExcitationCombinationMethod

Bases: object

Specifies combination method for multiple excitation combination

Enum Members

Enum Member Enum Member Description
Abs
Srs
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.