ModelUpdateSolutionCollection Class¶
-
class
NXOpen.CAE.
ModelUpdateSolutionCollection
¶ Bases:
object
Represents a collection of model update meta solution
To obtain an instance of this class, refer to
NXOpen.CAE.CorrelManager
Properties¶
Property | Description |
---|---|
ActiveSolution | Returns or sets the active solution |
Methods¶
Method | Description |
---|---|
CreateSensitivityViewerBuilder | Creates the builder object of model update sensitivity viewer |
CreateSolutionBuilder | Creates the builder object of model update meta solution |
FindObject | Finds a model update meta solution with specified solution name |
Property Detail¶
ActiveSolution¶
-
ModelUpdateSolutionCollection.
ActiveSolution
¶ Returns or sets the active solution
-------------------------------------
Getter Method
Signature
ActiveSolution
Returns: Return type: NXOpen.CAE.ModelUpdateSolution
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActiveSolution
Parameters: activeSolution ( NXOpen.CAE.ModelUpdateSolution
) –New in version NX7.5.0.
License requirements: None.
Method Detail¶
CreateSensitivityViewerBuilder¶
-
ModelUpdateSolutionCollection.
CreateSensitivityViewerBuilder
¶ Creates the builder object of model update sensitivity viewer
Signature
CreateSensitivityViewerBuilder(solution)
Parameters: solution ( NXOpen.CAE.ModelUpdateSolution
) – Model Update setupReturns: Return type: NXOpen.CAE.ModelUpdateSensitivityViewerBuilder
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
CreateSolutionBuilder¶
-
ModelUpdateSolutionCollection.
CreateSolutionBuilder
¶ Creates the builder object of model update meta solution
Signature
CreateSolutionBuilder(solution)
Parameters: solution ( NXOpen.CAE.ModelUpdateSolution
) – Model update solution being editReturns: Return type: NXOpen.CAE.ModelUpdateSolutionBuilder
New in version NX7.5.0.
License requirements: None.
FindObject¶
-
ModelUpdateSolutionCollection.
FindObject
¶ Finds a model update meta solution with specified solution name
Signature
FindObject(solutionName)
Parameters: solutionName (str) – Solution to be found Returns: Model Update meta solution found Return type: NXOpen.CAE.ModelUpdateSolution
New in version NX7.5.0.
License requirements: None.