ModelUpdateSolution Class¶
-
class
NXOpen.CAE.
ModelUpdateSolution
¶ Bases:
NXOpen.CAE.CorrelSolution
Represents a
NXOpen.CAE.ModelUpdateSolution
, which is a meta-solution used to update finite element models to match real life test dataTo create or edit an instance of this class, use
NXOpen.CAE.ModelUpdateSolutionBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
DesignVariables | The design variables collection for this meta solution. |
Methods¶
Method | Description |
---|---|
CalculateComacs | Computes the CoMAC correlation metric for active modes |
CalculateErrors | Calculates errors |
CloneCorrelation | Make a clone of a correl solution. |
CloneModelupdate | Make a clone of a model update solution. |
ComputeMacs | Computes the Model Assurance Criterion (MAC) correlation metric for active modes |
ComputeModePairsForSol | Compute mode pairs for correlation solution |
CreateAttributeIterator | Create an attribute iterator |
CreateCorrelMethodBuilder | Creates the builder object of model update correlation method |
CreateModePairingBuilder | Creates the builder object for mode pairing editing |
CreateOptimOptionsBuilder | Creates the builder object of model update optimize options |
CreateOptionsBuilder | Creates the builder object of model update options |
CreateOverallWeightsBuilder | Creates the builder object of model update overall weights |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
Destroy | Deletes a correlation solution |
ExportDesignVariablesCsvFile | Export the model update design variables to the csv file |
ExportErrorsCsvFile | Export the model update errors to the csv file |
ExportModePairCsvFile | Export mode pair to CSV file |
ExportNodeMapCsvFile | Export node map to CSV file |
ExportSensitivitiesCsvFile | Export the model update sensitivities to the csv file |
ExportShapeMetricsCsvFile | Export shape metrics to CSV file |
ExportTargetsCsvFile | Export the model update targets to the csv file |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GenerateComacResults | Create COMAC results |
GenerateMatchingDofset | Create Matching DOFSet |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDesignVarNumber | Gets the number of design variables |
GetDesignVariables | Returns the design variables in the model update solution |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSolutionName | Returns the correlation solution name |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
ImportNodeMapCsvFile | Import node map CSV file |
LockNodeMap | Lock the node map. |
Prints a representation of this object to the system log file. | |
ResetDesignVariables | Resets the design variables |
ResetTargets | Resets the targets |
SetActiveModePair | Sets a specific mode pair as active or not |
SetActiveRefMode | Sets a specific reference mode as active or not |
SetActiveSensor | Sets a specific sensor as active or not |
SetActiveSensorDof | Sets a specific sensor DOF as active or not |
SetActiveSensorDofOrientation | Sets a specific sensor DOF orientation |
SetActiveWorkMode | Sets a specific work mode as active or not |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetDesignVarActive | Sets a specific design variable as active or not |
SetDesignVarLowerBound | Sets lower bound for a specific design variable |
SetDesignVarUpperBound | Sets upper bound for a specific design variable |
SetDesignVarValue | Sets value for a specific design variable |
SetDesignVarWeight | Sets weight for a specific design variable |
SetDesignVariablesInitialValue | Sets the value of the design variables. |
SetFreqTargetActive | Sets active status for a specific frequency target |
SetFreqTargetWeight | Sets weight for a specific frequency target |
SetModeShapeTargetActive | Sets active status for a specific mode shape target |
SetModeShapeTargetWeight | Sets weight for a specific mode shape target |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSolutionName | Sets the correlation solution name |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
UnlockNodeMap | Unlock the node map. |
UpdateDesignVariables | Update the design variable modeling objects |
UpdateFiniteElementModel | Update the finite element model |
UpdateNodeMatchings | Update correlation node matchings |
UpdateResultsForSolution | Update results for correlation solution |
Enumerations¶
ModelUpdateSolutionTargetType Enumeration | Represents the type when export to targets and errors to csv file |
Property Detail¶
IsOccurrence¶
-
ModelUpdateSolution.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
ModelUpdateSolution.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
ModelUpdateSolution.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
ModelUpdateSolution.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
ModelUpdateSolution.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
ModelUpdateSolution.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
DesignVariables¶
-
ModelUpdateSolution.
DesignVariables
¶ The design variables collection for this meta solution.
Signature
DesignVariables
New in version NX8.0.1.
Returns: Return type: NXOpen.CAE.ModelUpdateDesignVariablesCollection
Method Detail¶
CalculateErrors¶
-
ModelUpdateSolution.
CalculateErrors
¶ Calculates errors
Signature
CalculateErrors()
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
CloneModelupdate¶
-
ModelUpdateSolution.
CloneModelupdate
¶ Make a clone of a model update solution.
Signature
CloneModelupdate()
Returns: Cloned solution Return type: NXOpen.CAE.ModelUpdateSolution
New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
CreateCorrelMethodBuilder¶
-
ModelUpdateSolution.
CreateCorrelMethodBuilder
¶ Creates the builder object of model update correlation method
Signature
CreateCorrelMethodBuilder()
Returns: Return type: NXOpen.CAE.ModelUpdateCorrelMethodBuilder
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
CreateOptimOptionsBuilder¶
-
ModelUpdateSolution.
CreateOptimOptionsBuilder
¶ Creates the builder object of model update optimize options
Signature
CreateOptimOptionsBuilder()
Returns: Return type: NXOpen.CAE.ModelUpdateOptimOptionsBuilder
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
CreateOptionsBuilder¶
-
ModelUpdateSolution.
CreateOptionsBuilder
¶ Creates the builder object of model update options
Signature
CreateOptionsBuilder()
Returns: Return type: NXOpen.CAE.ModelUpdateOptionsBuilder
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
CreateOverallWeightsBuilder¶
-
ModelUpdateSolution.
CreateOverallWeightsBuilder
¶ Creates the builder object of model update overall weights
Signature
CreateOverallWeightsBuilder()
Returns: Return type: NXOpen.CAE.ModelUpdateOverallWeightsBuilder
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
ExportDesignVariablesCsvFile¶
-
ModelUpdateSolution.
ExportDesignVariablesCsvFile
¶ Export the model update design variables to the csv file
Signature
ExportDesignVariablesCsvFile(fileName)
Parameters: fileName (str) – CSV file name. New in version NX7.5.1.
License requirements: nx_correl_update (“FE Model Update”)
ExportErrorsCsvFile¶
-
ModelUpdateSolution.
ExportErrorsCsvFile
¶ Export the model update errors to the csv file
Signature
ExportErrorsCsvFile(targetType, fileName)
Parameters: - targetType (
NXOpen.CAE.ModelUpdateSolutionTargetType
) – Target type of export to csv file - fileName (str) – CSV file name.
New in version NX7.5.1.
License requirements: nx_correl_update (“FE Model Update”)
- targetType (
ExportSensitivitiesCsvFile¶
-
ModelUpdateSolution.
ExportSensitivitiesCsvFile
¶ Export the model update sensitivities to the csv file
Signature
ExportSensitivitiesCsvFile(fileName)
Parameters: fileName (str) – CSV file name. New in version NX7.5.1.
License requirements: nx_correl_update (“FE Model Update”)
ExportTargetsCsvFile¶
-
ModelUpdateSolution.
ExportTargetsCsvFile
¶ Export the model update targets to the csv file
Signature
ExportTargetsCsvFile(tagetType, fileName)
Parameters: - tagetType (
NXOpen.CAE.ModelUpdateSolutionTargetType
) – Target type of export to csv file - fileName (str) – CSV file name.
New in version NX7.5.1.
License requirements: nx_correl_update (“FE Model Update”)
- tagetType (
FindObject¶
-
ModelUpdateSolution.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetDesignVarNumber¶
-
ModelUpdateSolution.
GetDesignVarNumber
¶ Gets the number of design variables
Signature
GetDesignVarNumber()
Returns: Return type: int New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
GetDesignVariables¶
-
ModelUpdateSolution.
GetDesignVariables
¶ Returns the design variables in the model update solution
Signature
GetDesignVariables()
Returns: Return type: list of NXOpen.CAE.ModelUpdateDesignVariable
New in version NX8.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
Print¶
-
ModelUpdateSolution.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
ResetDesignVariables¶
-
ModelUpdateSolution.
ResetDesignVariables
¶ Resets the design variables
Signature
ResetDesignVariables()
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
ResetTargets¶
-
ModelUpdateSolution.
ResetTargets
¶ Resets the targets
Signature
ResetTargets()
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
SetDesignVarActive¶
-
ModelUpdateSolution.
SetDesignVarActive
¶ Sets a specific design variable as active or not
Signature
SetDesignVarActive(designVarIndex, active)
Parameters: - designVarIndex (int) – index of design variable
- active (bool) – activate or deactivate flag
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
SetDesignVarLowerBound¶
-
ModelUpdateSolution.
SetDesignVarLowerBound
¶ Sets lower bound for a specific design variable
Signature
SetDesignVarLowerBound(designVarIndex, lowerBound)
Parameters: - designVarIndex (int) – index of design variable
- lowerBound (float) – new lower bound value of design variable
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
SetDesignVarUpperBound¶
-
ModelUpdateSolution.
SetDesignVarUpperBound
¶ Sets upper bound for a specific design variable
Signature
SetDesignVarUpperBound(designVarIndex, upperBound)
Parameters: - designVarIndex (int) – index of design variable
- upperBound (float) – new upper bound value of design variable
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
SetDesignVarValue¶
-
ModelUpdateSolution.
SetDesignVarValue
¶ Sets value for a specific design variable
Signature
SetDesignVarValue(designVarIndex, value)
Parameters: - designVarIndex (int) – index of design variable
- value (float) – new value of design variable
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
SetDesignVarWeight¶
-
ModelUpdateSolution.
SetDesignVarWeight
¶ Sets weight for a specific design variable
Signature
SetDesignVarWeight(designVarIndex, weight)
Parameters: - designVarIndex (int) – index of design variable
- weight (float) – new weight value of design variable
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
SetDesignVariablesInitialValue¶
-
ModelUpdateSolution.
SetDesignVariablesInitialValue
¶ Sets the value of the design variables.
Signature
SetDesignVariablesInitialValue(initialValue)
Parameters: initialValue (float) – New in version NX8.0.1.
License requirements: nx_correl_update (“FE Model Update”)
SetFreqTargetActive¶
-
ModelUpdateSolution.
SetFreqTargetActive
¶ Sets active status for a specific frequency target
Signature
SetFreqTargetActive(freqTargetIndex, active)
Parameters: - freqTargetIndex (int) – index of frequency target
- active (bool) – new active status of frequency target
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
SetFreqTargetWeight¶
-
ModelUpdateSolution.
SetFreqTargetWeight
¶ Sets weight for a specific frequency target
Signature
SetFreqTargetWeight(freqTargetIndex, weight)
Parameters: - freqTargetIndex (int) – index of frequency target
- weight (float) – new weight value of frequency target
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
SetModeShapeTargetActive¶
-
ModelUpdateSolution.
SetModeShapeTargetActive
¶ Sets active status for a specific mode shape target
Signature
SetModeShapeTargetActive(modeShapeTargetIndex, active)
Parameters: - modeShapeTargetIndex (int) – index of mode shape target
- active (bool) – new active status of mode shape target
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
SetModeShapeTargetWeight¶
-
ModelUpdateSolution.
SetModeShapeTargetWeight
¶ Sets weight for a specific mode shape target
Signature
SetModeShapeTargetWeight(modeShapeTargetIndex, modeShapeWeight)
Parameters: - modeShapeTargetIndex (int) – index of mode shape target
- modeShapeWeight (float) – new weight value of mode shape target
New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
SetName¶
-
ModelUpdateSolution.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.