CorrelSolution Class¶
-
class
NXOpen.CAE.
CorrelSolution
¶ Bases:
NXOpen.NXObject
Represents a
NXOpen.CAE.CorrelSolution
, which is a meta-solution used to compare results from two structural dynamics solutionsTo create or edit an instance of this class, use
NXOpen.CAE.CorrelSolutionBuilder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CalculateComacs | Computes the CoMAC correlation metric for active modes |
CloneCorrelation | Make a clone of a correl solution. |
ComputeMacs | Computes the Model Assurance Criterion (MAC) correlation metric for active modes |
ComputeModePairsForSol | Compute mode pairs for correlation solution |
CreateAttributeIterator | Create an attribute iterator |
CreateModePairingBuilder | Creates the builder object for mode pairing editing |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
Destroy | Deletes a correlation solution |
ExportModePairCsvFile | Export mode pair to CSV file |
ExportNodeMapCsvFile | Export node map to CSV file |
ExportShapeMetricsCsvFile | Export shape metrics to CSV file |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GenerateComacResults | Create COMAC results |
GenerateMatchingDofset | Create Matching DOFSet |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSolutionName | Returns the correlation solution name |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
ImportNodeMapCsvFile | Import node map CSV file |
LockNodeMap | Lock the node map. |
Prints a representation of this object to the system log file. | |
SetActiveModePair | Sets a specific mode pair as active or not |
SetActiveRefMode | Sets a specific reference mode as active or not |
SetActiveSensor | Sets a specific sensor as active or not |
SetActiveSensorDof | Sets a specific sensor DOF as active or not |
SetActiveSensorDofOrientation | Sets a specific sensor DOF orientation |
SetActiveWorkMode | Sets a specific work mode as active or not |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSolutionName | Sets the correlation solution name |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
UnlockNodeMap | Unlock the node map. |
UpdateNodeMatchings | Update correlation node matchings |
UpdateResultsForSolution | Update results for correlation solution |
Property Detail¶
IsOccurrence¶
-
CorrelSolution.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
CorrelSolution.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
CorrelSolution.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
CorrelSolution.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
CorrelSolution.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
CorrelSolution.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
CalculateComacs¶
-
CorrelSolution.
CalculateComacs
¶ Computes the CoMAC correlation metric for active modes
Signature
CalculateComacs()
Returns: a tuple Return type: A tuple consisting of (comacValues, referenceModeNumbers, workModeNumbers, referenceModeFrequencies, workModeFrequencies, refNodesHaveSensors, refNodeIndex, refDofIndex) comacValues is a list of float. comac values referenceModeNumbers is a list of int. reference mode numbers workModeNumbers is a list of int. work mode numbers referenceModeFrequencies is a list of float. reference mode frequencies workModeFrequencies is a list of float. work mode frequencies refNodesHaveSensors is a list of int. indicates if nodes have a sensor (0=yes, 1=no) refNodeIndex is a list of int. reference node index refDofIndex is a list of int. reference dof index New in version NX6.0.2.
License requirements: nx_correl_base (“FE Correlation”)
CloneCorrelation¶
-
CorrelSolution.
CloneCorrelation
¶ Make a clone of a correl solution.
Signature
CloneCorrelation()
Returns: Cloned solution Return type: NXOpen.CAE.CorrelSolution
New in version NX8.0.1.
License requirements: nx_correl_base (“FE Correlation”)
ComputeMacs¶
-
CorrelSolution.
ComputeMacs
¶ Computes the Model Assurance Criterion (MAC) correlation metric for active modes
Signature
ComputeMacs()
Returns: a tuple Return type: A tuple consisting of (macValues, referenceModeFrequencies, referenceModeNumbers, workModeFrequencies, workModeNumbers) macValues is a list of float. the MAC values computed referenceModeFrequencies is a list of float. ref mode frequencies referenceModeNumbers is a list of int. ref mode numbers workModeFrequencies is a list of float. work mode frequencies workModeNumbers is a list of int. work mode numbers New in version NX6.0.1.
License requirements: nx_correl_base (“FE Correlation”)
ComputeModePairsForSol¶
-
CorrelSolution.
ComputeModePairsForSol
¶ Compute mode pairs for correlation solution
Signature
ComputeModePairsForSol()
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
CreateModePairingBuilder¶
-
CorrelSolution.
CreateModePairingBuilder
¶ Creates the builder object for mode pairing editing
Signature
CreateModePairingBuilder()
Returns: Return type: NXOpen.CAE.CorrelModePairingBuilder
New in version NX6.0.1.
License requirements: nx_correl_base (“FE Correlation”)
Destroy¶
-
CorrelSolution.
Destroy
¶ Deletes a correlation solution
Signature
Destroy(deleteResultFile)
Parameters: deleteResultFile (bool) – delete the result files associated with the solution or not New in version NX5.0.0.
License requirements: nx_correl_base (“FE Correlation”)
ExportModePairCsvFile¶
-
CorrelSolution.
ExportModePairCsvFile
¶ Export mode pair to CSV file
Signature
ExportModePairCsvFile(filename)
Parameters: filename (str) – CSV file name. New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
ExportNodeMapCsvFile¶
-
CorrelSolution.
ExportNodeMapCsvFile
¶ Export node map to CSV file
Signature
ExportNodeMapCsvFile(filename)
Parameters: filename (str) – CSV file name. New in version NX9.0.1.
License requirements: nx_correl_base (“FE Correlation”)
ExportShapeMetricsCsvFile¶
-
CorrelSolution.
ExportShapeMetricsCsvFile
¶ Export shape metrics to CSV file
Signature
ExportShapeMetricsCsvFile(metricCode, filename)
Parameters: - metricCode (
NXOpen.CAE.CorrelShapemetrictype
) – shape metric code - filename (str) – CSV file name.
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
- metricCode (
FindObject¶
-
CorrelSolution.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GenerateComacResults¶
-
CorrelSolution.
GenerateComacResults
¶ Create COMAC results
Signature
GenerateComacResults()
New in version NX7.5.1.
License requirements: nx_correl_base (“FE Correlation”)
GenerateMatchingDofset¶
-
CorrelSolution.
GenerateMatchingDofset
¶ Create Matching DOFSet
Signature
GenerateMatchingDofset()
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
GetSolutionName¶
-
CorrelSolution.
GetSolutionName
¶ Returns the correlation solution name
Signature
GetSolutionName()
Returns: the NXOpen.CAE.CorrelSolution
nameReturn type: str New in version NX5.0.0.
License requirements: None.
ImportNodeMapCsvFile¶
-
CorrelSolution.
ImportNodeMapCsvFile
¶ Import node map CSV file
Signature
ImportNodeMapCsvFile(filename)
Parameters: filename (str) – CSV file name. New in version NX9.0.1.
License requirements: nx_correl_base (“FE Correlation”)
LockNodeMap¶
-
CorrelSolution.
LockNodeMap
¶ Lock the node map.
Signature
LockNodeMap()
New in version NX11.0.0.
License requirements: nx_correl_base (“FE Correlation”)
Print¶
-
CorrelSolution.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetActiveModePair¶
-
CorrelSolution.
SetActiveModePair
¶ Sets a specific mode pair as active or not
Signature
SetActiveModePair(referenceModeNumber, workModeNumber, active)
Parameters: - referenceModeNumber (int) – reference mode of the pair
- workModeNumber (int) – work mode of the pair
- active (bool) – activate or deactivate flag
New in version NX6.0.1.
License requirements: nx_correl_base (“FE Correlation”)
SetActiveRefMode¶
-
CorrelSolution.
SetActiveRefMode
¶ Sets a specific reference mode as active or not
Signature
SetActiveRefMode(refModeNumber, active)
Parameters: - refModeNumber (int) – reference mode to activate or deactivate
- active (bool) – activate or deactivate flag
New in version NX6.0.1.
License requirements: nx_correl_base (“FE Correlation”)
SetActiveSensor¶
-
CorrelSolution.
SetActiveSensor
¶ Sets a specific sensor as active or not
Signature
SetActiveSensor(sensorNumber, active)
Parameters: - sensorNumber (int) – sensor number
- active (bool) – activate or deactivate flag
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
SetActiveSensorDof¶
-
CorrelSolution.
SetActiveSensorDof
¶ Sets a specific sensor DOF as active or not
Signature
SetActiveSensorDof(sensorNumber, dofNumber, active)
Parameters: - sensorNumber (int) – sensor number
- dofNumber (int) – dof number
- active (bool) – activate or deactivate flag
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
SetActiveSensorDofOrientation¶
-
CorrelSolution.
SetActiveSensorDofOrientation
¶ Sets a specific sensor DOF orientation
Signature
SetActiveSensorDofOrientation(sensorNumber, dofNumber, orientation)
Parameters: - sensorNumber (int) – sensor number
- dofNumber (int) – dof number
- orientation (bool) – true for positive orientation or false for negative orientation
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
SetActiveWorkMode¶
-
CorrelSolution.
SetActiveWorkMode
¶ Sets a specific work mode as active or not
Signature
SetActiveWorkMode(workModeNumber, active)
Parameters: - workModeNumber (int) – work mode to activate or deactivate
- active (bool) – activate or deactivate flag
New in version NX6.0.1.
License requirements: nx_correl_base (“FE Correlation”)
SetName¶
-
CorrelSolution.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetSolutionName¶
-
CorrelSolution.
SetSolutionName
¶ Sets the correlation solution name
Signature
SetSolutionName(solutionName, renameResultFile)
Parameters: - solutionName (str) – new solution name
- renameResultFile (bool) – if there are result files associated with the solution, rename the files or not
New in version NX5.0.0.
License requirements: nx_correl_base (“FE Correlation”)
UnlockNodeMap¶
-
CorrelSolution.
UnlockNodeMap
¶ Unlock the node map.
Signature
UnlockNodeMap()
New in version NX11.0.0.
License requirements: nx_correl_base (“FE Correlation”)
UpdateNodeMatchings¶
-
CorrelSolution.
UpdateNodeMatchings
¶ Update correlation node matchings
Signature
UpdateNodeMatchings()
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
UpdateResultsForSolution¶
-
CorrelSolution.
UpdateResultsForSolution
¶ Update results for correlation solution
Signature
UpdateResultsForSolution(tSolution, ignoreReload)
Parameters: - tSolution (
NXOpen.CAE.SimSolution
) – solution - ignoreReload (bool) – ignore reload
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
- tSolution (