MeshPointProjectBuilder Class¶
-
class
NXOpen.CAE.
MeshPointProjectBuilder
¶ Bases:
NXOpen.CAE.MeshPointBaseBuilder
Represents a
NXOpen.CAE.MeshPointProjectBuilder
To create a new instance of this class, use
NXOpen.CAE.MeshPointCollection.CreateMeshpointProjectBuilder()
New in version NX5.0.2.
Properties¶
Property | Description |
---|---|
Direction | Returns or sets the direction |
MeshPointToEdit | Returns or sets the base mesh point that will be replaced or edited after the commit operation (Edit Operation). |
NodeLabel | Returns or sets the node label assigned to mesh point so that node created on the mesh point will have that label. |
Point | Returns or sets the point |
Points | Returns the points selection list |
PointsList | Returns the points selection list |
ProjectToNearestGeometry | Returns or sets the toggle |
ProjectionOption | Returns or sets the projection method type |
ProjectionTolerance | Returns or sets the projection tolerance |
Tag | Returns the Tag for this object. |
Target | Returns the target |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MeshPointProjectBuilderProjectionMethod Enumeration | the projection method types |
Property Detail¶
Direction¶
-
MeshPointProjectBuilder.
Direction
¶ Returns or sets the direction
-------------------------------------
Getter Method
Signature
Direction
Returns: Return type: NXOpen.Direction
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Direction
Parameters: direction ( NXOpen.Direction
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Point¶
-
MeshPointProjectBuilder.
Point
¶ Returns or sets the point
-------------------------------------
Getter Method
Signature
Point
Returns: Return type: NXOpen.Point
New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point
Parameters: point ( NXOpen.Point
) –New in version NX5.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
Points¶
-
MeshPointProjectBuilder.
Points
¶ Returns the points selection list
-------------------------------------
Getter Method
Signature
Points
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX11.0.0.
Deprecated since version NX12.0.0: use
NXOpen.CAE.MeshPointProjectBuilder.PointsList()
as the replacement for this property.License requirements: None.
PointsList¶
-
MeshPointProjectBuilder.
PointsList
¶ Returns the points selection list
-------------------------------------
Getter Method
Signature
PointsList
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX12.0.0.
License requirements: None.
ProjectToNearestGeometry¶
-
MeshPointProjectBuilder.
ProjectToNearestGeometry
¶ Returns or sets the toggle
-------------------------------------
Getter Method
Signature
ProjectToNearestGeometry
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectToNearestGeometry
Parameters: toggle (bool) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ProjectionOption¶
-
MeshPointProjectBuilder.
ProjectionOption
¶ Returns or sets the projection method type
-------------------------------------
Getter Method
Signature
ProjectionOption
Returns: Return type: NXOpen.CAE.MeshPointProjectBuilderProjectionMethod
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectionOption
Parameters: projectionType ( NXOpen.CAE.MeshPointProjectBuilderProjectionMethod
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ProjectionTolerance¶
-
MeshPointProjectBuilder.
ProjectionTolerance
¶ Returns or sets the projection tolerance
-------------------------------------
Getter Method
Signature
ProjectionTolerance
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectionTolerance
Parameters: projectionTol (float) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Target¶
-
MeshPointProjectBuilder.
Target
¶ Returns the target
-------------------------------------
Getter Method
Signature
Target
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX6.0.2.
License requirements: None.
Method Detail¶
Validate¶
-
MeshPointProjectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.