MeshPointProjectBuilderProjectionMethod Enumeration

NXOpen.CAE.MeshPointProjectBuilder.ProjectionMethod is an alias for NXOpen.CAE.MeshPointProjectBuilderProjectionMethod

class NXOpen.CAE.MeshPointProjectBuilderProjectionMethod

Bases: object

the projection method types

Enum Members

Enum Member Enum Member Description
TypeNearestPoint
TypeAlongVector
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.