LaminateRandomEventBuilder Class¶
-
class
NXOpen.CAE.
LaminateRandomEventBuilder
¶ Bases:
NXOpen.CAE.LaminateDynamicEventBuilder
Represents a
NXOpen.CAE.LaminateRandomEvent
builderTo create a new instance of this class, use
NXOpen.CAE.LaminateDynamicEventCollection.CreateRandomEventBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ConfidenceLevel | Returns or sets the confidence level (in %) |
ConfidenceLevelOption | Returns or sets the confidence level option |
DynamicEventName | Returns or sets the event name |
EventName | Returns or sets the event name |
ExcitationAxis | Returns or sets the excitation axis |
ExcitationCoordinateSystem | Returns or sets the excitation coordinate system |
ExcitationCsys | Returns or sets the excitation coordinate system |
ExcitationSelectedAxis | Returns or sets the excitation axis |
Function | Returns or sets the function. |
LowerBoundFreq | Returns or sets the lower bound freq |
LowerBoundFrequency | Returns or sets the lower bound freq |
NastranBasic | Returns or sets the nastran basic |
NastranBasicCsys | Returns or sets the nastran basic |
Reference | Returns or sets the reference |
ReferenceType | Returns or sets the reference type |
StandardDeviation | Returns or sets the number of standard deviations used to calculate the confidence level |
Tag | Returns the Tag for this object. |
UpperBoundFreq | Returns or sets the upper bound freq |
UpperBoundFrequency | Returns or sets the upper bound freq |
UserFunction | Returns or sets the function. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOutputRequest | Get the output request. |
GetOutputRequestObject | Get the output request. |
SetOutputRequest | Set the output request. |
SetOutputRequestObject | Set the output request. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LaminateRandomEventBuilderConfidenceLevelOptionEnum Enumeration | The confidence level option. |
LaminateRandomEventBuilderExcitationAxisEnum Enumeration | The excitation axis enum. |
LaminateRandomEventBuilderReferenceEnum Enumeration | The reference enum. |
Property Detail¶
ConfidenceLevel¶
-
LaminateRandomEventBuilder.
ConfidenceLevel
¶ Returns or sets the confidence level (in %)
-------------------------------------
Getter Method
Signature
ConfidenceLevel
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConfidenceLevel
Parameters: confidenceLevel (float) – New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ConfidenceLevelOption¶
-
LaminateRandomEventBuilder.
ConfidenceLevelOption
¶ Returns or sets the confidence level option
-------------------------------------
Getter Method
Signature
ConfidenceLevelOption
Returns: Return type: NXOpen.CAE.LaminateRandomEventBuilderConfidenceLevelOptionEnum
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConfidenceLevelOption
Parameters: confidenceLevelOption ( NXOpen.CAE.LaminateRandomEventBuilderConfidenceLevelOptionEnum
) –New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
EventName¶
-
LaminateRandomEventBuilder.
EventName
¶ Returns or sets the event name
-------------------------------------
Getter Method
Signature
EventName
Returns: Return type: str New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.DynamicEventName()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
EventName
Parameters: eventName (str) – New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetDynamicEventName()
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ExcitationAxis¶
-
LaminateRandomEventBuilder.
ExcitationAxis
¶ Returns or sets the excitation axis
-------------------------------------
Getter Method
Signature
ExcitationAxis
Returns: Return type: NXOpen.CAE.LaminateRandomEventBuilderExcitationAxisEnum
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.ExcitationSelectedAxis()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ExcitationAxis
Parameters: excitationAxis ( NXOpen.CAE.LaminateRandomEventBuilderExcitationAxisEnum
) –New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetExcitationSelectedAxis()
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ExcitationCoordinateSystem¶
-
LaminateRandomEventBuilder.
ExcitationCoordinateSystem
¶ Returns or sets the excitation coordinate system
-------------------------------------
Getter Method
Signature
ExcitationCoordinateSystem
Returns: Return type: NXOpen.CoordinateSystem
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.ExcitationCsys()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ExcitationCoordinateSystem
Parameters: excitationCoordinateSystem ( NXOpen.CoordinateSystem
) –New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetExcitationCsys()
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Function¶
-
LaminateRandomEventBuilder.
Function
¶ Returns or sets the function.
-------------------------------------
Getter Method
Signature
Function
Returns: Return type: NXOpen.TaggedObject
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.UserFunction()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Function
Parameters: functionTag ( NXOpen.TaggedObject
) –New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetUserFunction()
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
LowerBoundFreq¶
-
LaminateRandomEventBuilder.
LowerBoundFreq
¶ Returns or sets the lower bound freq
-------------------------------------
Getter Method
Signature
LowerBoundFreq
Returns: Return type: float New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.LowerBoundFrequency()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
LowerBoundFreq
Parameters: lowerBoundFreq (float) – New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetLowerBoundFrequency()
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
NastranBasic¶
-
LaminateRandomEventBuilder.
NastranBasic
¶ Returns or sets the nastran basic
-------------------------------------
Getter Method
Signature
NastranBasic
Returns: Return type: bool New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.NastranBasicCsys()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
NastranBasic
Parameters: nastranBasic (bool) – New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetNastranBasicCsys()
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Reference¶
-
LaminateRandomEventBuilder.
Reference
¶ Returns or sets the reference
-------------------------------------
Getter Method
Signature
Reference
Returns: Return type: NXOpen.CAE.LaminateRandomEventBuilderReferenceEnum
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.ReferenceType()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Reference
Parameters: reference ( NXOpen.CAE.LaminateRandomEventBuilderReferenceEnum
) –New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetReferenceType()
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
StandardDeviation¶
-
LaminateRandomEventBuilder.
StandardDeviation
¶ Returns or sets the number of standard deviations used to calculate the confidence level
-------------------------------------
Getter Method
Signature
StandardDeviation
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StandardDeviation
Parameters: standardDeviation (float) – New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
UpperBoundFreq¶
-
LaminateRandomEventBuilder.
UpperBoundFreq
¶ Returns or sets the upper bound freq
-------------------------------------
Getter Method
Signature
UpperBoundFreq
Returns: Return type: float New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.UpperBoundFrequency()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
UpperBoundFreq
Parameters: upperBoundFreq (float) – New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetUpperBoundFrequency()
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Method Detail¶
GetOutputRequest¶
-
LaminateRandomEventBuilder.
GetOutputRequest
¶ Get the output request.
Signature
GetOutputRequest()
Returns: Return type: NXOpen.CAE.ModelingObjectPropertyTable
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.GetOutputRequestObject()
instead.License requirements: None.
SetOutputRequest¶
-
LaminateRandomEventBuilder.
SetOutputRequest
¶ Set the output request.
Signature
SetOutputRequest(ssmo)
Parameters: ssmo ( NXOpen.CAE.ModelingObjectPropertyTable
) –New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateDynamicEventBuilder.SetOutputRequestObject()
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Validate¶
-
LaminateRandomEventBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.