LaminateRandomEventBuilderConfidenceLevelOptionEnum Enumeration

NXOpen.CAE.LaminateRandomEventBuilder.ConfidenceLevelOptionEnum is an alias for NXOpen.CAE.LaminateRandomEventBuilderConfidenceLevelOptionEnum

class NXOpen.CAE.LaminateRandomEventBuilderConfidenceLevelOptionEnum

Bases: object

The confidence level option.

Enum Members

Enum Member Enum Member Description
UserDef
StandardDev
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.