LaminateRandomEventBuilderReferenceEnum Enumeration

NXOpen.CAE.LaminateRandomEventBuilder.ReferenceEnum is an alias for NXOpen.CAE.LaminateRandomEventBuilderReferenceEnum

class NXOpen.CAE.LaminateRandomEventBuilderReferenceEnum

Bases: object

The reference enum.

Deprecated since version NX10.0.0: Use NXOpen.CAE.LaminateDynamicEventBuilderReferenceTypeEnum instead.

Enum Members

Enum Member Enum Member Description
Relative
Absolute
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.