LaminateDynamicEventBuilderReferenceTypeEnum Enumeration

NXOpen.CAE.LaminateDynamicEventBuilder.ReferenceTypeEnum is an alias for NXOpen.CAE.LaminateDynamicEventBuilderReferenceTypeEnum

class NXOpen.CAE.LaminateDynamicEventBuilderReferenceTypeEnum

Bases: object

The reference enum.

Enum Members

Enum Member Enum Member Description
Relative
Absolute
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.