ElementAssociatedDataUtils Class¶
-
class
NXOpen.CAE.
ElementAssociatedDataUtils
¶ Bases:
object
Represents a system to access element associated data
To obtain an instance of this class, refer to
NXOpen.CAE.NodeElementManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
AskBeamData | Returns beam element associated data. |
AskBushingData | Returns bushing element associated data. |
AskConstraintEquationData | Returns constraint element associated data. |
AskDamperData | Returns damper element associated data. |
AskGapData | Returns gap element associated data. |
AskInterpolationData | Returns interpolation element associated data. |
AskLumpedMassData | Returns lumped mass element associated data. |
AskRigidData | Returns rigid element associated data. |
AskShellData | Returns shell element associated data. |
AskSpringData | Returns spring element associated data. |
SetBeamData | Sets beam element associated data. |
SetBushingData | Sets bushing element associated data. |
SetConstraintEquationData | Sets constraint element associated data. |
SetDamperData | Sets damper element associated data. |
SetGapData | Sets gap element associated data. |
SetInterpolationData | Sets interpolation element associated data. |
SetLumpedMassData | Sets lumped mass element associated data. |
SetRigidData | Sets rigid element associated data. |
SetShellData | Sets shell element associated data. |
SetSpringData | Sets spring element associated data. |
Method Detail¶
AskBeamData¶
-
ElementAssociatedDataUtils.
AskBeamData
¶ Returns beam element associated data.
Signature
AskBeamData(element)
Parameters: element ( NXOpen.CAE.FEElement
) –Returns: a tuple Return type: A tuple consisting of (hasAssociatedDataDefined, physicalPropertyTable, oriMethod, vectorType, direction, orientationNode, endAState, pinFlagEndADOF1, pinFlagEndADOF2, pinFlagEndADOF3, pinFlagEndADOF4, pinFlagEndADOF5, pinFlagEndADOF6, endBState, pinFlagEndBDOF1, pinFlagEndBDOF2, pinFlagEndBDOF3, pinFlagEndBDOF4, pinFlagEndBDOF5, pinFlagEndBDOF6, xOffsetEndA, yOffsetEndA, zOffsetEndA, xOffsetEndB, yOffsetEndB, zOffsetEndB). hasAssociatedDataDefined is a bool. True if element has element associated data defined. If false, the parameters that follow are ignored. physicalPropertyTable is a NXOpen.CAE.PhysicalPropertyTable
. Physical property table of the beam element. oriMethod is aNXOpen.CAE.CaeElementAssociatedDataUtilsOrientationMethod
. Orientation method. vectorType is aNXOpen.CAE.CaeElementAssociatedDataUtilsVectorChoiceType
. Orientation vector type. Only used if orientation method is vector. direction is aNXOpen.Direction
. Orientation direction. Only used if orientation method is vector. orientationNode is aNXOpen.CAE.FENode
. Orientation node. Only used if orientation method is node. endAState is aNXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseState
. Pin flags End A state pinFlagEndADOF1 is aNXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
. Pin flag End A for DOF 1. pinFlagEndADOF2 is aNXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
. Pin flag End A for DOF 2. pinFlagEndADOF3 is aNXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
. Pin flag End A for DOF 3. pinFlagEndADOF4 is aNXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
. Pin flag End A for DOF 4. pinFlagEndADOF5 is aNXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
. Pin flag End A for DOF 5. pinFlagEndADOF6 is aNXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
. Pin flag End A for DOF 6. endBState is aNXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseState
. Pin flags End B state pinFlagEndBDOF1 is aNXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
. Pin flag End B for DOF 1. pinFlagEndBDOF2 is aNXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
. Pin flag End B for DOF 2. pinFlagEndBDOF3 is aNXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
. Pin flag End B for DOF 3. pinFlagEndBDOF4 is aNXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
. Pin flag End B for DOF 4. pinFlagEndBDOF5 is aNXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
. Pin flag End B for DOF 5. pinFlagEndBDOF6 is aNXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
. Pin flag End B for DOF 6. xOffsetEndA is a float. X offset to shear center in nodal displacement coordinate system for End A in units mm or in. yOffsetEndA is a float. Y offset to shear center in nodal displacement coordinate system for End A in units mm or in. zOffsetEndA is a float. Z offset to shear center in nodal displacement coordinate system for End A in units mm or in. xOffsetEndB is a float. X offset to shear center in nodal displacement coordinate system for End B in units mm or in. yOffsetEndB is a float. Y offset to shear center in nodal displacement coordinate system for End B in units mm or in. zOffsetEndB is a float. Z offset to shear center in nodal displacement coordinate system for End B in units mm or in.New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
AskBushingData¶
-
ElementAssociatedDataUtils.
AskBushingData
¶ Returns bushing element associated data.
Signature
AskBushingData(element, originPoint, zAxisPoint, planePoint)
Parameters: - element (
NXOpen.CAE.FEElement
) – - originPoint (
NXOpen.Point3d
) – Orientation csys data origin point. - zAxisPoint (
NXOpen.Point3d
) – Orientation csys data point on z-axis. - planePoint (
NXOpen.Point3d
) – Orientation csys data point in the x-z plane if cartesian csys or azimuthal origin plane if cylindrical/spherical csys.
Returns: a tuple
Return type: A tuple consisting of (hasAssociatedDataDefined, physicalPropertyTable, oriMethod, oriDirr, coordinateSystem, oriNode, csysDataType, preferredLabel). hasAssociatedDataDefined is a bool. True if element has element associated data defined. If false, the parameters that follow are ignored. physicalPropertyTable is a
NXOpen.CAE.PhysicalPropertyTable
. Physical property table of the bushing element. oriMethod is aNXOpen.CAE.CaeElementAssociatedDataUtilsOrientationMethod
. Orientation method. oriDirr is aNXOpen.Direction
. Orientation vector. coordinateSystem is aNXOpen.CoordinateSystem
. Coordinate system for orienting by coordinate system. oriNode is aNXOpen.CAE.FENode
. Orientation node. csysDataType is aNXOpen.CAE.CaeElementAssociatedDataUtilsCsysDataType
. Orientation coordinate system type for csys data option. preferredLabel is a int. Preferred coordinate system label for csys data export.New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- element (
AskConstraintEquationData¶
-
ElementAssociatedDataUtils.
AskConstraintEquationData
¶ Returns constraint element associated data.
Signature
AskConstraintEquationData(element)
Parameters: element ( NXOpen.CAE.FEElement
) –Returns: a tuple Return type: A tuple consisting of (hasAssociatedDataDefined, terms, constantTerm). hasAssociatedDataDefined is a bool. True if element has element associated data defined. If false, the parameters that follow are ignored. terms is a list of NXOpen.CAE.DofTerm
. Term of dof in the constraint equation. The first degree of freedom in the array defines the dependent degree of freedom. constantTerm is a float. The constant term is the constant that the constraint equation equals. This value is not used by all solvers.New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
AskDamperData¶
-
ElementAssociatedDataUtils.
AskDamperData
¶ Returns damper element associated data.
Signature
AskDamperData(element)
Parameters: element ( NXOpen.CAE.FEElement
) –Returns: a tuple Return type: A tuple consisting of (hasAssociatedDataDefined, viscousDamping, physicalPropertyTable, componentEndA, componentEndB). hasAssociatedDataDefined is a bool. True if element has element associated data defined. If false, the parameters that follow are ignored. viscousDamping is a float. Viscous damping value either translational in units N-sec/mm or lbf-sec/in or rotational in units mN-mm-sec or lbf-in-sec. physicalPropertyTable is a NXOpen.CAE.PhysicalPropertyTable
. Physical property table of the damper element. componentEndA is aNXOpen.CAE.CaeElementAssociatedDataUtilsComponentEnd
. Component end A of the damper element (either translational or rotational). componentEndB is aNXOpen.CAE.CaeElementAssociatedDataUtilsComponentEnd
. Component end B of the damper element (either translational or rotational).New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
AskGapData¶
-
ElementAssociatedDataUtils.
AskGapData
¶ Returns gap element associated data.
Signature
AskGapData(element)
Parameters: element ( NXOpen.CAE.FEElement
) –Returns: a tuple Return type: A tuple consisting of (hasAssociatedDataDefined, physicalPropertyTable, oriMethod, oriDirr, coordinateSystem, oriNode). hasAssociatedDataDefined is a bool. True if element has element associated data defined. If false, the parameters that follow are ignored. physicalPropertyTable is a NXOpen.CAE.PhysicalPropertyTable
. Physical property table of the gap element. oriMethod is aNXOpen.CAE.CaeElementAssociatedDataUtilsOrientationMethod
. Orientation method. oriDirr is aNXOpen.Direction
. Orientation vector. coordinateSystem is aNXOpen.CoordinateSystem
. Coordinate system for orienting by coordinate system. oriNode is aNXOpen.CAE.FENode
. Orientation node.New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
AskInterpolationData¶
-
ElementAssociatedDataUtils.
AskInterpolationData
¶ Returns interpolation element associated data.
Signature
AskInterpolationData(element)
Parameters: element ( NXOpen.CAE.FEElement
) –Returns: a tuple Return type: A tuple consisting of (umData, hasAssociatedDataDefined, dofDataTerms). umData is a list of int. Data that indicates the start of the degrees-of-freedom belonging to the m-set. This value is not used by all solvers. hasAssociatedDataDefined is a bool. True if element has element associated data defined. If false, the parameters that follow are ignored. dofDataTerms is a list of NXOpen.CAE.DofTerm
. Term of dof in the interpolation element.New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
AskLumpedMassData¶
-
ElementAssociatedDataUtils.
AskLumpedMassData
¶ Returns lumped mass element associated data.
Signature
AskLumpedMassData(element)
Parameters: element ( NXOpen.CAE.FEElement
) –Returns: a tuple Return type: A tuple consisting of (hasAssociatedDataDefined, mass) hasAssociatedDataDefined is a bool. True if element has element associated data defined. If false, the parameters that follow are ignored. mass is a float. Mass value. New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
AskRigidData¶
-
ElementAssociatedDataUtils.
AskRigidData
¶ Returns rigid element associated data.
Signature
AskRigidData(element)
Parameters: element ( NXOpen.CAE.FEElement
) –Returns: a tuple Return type: A tuple consisting of (hasAssociatedDataDefined, dofs). hasAssociatedDataDefined is a bool. True if element has element associated data defined. If false, the parameters that follow are ignored. dofs is a list of NXOpen.CAE.CaeElementAssociatedDataUtilsDof
. The 6 dofs of the rigid element.New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
AskShellData¶
-
ElementAssociatedDataUtils.
AskShellData
¶ Returns shell element associated data.
Signature
AskShellData(element, originPoint, zAxisPoint, planePoint)
Parameters: - element (
NXOpen.CAE.FEElement
) – - originPoint (
NXOpen.Point3d
) – Material orientation csys data origin point. - zAxisPoint (
NXOpen.Point3d
) – Material orientation csys data point on z-axis. - planePoint (
NXOpen.Point3d
) – Material orientation csys data point in the x-z plane if cartesian csys or azimuthal origin plane if cylindrical/spherical csys.
Returns: a tuple
Return type: A tuple consisting of (hasAssociatedDataDefined, cornerNodeThicknesses, cornerNodeGapValues, zOffset, physicalPropertyTable, matOriMethod, coordinateSystem, matOriAngle, csysDataType, preferredLabel). hasAssociatedDataDefined is a bool. True if element has element associated data defined. If false, the parameters that follow are ignored. cornerNodeThicknesses is a list of float. Corner node thicknesses in units mm or in. cornerNodeGapValues is a list of float. Corner node gap values in units mm or in. zOffset is a float. Z offset value. physicalPropertyTable is a
NXOpen.CAE.PhysicalPropertyTable
. Physical property table of the shell element. matOriMethod is aNXOpen.CAE.CaeElementAssociatedDataUtilsMatOrientationMethod
. Material orientation method. coordinateSystem is aNXOpen.CoordinateSystem
. Coordinate system for orienting by coordinate system. matOriAngle is a float. Material orientation angle. csysDataType is aNXOpen.CAE.CaeElementAssociatedDataUtilsCsysDataType
. Material orientation coordinate system type for csys data option. preferredLabel is a int. Preferred coordinate system label for csys data export.New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- element (
AskSpringData¶
-
ElementAssociatedDataUtils.
AskSpringData
¶ Returns spring element associated data.
Signature
AskSpringData(element)
Parameters: element ( NXOpen.CAE.FEElement
) –Returns: a tuple Return type: A tuple consisting of (hasAssociatedDataDefined, physicalPropertyTable, stiffness, componentEndA, componentEndB). hasAssociatedDataDefined is a bool. True if element has element associated data defined. If false, the parameters that follow are ignored. physicalPropertyTable is a NXOpen.CAE.PhysicalPropertyTable
. Physical property table of the spring element. stiffness is a float. Spring stiffness value either translational in units N/mm or lbf/in or rotational in units N-mm or lbf-in. componentEndA is aNXOpen.CAE.CaeElementAssociatedDataUtilsComponentEnd
. Component end A of the spring element (either translational or rotational). componentEndB is aNXOpen.CAE.CaeElementAssociatedDataUtilsComponentEnd
. Component end B of the spring element (either translational or rotational).New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetBeamData¶
-
ElementAssociatedDataUtils.
SetBeamData
¶ Sets beam element associated data.
Signature
SetBeamData(element, physicalPropertyTable, oriMethod, vectorType, direction, orientationNode, endReleaseA, pinFlagEndADOF1, pinFlagEndADOF2, pinFlagEndADOF3, pinFlagEndADOF4, pinFlagEndADOF5, pinFlagEndADOF6, endReleaseB, pinFlagEndBDOF1, pinFlagEndBDOF2, pinFlagEndBDOF3, pinFlagEndBDOF4, pinFlagEndBDOF5, pinFlagEndBDOF6, xOffsetEndA, yOffsetEndA, zOffsetEndA, xOffsetEndB, yOffsetEndB, zOffsetEndB)
Parameters: - element (
NXOpen.CAE.FEElement
) – - physicalPropertyTable (
NXOpen.CAE.PhysicalPropertyTable
) – Physical property table of the beam element. - oriMethod (
NXOpen.CAE.CaeElementAssociatedDataUtilsOrientationMethod
) – Orientation method. - vectorType (
NXOpen.CAE.CaeElementAssociatedDataUtilsVectorChoiceType
) – Orientation vector type. Only used if orientation method is vector. - direction (
NXOpen.Direction
) – Orientation direction. Only used if orientation method is vector. - orientationNode (
NXOpen.CAE.FENode
) – Orientation node. Only used if orientation method is node. - endReleaseA (
NXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseState
) – End Release A state. - pinFlagEndADOF1 (
NXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
) – Pin flag End A for DOF 1. - pinFlagEndADOF2 (
NXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
) – Pin flag End A for DOF 2. - pinFlagEndADOF3 (
NXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
) – Pin flag End A for DOF 3. - pinFlagEndADOF4 (
NXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
) – Pin flag End A for DOF 4. - pinFlagEndADOF5 (
NXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
) – Pin flag End A for DOF 5. - pinFlagEndADOF6 (
NXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
) – Pin flag End A for DOF 6. - endReleaseB (
NXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseState
) – End Release B state. - pinFlagEndBDOF1 (
NXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
) – Pin flag End B for DOF 1. - pinFlagEndBDOF2 (
NXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
) – Pin flag End B for DOF 2. - pinFlagEndBDOF3 (
NXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
) – Pin flag End B for DOF 3. - pinFlagEndBDOF4 (
NXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
) – Pin flag End B for DOF 4. - pinFlagEndBDOF5 (
NXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
) – Pin flag End B for DOF 5. - pinFlagEndBDOF6 (
NXOpen.CAE.CaeElementAssociatedDataUtilsEndReleaseSetting
) – Pin flag End B for DOF 6. - xOffsetEndA (float) – X offset to shear center in nodal displacement coordinate system for End A in units mm or in.
- yOffsetEndA (float) – Y offset to shear center in nodal displacement coordinate system for End A in units mm or in.
- zOffsetEndA (float) – Z offset to shear center in nodal displacement coordinate system for End A in units mm or in.
- xOffsetEndB (float) – X offset to shear center in nodal displacement coordinate system for End B in units mm or in.
- yOffsetEndB (float) – Y offset to shear center in nodal displacement coordinate system for End B in units mm or in.
- zOffsetEndB (float) – Z offset to shear center in nodal displacement coordinate system for End B in units mm or in.
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- element (
SetBushingData¶
-
ElementAssociatedDataUtils.
SetBushingData
¶ Sets bushing element associated data.
Signature
SetBushingData(element, physicalPropertyTable, oriMethod, oriDirr, coordinateSystem, oriNode, csysDataType, originPoint, zAxisPoint, planePoint, preferredLabel)
Parameters: - element (
NXOpen.CAE.FEElement
) – - physicalPropertyTable (
NXOpen.CAE.PhysicalPropertyTable
) – Physical property table of the bushing element. - oriMethod (
NXOpen.CAE.CaeElementAssociatedDataUtilsOrientationMethod
) – Material orientation method. - oriDirr (
NXOpen.Direction
) – Orientation vector. - coordinateSystem (
NXOpen.CoordinateSystem
) – Coordinate system for orienting by coordinate system. - oriNode (
NXOpen.CAE.FENode
) – Orientation node. - csysDataType (
NXOpen.CAE.CaeElementAssociatedDataUtilsCsysDataType
) – Orientation coordinate system type for csys data option. - originPoint (
NXOpen.Point3d
) – Orientation csys data origin point. - zAxisPoint (
NXOpen.Point3d
) – Orientation csys data point on z-axis. - planePoint (
NXOpen.Point3d
) – Orientation csys data point in the x-z plane if cartesian csys or azimuthal origin plane if cylindrical/spherical csys. - preferredLabel (int) – Preferred coordinate system label for csys data export.
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- element (
SetConstraintEquationData¶
-
ElementAssociatedDataUtils.
SetConstraintEquationData
¶ Sets constraint element associated data.
Signature
SetConstraintEquationData(element, terms, constantTerm)
Parameters: - element (
NXOpen.CAE.FEElement
) – - terms (list of
NXOpen.CAE.DofTerm
) – Term of dof in the constraint equation. The first degree of freedom in the array defines the dependent degree of freedom. - constantTerm (float) – The constant term is the constant that the constraint equation equals. This value is not used by all solvers.
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- element (
SetDamperData¶
-
ElementAssociatedDataUtils.
SetDamperData
¶ Sets damper element associated data.
Signature
SetDamperData(element, viscousDamping, physicalPropertyTable, componentEndA, componentEndB)
Parameters: - element (
NXOpen.CAE.FEElement
) – - viscousDamping (float) – Viscous damping value either translational in units N-sec/mm or lbf-sec/in or rotational in units mN-mm-sec or lbf-in-sec.
- physicalPropertyTable (
NXOpen.CAE.PhysicalPropertyTable
) – Physical property table of the damper element. - componentEndA (
NXOpen.CAE.CaeElementAssociatedDataUtilsComponentEnd
) – Component end A of the damper element (either translational or rotational. - componentEndB (
NXOpen.CAE.CaeElementAssociatedDataUtilsComponentEnd
) – Component end B of the damper element (either translational or rotational.
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- element (
SetGapData¶
-
ElementAssociatedDataUtils.
SetGapData
¶ Sets gap element associated data.
Signature
SetGapData(element, physicalPropertyTable, oriMethod, oriDirr, coordinateSystem, oriNode)
Parameters: - element (
NXOpen.CAE.FEElement
) – - physicalPropertyTable (
NXOpen.CAE.PhysicalPropertyTable
) – Physical property table of the gap element. - oriMethod (
NXOpen.CAE.CaeElementAssociatedDataUtilsOrientationMethod
) – Material orientation method. - oriDirr (
NXOpen.Direction
) – Orientation vector. - coordinateSystem (
NXOpen.CoordinateSystem
) – Coordinate system for orienting by coordinate system. - oriNode (
NXOpen.CAE.FENode
) – Orientation node.
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- element (
SetInterpolationData¶
-
ElementAssociatedDataUtils.
SetInterpolationData
¶ Sets interpolation element associated data.
Signature
SetInterpolationData(element, dofDataTerms, umData)
Parameters: - element (
NXOpen.CAE.FEElement
) – - dofDataTerms (list of
NXOpen.CAE.DofTerm
) – Term of dof in the interpolation element. - umData (list of int) – Data that indicates the start of the degrees-of-freedom belonging to the m-set. This value is not used by all solvers.
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- element (
SetLumpedMassData¶
-
ElementAssociatedDataUtils.
SetLumpedMassData
¶ Sets lumped mass element associated data.
Signature
SetLumpedMassData(element, mass)
Parameters: - element (
NXOpen.CAE.FEElement
) – - mass (float) – Mass value in units kg or lbm.
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- element (
SetRigidData¶
-
ElementAssociatedDataUtils.
SetRigidData
¶ Sets rigid element associated data.
Signature
SetRigidData(element, dofs)
Parameters: - element (
NXOpen.CAE.FEElement
) – - dofs (list of
NXOpen.CAE.CaeElementAssociatedDataUtilsDof
) – The 6 dofs of the rigid element.
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- element (
SetShellData¶
-
ElementAssociatedDataUtils.
SetShellData
¶ Sets shell element associated data.
Signature
SetShellData(element, cornerNodeThicknesses, cornerNodeGapValues, zOffset, physicalPropertyTable, matOriMethod, coordinateSystem, matOriAngle, csysDataType, originPoint, zAxisPoint, planePoint, preferredLabel)
Parameters: - element (
NXOpen.CAE.FEElement
) – - cornerNodeThicknesses (list of float) – Corner node thicknesses in units mm or in.
- cornerNodeGapValues (list of float) – Corner node gap values in units mm or in.
- zOffset (float) – Z offset value.
- physicalPropertyTable (
NXOpen.CAE.PhysicalPropertyTable
) – Physical property table of the shell element. - matOriMethod (
NXOpen.CAE.CaeElementAssociatedDataUtilsMatOrientationMethod
) – Material orientation method. - coordinateSystem (
NXOpen.CoordinateSystem
) – Coordinate system for orienting by coordinate system. - matOriAngle (float) – Material orientation angle.
- csysDataType (
NXOpen.CAE.CaeElementAssociatedDataUtilsCsysDataType
) – Material orientation coordinate system type for csys data option. - originPoint (
NXOpen.Point3d
) – Material orientation csys data origin point. - zAxisPoint (
NXOpen.Point3d
) – Material orientation csys data point on z-axis. - planePoint (
NXOpen.Point3d
) – Material orientation csys data point in the x-z plane if cartesian csys or azimuthal origin plane if cylindrical/spherical csys. - preferredLabel (int) – Preferred coordinate system label for csys data export.
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- element (
SetSpringData¶
-
ElementAssociatedDataUtils.
SetSpringData
¶ Sets spring element associated data.
Signature
SetSpringData(element, physicalPropertyTable, stiffness, componentEndA, componentEndB)
Parameters: - element (
NXOpen.CAE.FEElement
) – - physicalPropertyTable (
NXOpen.CAE.PhysicalPropertyTable
) – Physical property table of the spring element. - stiffness (float) – Spring stiffness value either translational in units N/mm or lbf/in or rotational in units N-mm or lbf-in.
- componentEndA (
NXOpen.CAE.CaeElementAssociatedDataUtilsComponentEnd
) – Component end A of the spring element (either translational or rotational. - componentEndB (
NXOpen.CAE.CaeElementAssociatedDataUtilsComponentEnd
) – Component end B of the spring element (either translational or rotational.
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- element (