CaeElementAssociatedDataUtilsOrientationMethod Enumeration¶
-
class
NXOpen.CAE.
CaeElementAssociatedDataUtilsOrientationMethod
¶ Bases:
object
Indicates which orientation method to use Enum Members
Enum Member Enum Member Description NotSet No material orientation specified. Vector Use a vector to orient the element Csystem Use a csystem to orient the element Node Use a node to orient the element CsystemData Use a csys data to orient the element -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-