CaeElementAssociatedDataUtilsCsysDataType Enumeration¶
-
class
NXOpen.CAE.
CaeElementAssociatedDataUtilsCsysDataType
¶ Bases:
object
Indicates which type of coordinate system to use if using coordinate system data to orient the material. Enum Members
Enum Member Enum Member Description Cartesian Use cartesian coordinate system data to orient the material. Cylindrical Use cylindrical coordinate system data to orient the material. Spherical Use spherical coordinate system data to orient the material. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-