BlockDialog Class¶
-
class
NXOpen.BlockStyler.
BlockDialog
¶ Bases:
NXOpen.TransientObject
Represents a Dialog
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
TopBlock | Returns a composite block that contains all the blocks in the dialog |
Methods¶
Method | Description |
---|---|
AddApplyHandler | Adds Apply callback handler to the dialog. |
AddCancelHandler | Adds Cancel callback handler to the dialog. |
AddCloseHandler | Adds Close callback handler to the dialog. |
AddDialogShownHandler | Adds Dialog Shown callback handler to the dialog. |
AddEnableOKButtonHandler | Adds enable-ok-button callback handler to the dialog. |
AddFilterHandler | Adds Filter callback handler to the dialog. |
AddFocusNotifyHandler | Adds focus notify callback handler to the dialog. |
AddInitializeHandler | Adds Initialize callback handler to the dialog. |
AddKeyboardFocusNotifyHandler | Adds keyboard focus notify callback handler to the dialog. |
AddOkHandler | Adds Ok callback handler to the dialog. |
AddUpdateHandler | Adds Update callback handler to the dialog. |
Dispose | Frees the object from memory. |
GetBlockProperties | Gets the properties of a block |
PerformApply | Performs an Apply and restarts the dialog. |
RegisterUserDefinedUIBlock | Registers the reusable block with the dialog |
Show | Shows the dialog in BlockStyler.BlockDialogDialogMode.Create mode. |
Enumerations¶
BlockDialogDialogMode Enumeration | Datatype containing options for showing the dialog |
Property Detail¶
TopBlock¶
-
BlockDialog.
TopBlock
¶ Returns a composite block that contains all the blocks in the dialog
-------------------------------------
Getter Method
Signature
TopBlock
Returns: Return type: NXOpen.BlockStyler.CompositeBlock
New in version NX6.0.0.
License requirements: None.
Method Detail¶
AddApplyHandler¶
-
BlockDialog.
AddApplyHandler
¶ Adds Apply callback handler to the dialog.
Signature
AddApplyHandler(applyCb)
Parameters: applyCb (CallableObject) – New in version NX6.0.0.
License requirements: None.
AddCancelHandler¶
-
BlockDialog.
AddCancelHandler
¶ Adds Cancel callback handler to the dialog.
Signature
AddCancelHandler(cancelCb)
Parameters: cancelCb (CallableObject) – New in version NX6.0.0.
License requirements: None.
AddCloseHandler¶
-
BlockDialog.
AddCloseHandler
¶ Adds Close callback handler to the dialog.
Signature
AddCloseHandler(closeCb)
Parameters: closeCb (CallableObject) – New in version NX8.5.0.
License requirements: None.
AddDialogShownHandler¶
-
BlockDialog.
AddDialogShownHandler
¶ Adds Dialog Shown callback handler to the dialog.
The callback function is called before the dialog is shown. The callback can be used to overwrite changes that are made during dialog initialization when user inputs saved in dialog memory are applied to the dialog.
Signature
AddDialogShownHandler(cb)
Parameters: cb (CallableObject) – New in version NX6.0.0.
License requirements: None.
AddEnableOKButtonHandler¶
-
BlockDialog.
AddEnableOKButtonHandler
¶ Adds enable-ok-button callback handler to the dialog.
Signature
AddEnableOKButtonHandler(cb)
Parameters: cb (CallableObject) – New in version NX7.5.3.
License requirements: None.
AddFilterHandler¶
-
BlockDialog.
AddFilterHandler
¶ Adds Filter callback handler to the dialog.
Signature
AddFilterHandler(cb)
Parameters: cb (CallableObject) – New in version NX6.0.0.
License requirements: None.
AddFocusNotifyHandler¶
-
BlockDialog.
AddFocusNotifyHandler
¶ Adds focus notify callback handler to the dialog.
Signature
AddFocusNotifyHandler(cb)
Parameters: cb (CallableObject) – New in version NX6.0.2.
License requirements: None.
AddInitializeHandler¶
-
BlockDialog.
AddInitializeHandler
¶ Adds Initialize callback handler to the dialog.
The callback function is called while the dialog is being initialized. The callback is called before applying any user inputs saved in dialog memory.
Signature
AddInitializeHandler(cb)
Parameters: cb (CallableObject) – New in version NX6.0.0.
License requirements: None.
AddKeyboardFocusNotifyHandler¶
-
BlockDialog.
AddKeyboardFocusNotifyHandler
¶ Adds keyboard focus notify callback handler to the dialog.
Signature
AddKeyboardFocusNotifyHandler(cb)
Parameters: cb (CallableObject) – New in version NX7.5.0.
License requirements: None.
AddOkHandler¶
-
BlockDialog.
AddOkHandler
¶ Adds Ok callback handler to the dialog.
Signature
AddOkHandler(okCb)
Parameters: okCb (CallableObject) – New in version NX6.0.0.
License requirements: None.
AddUpdateHandler¶
-
BlockDialog.
AddUpdateHandler
¶ Adds Update callback handler to the dialog.
Signature
AddUpdateHandler(cb)
Parameters: cb (CallableObject) – New in version NX6.0.0.
License requirements: None.
Dispose¶
-
BlockDialog.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.0.
License requirements: None.
GetBlockProperties¶
-
BlockDialog.
GetBlockProperties
¶ Gets the properties of a block
Signature
GetBlockProperties(blockName)
Parameters: blockName (str) – BlockID of the block Returns: Return type: NXOpen.BlockStyler.PropertyList
New in version NX8.5.0.
License requirements: None.
PerformApply¶
-
BlockDialog.
PerformApply
¶ Performs an Apply and restarts the dialog.
This invokes the apply callback on the dialog. This method is meant to be called when the dialog is shown and while inside the update callback.
Signature
PerformApply()
New in version NX6.0.0.
License requirements: None.
RegisterUserDefinedUIBlock¶
-
BlockDialog.
RegisterUserDefinedUIBlock
¶ Registers the reusable block with the dialog
Signature
RegisterUserDefinedUIBlock(blockDialog, blockId)
Parameters: - blockDialog (
NXOpen.BlockStyler.BlockDialog
) – Dialog which contains the reusable block - blockId (str) – “Block ID” of reusable block
New in version NX8.0.0.
License requirements: None.
- blockDialog (
Show¶
-
BlockDialog.
Show
¶ Overloaded method Show
Show()
Show(dialogMode)
-------------------------------------
Shows the dialog in
BlockStyler.BlockDialogDialogMode.Create
mode. This method will not return until the dialog is closed, which typically is when the dialog’s OK or Cancel button is pressed.Signature
Show()
Returns: Return type: NXOpen.SelectionResponse
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Shows the dialog based upon the mode specified in
BlockStyler.BlockDialogDialogMode
. This method will not return until the dialog is closed, which typically is when the dialog’s OK or Cancel button is pressed.Signature
Show(dialogMode)
Parameters: dialogMode ( NXOpen.BlockStyler.BlockDialogDialogMode
) – Dialog mode as Create or Edit.BlockStyler.BlockDialogDialogMode
Returns: Return type: NXOpen.SelectionResponse
New in version NX6.0.0.
License requirements: None.
-------------------------------------