SelectionResponse Enumeration¶
NXOpen.Selection.Response is an alias for NXOpen.SelectionResponse
-
class
NXOpen.
SelectionResponse
¶ Bases:
object
Specify the user response for the selection operation.
Enum Members
Enum Member Enum Member Description Back User selected Back Cancel User selected Cancel Ok User selected Ok ObjectSelectedByName User selected object by name ObjectSelected User selected an object -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-