BaseRadialDimensionBuilder Class¶
-
class
NXOpen.Annotations.
BaseRadialDimensionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Annotations.Dimension
builderThis is an abstract class and cannot be instantiated.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AppendedText | Returns the appended text |
DiameterDimensionDimLineAngle | Returns or sets the diameter dimension’s dimension-line-angle |
FirstAssociativity | Returns the first associativity. |
FoldLocation | Returns the fold location |
Inherit | Returns the inherit |
IsFoldedRadius | Returns or sets the is folded radius |
IsHoleStyle | Returns or sets the is hole style dimension |
IsRadiusToCenter | Returns or sets the is radius to center |
Measurement | Returns the measurement |
OffsetCenterPoint | Returns the offset center point |
Origin | Returns the origin |
Style | Returns the style |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AppendedText¶
-
BaseRadialDimensionBuilder.
AppendedText
¶ Returns the appended text
-------------------------------------
Getter Method
Signature
AppendedText
Returns: Return type: NXOpen.Annotations.AppendedTextBuilder
New in version NX9.0.0.
License requirements: None.
DiameterDimensionDimLineAngle¶
-
BaseRadialDimensionBuilder.
DiameterDimensionDimLineAngle
¶ Returns or sets the diameter dimension’s dimension-line-angle
-------------------------------------
Getter Method
Signature
DiameterDimensionDimLineAngle
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiameterDimensionDimLineAngle
Parameters: dimLineAngle (float) – New in version NX11.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstAssociativity¶
-
BaseRadialDimensionBuilder.
FirstAssociativity
¶ Returns the first associativity.
Supported object types include Feature and DisplayableObject.
-------------------------------------
Getter Method
Signature
FirstAssociativity
Returns: Return type: NXOpen.SelectNXObject
New in version NX9.0.0.
License requirements: None.
FoldLocation¶
-
BaseRadialDimensionBuilder.
FoldLocation
¶ Returns the fold location
-------------------------------------
Getter Method
Signature
FoldLocation
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX9.0.0.
License requirements: None.
Inherit¶
-
BaseRadialDimensionBuilder.
Inherit
¶ Returns the inherit
-------------------------------------
Getter Method
Signature
Inherit
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX9.0.0.
License requirements: None.
IsFoldedRadius¶
-
BaseRadialDimensionBuilder.
IsFoldedRadius
¶ Returns or sets the is folded radius
-------------------------------------
Getter Method
Signature
IsFoldedRadius
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsFoldedRadius
Parameters: isFoldedRadius (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
IsHoleStyle¶
-
BaseRadialDimensionBuilder.
IsHoleStyle
¶ Returns or sets the is hole style dimension
-------------------------------------
Getter Method
Signature
IsHoleStyle
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsHoleStyle
Parameters: isArrowsOutDia (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
IsRadiusToCenter¶
-
BaseRadialDimensionBuilder.
IsRadiusToCenter
¶ Returns or sets the is radius to center
-------------------------------------
Getter Method
Signature
IsRadiusToCenter
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsRadiusToCenter
Parameters: isRadiusToCenter (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Measurement¶
-
BaseRadialDimensionBuilder.
Measurement
¶ Returns the measurement
-------------------------------------
Getter Method
Signature
Measurement
Returns: Return type: NXOpen.Annotations.DimensionMeasurementBuilder
New in version NX9.0.0.
License requirements: None.
OffsetCenterPoint¶
-
BaseRadialDimensionBuilder.
OffsetCenterPoint
¶ Returns the offset center point
-------------------------------------
Getter Method
Signature
OffsetCenterPoint
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX9.0.0.
License requirements: None.
Origin¶
-
BaseRadialDimensionBuilder.
Origin
¶ Returns the origin
-------------------------------------
Getter Method
Signature
Origin
Returns: Return type: NXOpen.Annotations.OriginBuilder
New in version NX9.0.0.
License requirements: None.
Style¶
-
BaseRadialDimensionBuilder.
Style
¶ Returns the style
-------------------------------------
Getter Method
Signature
Style
Returns: Return type: NXOpen.Annotations.StyleBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
BaseRadialDimensionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.