AppendedTextBuilder Class¶
-
class
NXOpen.Annotations.
AppendedTextBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class is used to set/access the appended text of a dimension
This is a sub-builder class and cannot be directly instantiated
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
UserDefinedSymbolAspectRatio | Returns or sets the aspect ratio for user defined symbol |
UserDefinedSymbolHeight | Returns or sets the height for user defined symbol |
UserDefinedSymbolLength | Returns or sets the length for user defined symbol |
UserDefinedSymbolScale | Returns or sets the scale for user defined symbol |
Methods¶
Method | Description |
---|---|
GetAbove | Gets the appended text above the annotation |
GetAfter | Gets the appended text after the annotation |
GetBefore | Gets the appended text before the annotation |
GetBelow | Gets the appended text below the annotation |
SetAbove | Sets the appended text above the annotation |
SetAfter | Sets the appended text after the annotation |
SetBefore | Sets the appended text before the annotation |
SetBelow | Sets the appended text below the annotation |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
UserDefinedSymbolAspectRatio¶
-
AppendedTextBuilder.
UserDefinedSymbolAspectRatio
¶ Returns or sets the aspect ratio for user defined symbol
-------------------------------------
Getter Method
Signature
UserDefinedSymbolAspectRatio
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserDefinedSymbolAspectRatio
Parameters: aspectRatio (float) – New in version NX11.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
UserDefinedSymbolHeight¶
-
AppendedTextBuilder.
UserDefinedSymbolHeight
¶ Returns or sets the height for user defined symbol
-------------------------------------
Getter Method
Signature
UserDefinedSymbolHeight
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserDefinedSymbolHeight
Parameters: height (float) – New in version NX11.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
UserDefinedSymbolLength¶
-
AppendedTextBuilder.
UserDefinedSymbolLength
¶ Returns or sets the length for user defined symbol
-------------------------------------
Getter Method
Signature
UserDefinedSymbolLength
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserDefinedSymbolLength
Parameters: length (float) – New in version NX11.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
UserDefinedSymbolScale¶
-
AppendedTextBuilder.
UserDefinedSymbolScale
¶ Returns or sets the scale for user defined symbol
-------------------------------------
Getter Method
Signature
UserDefinedSymbolScale
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserDefinedSymbolScale
Parameters: scale (float) – New in version NX11.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Method Detail¶
GetAbove¶
-
AppendedTextBuilder.
GetAbove
¶ Gets the appended text above the annotation
Signature
GetAbove()
Returns: List of lines Return type: list of str New in version NX9.0.0.
License requirements: None.
GetAfter¶
-
AppendedTextBuilder.
GetAfter
¶ Gets the appended text after the annotation
Signature
GetAfter()
Returns: List of lines Return type: list of str New in version NX9.0.0.
License requirements: None.
GetBefore¶
-
AppendedTextBuilder.
GetBefore
¶ Gets the appended text before the annotation
Signature
GetBefore()
Returns: List of lines Return type: list of str New in version NX9.0.0.
License requirements: None.
GetBelow¶
-
AppendedTextBuilder.
GetBelow
¶ Gets the appended text below the annotation
Signature
GetBelow()
Returns: List of lines Return type: list of str New in version NX9.0.0.
License requirements: None.
SetAbove¶
-
AppendedTextBuilder.
SetAbove
¶ Sets the appended text above the annotation
Signature
SetAbove(lines)
Parameters: lines (list of str) – List of new lines New in version NX9.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
SetAfter¶
-
AppendedTextBuilder.
SetAfter
¶ Sets the appended text after the annotation
Signature
SetAfter(lines)
Parameters: lines (list of str) – List of new lines New in version NX9.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
SetBefore¶
-
AppendedTextBuilder.
SetBefore
¶ Sets the appended text before the annotation
Signature
SetBefore(lines)
Parameters: lines (list of str) – List of new lines New in version NX9.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
SetBelow¶
-
AppendedTextBuilder.
SetBelow
¶ Sets the appended text below the annotation
Signature
SetBelow(lines)
Parameters: lines (list of str) – List of new lines New in version NX9.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Validate¶
-
AppendedTextBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.