SelectionBaseDefinitionBuilder Class¶
-
class
NXOpen.AME.
SelectionBaseDefinitionBuilder
¶ Bases:
NXOpen.TaggedObject
Journalling Interface class for Builder which allows selection of BaseDefinition.
This object does not need a creator.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
ReuseLibraryItem | Returns the builder for reuse library selection item |
SelectBaseDefinitionNode | Returns the builder for selected base definition node |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetSelectedBaseDefinition | Gets selected base definition |
SetSelectedBaseDefinition | Sets the selected base definition |
Property Detail¶
ReuseLibraryItem¶
-
SelectionBaseDefinitionBuilder.
ReuseLibraryItem
¶ Returns the builder for reuse library selection item
-------------------------------------
Getter Method
Signature
ReuseLibraryItem
Returns: Return type: NXOpen.AME.InstantiateBaseDefinitionReuseSelectionBuilder
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SelectBaseDefinitionNode¶
-
SelectionBaseDefinitionBuilder.
SelectBaseDefinitionNode
¶ Returns the builder for selected base definition node
-------------------------------------
Getter Method
Signature
SelectBaseDefinitionNode
Returns: Return type: NXOpen.AME.SelectBaseDefinitionNodeBuilder
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
GetSelectedBaseDefinition¶
-
SelectionBaseDefinitionBuilder.
GetSelectedBaseDefinition
¶ Gets selected base definition
Signature
GetSelectedBaseDefinition()
Returns: Return type: NXOpen.NXObject
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetSelectedBaseDefinition¶
-
SelectionBaseDefinitionBuilder.
SetSelectedBaseDefinition
¶ Sets the selected base definition
Signature
SetSelectedBaseDefinition(baseDefinition)
Parameters: baseDefinition ( NXOpen.NXObject
) –New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)