InstantiateBaseDefinitionReuseSelectionBuilder Class¶
-
class
NXOpen.AME.
InstantiateBaseDefinitionReuseSelectionBuilder
¶ Bases:
NXOpen.Builder
Builder for selecting base definition
this is a block
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
ReuseLibraryItem | Returns the reuse library item selection |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetSelection | Sets the selection item |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ReuseLibraryItem¶
-
InstantiateBaseDefinitionReuseSelectionBuilder.
ReuseLibraryItem
¶ Returns the reuse library item selection
-------------------------------------
Getter Method
Signature
ReuseLibraryItem
Returns: Return type: NXOpen.Tooling.SelectReuseLibraryItemBuilder
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
SetSelection¶
-
InstantiateBaseDefinitionReuseSelectionBuilder.
SetSelection
¶ Sets the selection item
Signature
SetSelection(path)
Parameters: path (str) – the path of a part New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Validate¶
-
InstantiateBaseDefinitionReuseSelectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.