EngineeringObjectBuilder Class¶
-
class
NXOpen.AME.
EngineeringObjectBuilder
¶ Bases:
NXOpen.AME.EngineeringObjectBaseBuilder
JA class for the insert Eng object dialog
To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateEngineeringObjectBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
CreatedEo | Returns the created eo |
ProjectEngObject | Returns the project eo ui block |
ReuseLibraryItem | Returns the selection base definition builder |
SelectionBaseDefinition | Returns the selection base definition builder |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedAspects | Get the commited Aspect |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetNewObjects | Get the commited Aspect |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CreatedEo¶
-
EngineeringObjectBuilder.
CreatedEo
¶ Returns the created eo
-------------------------------------
Getter Method
Signature
CreatedEo
Returns: Return type: NXOpen.NXObject
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ProjectEngObject¶
-
EngineeringObjectBuilder.
ProjectEngObject
¶ Returns the project eo ui block
-------------------------------------
Getter Method
Signature
ProjectEngObject
Returns: Return type: NXOpen.AME.ProjectEngineeringObjectBuilder
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ReuseLibraryItem¶
-
EngineeringObjectBuilder.
ReuseLibraryItem
¶ Returns the selection base definition builder
-------------------------------------
Getter Method
Signature
ReuseLibraryItem
Returns: Return type: NXOpen.Tooling.SelectReuseLibraryItemBuilder
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SelectionBaseDefinition¶
-
EngineeringObjectBuilder.
SelectionBaseDefinition
¶ Returns the selection base definition builder
-------------------------------------
Getter Method
Signature
SelectionBaseDefinition
Returns: Return type: NXOpen.AME.SelectionBaseDefinitionBuilder
New in version NX12.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
Method Detail¶
Validate¶
-
EngineeringObjectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.