ElectricalConnectionSettingsBuilder Class¶
-
class
NXOpen.AME.
ElectricalConnectionSettingsBuilder
¶ Bases:
NXOpen.Builder
Builder object for changing electrical connection settings on diagramming pages associated with the
NXOpen.AME.Project
.To create a new instance of this class, use
NXOpen.AME.AMEManager.CreateElectricalConnectionSettingsBuilder()
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetStyleColorCode | Style color code property of a given electrical connection sub-type. |
GetStyleFont | Style font property of a given electrical connection sub-type. |
GetStyleWidth | Style width property of a given electrical connection sub-type. |
GetWireColorCode | Wire color code property of a given electrical connection sub-type. |
GetWireCrossSection | Wire cross section property of a given electrical connection sub-type. |
GetWireType | Wire type property of a given electrical connection sub-type. |
ResetToDefault | Resets electrical connection settings to default |
SetStyleColorCode | |
SetStyleFont | |
SetStyleWidth | |
SetWireColorCode | |
SetWireCrossSection | |
SetWireType | |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetStyleColorCode¶
-
ElectricalConnectionSettingsBuilder.
GetStyleColorCode
¶ Style color code property of a given electrical connection sub-type.
Signature
GetStyleColorCode(potentialType)
Parameters: potentialType ( NXOpen.AME.AmeElectricalConnectionPotentialType
) –Returns: Return type: Id New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
GetStyleFont¶
-
ElectricalConnectionSettingsBuilder.
GetStyleFont
¶ Style font property of a given electrical connection sub-type.
Signature
GetStyleFont(potentialType)
Parameters: potentialType ( NXOpen.AME.AmeElectricalConnectionPotentialType
) –Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
GetStyleWidth¶
-
ElectricalConnectionSettingsBuilder.
GetStyleWidth
¶ Style width property of a given electrical connection sub-type.
Signature
GetStyleWidth(potentialType)
Parameters: potentialType ( NXOpen.AME.AmeElectricalConnectionPotentialType
) –Returns: Return type: NXOpen.DisplayableObjectObjectWidth
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
GetWireColorCode¶
-
ElectricalConnectionSettingsBuilder.
GetWireColorCode
¶ Wire color code property of a given electrical connection sub-type.
Signature
GetWireColorCode(potentialType)
Parameters: potentialType ( NXOpen.AME.AmeElectricalConnectionPotentialType
) –Returns: Caller needs to free this memory. Return type: str New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
GetWireCrossSection¶
-
ElectricalConnectionSettingsBuilder.
GetWireCrossSection
¶ Wire cross section property of a given electrical connection sub-type.
Signature
GetWireCrossSection(potentialType)
Parameters: potentialType ( NXOpen.AME.AmeElectricalConnectionPotentialType
) –Returns: Return type: float New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
GetWireType¶
-
ElectricalConnectionSettingsBuilder.
GetWireType
¶ Wire type property of a given electrical connection sub-type.
Signature
GetWireType(potentialType)
Parameters: potentialType ( NXOpen.AME.AmeElectricalConnectionPotentialType
) –Returns: Caller needs to free this memory. Return type: str New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
ResetToDefault¶
-
ElectricalConnectionSettingsBuilder.
ResetToDefault
¶ Resets electrical connection settings to default
Signature
ResetToDefault()
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
SetStyleColorCode¶
-
ElectricalConnectionSettingsBuilder.
SetStyleColorCode
¶ Signature
SetStyleColorCode(potentialType, styleColorCode)
Parameters: - potentialType (
NXOpen.AME.AmeElectricalConnectionPotentialType
) – - styleColorCode (Id) –
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
- potentialType (
SetStyleFont¶
-
ElectricalConnectionSettingsBuilder.
SetStyleFont
¶ Signature
SetStyleFont(potentialType, styleFont)
Parameters: - potentialType (
NXOpen.AME.AmeElectricalConnectionPotentialType
) – - styleFont (
NXOpen.DisplayableObjectObjectFont
) –
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
- potentialType (
SetStyleWidth¶
-
ElectricalConnectionSettingsBuilder.
SetStyleWidth
¶ Signature
SetStyleWidth(potentialType, styleWidth)
Parameters: - potentialType (
NXOpen.AME.AmeElectricalConnectionPotentialType
) – - styleWidth (
NXOpen.DisplayableObjectObjectWidth
) –
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
- potentialType (
SetWireColorCode¶
-
ElectricalConnectionSettingsBuilder.
SetWireColorCode
¶ Signature
SetWireColorCode(potentialType, wireColorCode)
Parameters: - potentialType (
NXOpen.AME.AmeElectricalConnectionPotentialType
) – - wireColorCode (str) –
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
- potentialType (
SetWireCrossSection¶
-
ElectricalConnectionSettingsBuilder.
SetWireCrossSection
¶ Signature
SetWireCrossSection(potentialType, wireCrossSection)
Parameters: - potentialType (
NXOpen.AME.AmeElectricalConnectionPotentialType
) – - wireCrossSection (float) –
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
- potentialType (
SetWireType¶
-
ElectricalConnectionSettingsBuilder.
SetWireType
¶ Signature
SetWireType(potentialType, wireType)
Parameters: - potentialType (
NXOpen.AME.AmeElectricalConnectionPotentialType
) – - wireType (str) –
New in version NX11.0.0.
License requirements: ad_automation_design (“FULL AUTOMATION DESIGNER”)
- potentialType (
Validate¶
-
ElectricalConnectionSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.