GRIP Introduction | Point and Curve Creation Statement List
This topic covers the GRIP statements used to create point and curve objects. Also included is a statement which allows you to trim a curve using bounding objects.
Point and Curve Creation operations fall into the following categories:
If a Modeling Application statement allows you to specify a distance or angle tolerance value and you do not provide one, the default is the value set in the NXoption for Preferences->Modeling. You can read and set these tolerance values using the &DISTOL and &ANGTOL GPAs.
If a Modeling Application statement performs an approximation and that statement does not allow the minor word TOLER, the system uses the tolerance value set in Unigraphics NX.