Point and Curve Creation Overview | Statement List
A CIRCLE is created in a counterclockwise direction from the positive X axis of the work coordinate system. The start and end angles of the arc may be specified in some of the circle definitions. However, if the start and end angles are omitted or are not considered in the definition statement, a full circle is created.