/*
uf_obj.h
File description:
The routines in this chapter enable you to:
. get the version of the part in which the given object was created and
the version in which it was last modified.
. get the highlight status of an object.
. return the objects status.
. return a logical value indicating whether or not the object type is
capable of having a matrix pointer which can be read with
UF_CSYS_ask_matrix_of_object
. return all objects in a given part on all layers regardless of
their current status or displayability.
. return all objects in the part of all types on all layers regardless
of their current state of displayability.
. return a logical indicating whether the object is displayable,
and therefore possessing color, width, font, and layer.
. modify current default parameters for color, work layer,
line width, line font.
. temporarily modify current default parameters for color, work layer,
line width, line font and saves your previous default settings
in a temporary memory buffer.
This chapter provides access to specific color, line font, and width
object creation settings for specific object type and subtype combinations.
The routines provide functionality to ask/set the object creation color,
line font and width of a specific object type. Access to these settings is
provided by:
UF_OBJ_ask_cre_settings
UF_OBJ_set_cre_color
UF_OBJ_set_cre_line_font
UF_OBJ_set_cre_width
The routines provide functionality to ask/set the default object creation
color, line font and width. The default object creation settings apply to
all types without specific object settings. Access to the default object
creation settings is provided by:
UF_OBJ_ask_def_cre_settings
UF_OBJ_set_def_cre_color
UF_OBJ_set_def_cre_line_font
UF_OBJ_set_def_cre_width
Object types with specific object creation settings can use the default
settings by using the following routines:
UF_OBJ_is_def_cre_color
UF_OBJ_is_def_cre_line_font
UF_OBJ_is_def_cre_width
UF_OBJ_set_cre_color_to_def
UF_OBJ_set_cre_line_font_to_def
UF_OBJ_set_cre_width_to_def
For information on type, subtype and properties click here.
*******************************************************************************/
#ifndef UF_OBJ_INCLUDED
#define UF_OBJ_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_cfi_types.h>
#include <uf_obj_types.h>
#include <uf_retiring.h>
#include <libufun_exports.h>
/******************************************************************************
Returns all objects in a given part on all layers regardless of their
current status or displayability. This includes temporary (system created) objects.
It does not return expressions.
This function returns the tag of the object that was found. To continue
cycling, pass the returned object in as the second argument to this
function.
NOTE: You are strongly advised to avoid doing anything to non-alive
objects unless you are familiar with their use. NX may delete or reuse
these objects at any time. Some of these objects do not get filed with
the part.
NOTE: This routine is invalid for partially loaded parts. If you call this
function using a partially loaded part, it returns a NULL_TAG from
the beginning of the cycle.
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
Return:
This function returns the object identifier of the next object.
The cycle is completed when a NULL_TAG is returned
Environment: Internal and External
See Also:
Please refer to the usage and the
example
History:
******************************************************************************/
extern UFUNEXPORT tag_t UF_OBJ_cycle_all(
tag_t part_tag ,/* <I>
Tag of part you wish to cycle
*/
tag_t object /* <I>
Begin the cycle by passing in object = NULL_TAG
*/
);/* */
/*******************************************************************************
Returns all objects in the part of the specified types on all layers (including
layers not writable or viewable) regardless of their current state of displayability.
This routine does not return expressions, condemned objects, temporary (system created)
objects, or sleepy objects. An object that is asleep is one that has been removed from
the model. For example, if you blend an edge, then the edge is asleep. The WCS will not
be returned unless it has been saved.
NOTE: This routine cycles the features in a part when the type
specified is UF_feature_type.
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
Environment: Internal and External
See Also:
For example please refer to the example
History:
******************************************************************************/
extern UFUNEXPORT int UF_OBJ_cycle_objs_in_part(
tag_t part_tag ,/* <I>
Tag of part you wish to cycle
*/
int type ,/* <I>
Type of object on which to cycle
*/
tag_t * object /* <I/O>
On input the object found by the last call to this routine. if
this routine has not been called yet, then set object=NULL_TAG
to start cycling. On output the next object of the type
specified. If there is no object, and the cycling is complete
a NULL_TAG is returned.
*/
);
/*******************************************************************************
Returns all objects in the part of the specified types that are found on layers
1 thru 256 regardless of their current state of displayability. This routine does not
return expressions, condemned objects, temporary (system created) objects, or sleepy objects. An object that is asleep is one that has been removed from the model.
For example, if you blend an edge, then the edge is asleep. The WCS will not
be returned unless it has been saved.
NOTE: This routine cycles the features in a part when the type
specified is UF_feature_type.
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
Environment: Internal and External
See Also:
For example please refer to the example
History: NX10.0.0
******************************************************************************/
extern UFUNEXPORT int UF_OBJ_cycle_objs_in_part1(
tag_t part_tag ,/* <I>
Tag of part you wish to cycle
*/
int type ,/* <I>
Type of object on which to cycle
*/
tag_t * object /* <I/O>
On input the object found by the last call to this routine. if
this routine has not been called yet, then set object=NULL_TAG
to start cycling. On output the next object of the type
specified. If there is no object, and the cycling is complete
a NULL_TAG is returned.
*/
);
/*******************************************************************************
This routine has been added to deal with extended object types (extended object types have
values over 256).
Returns all objects in the part of the specified types on all layers
regardless of their current state of displayability. This routine does not
return expressions, condemned objects, temporary (system created) objects, or sleepy objects.
An object that is asleep is one that has been removed from the model.
For example, if you blend an edge, then the edge is asleep. The WCS will not
be returned unless it has been saved.
Although this works like UF_OBJ_cycle_objs_in_part, there is a difference.
When type is UF_extended_type, this routine (UF_OBJ_cycle_typed_objs_in_part) will not returns any objects.
Whereas UF_OBJ_cycle_objs_in_part will return all the objects with extended entity types for type UF_extended_type.
For more details on how UF_OBJ_cycle_objs_in_part works, please see comment for UF_OBJ_cycle_objs_in_part
NOTE: This routine cycles the features in a part when the type
specified is UF_feature_type.
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
See Also:
UF_OBJ_cycle_objs_in_part
History:
******************************************************************************/
extern UFUNEXPORT int UF_OBJ_cycle_typed_objs_in_part(
tag_t part_tag ,/* <I>
Tag of part you wish to cycle
*/
int type ,/* <I>
Type of object on which to cycle
*/
tag_t * object /* <I/O>
On input the object found by the last call to this routine. if
this routine has not been called yet, then set object=NULL_TAG
to start cycling. On output the next object of the type
specified. If there is no object, and the cycling is complete
a NULL_TAG is returned.
*/
);
/*******************************************************************************
Cycle the objects of a given name in current work part. Note that the name of
an object of type UF_occ_instance_type is not necessarily the instance name.
Note that the name must match exactly. If the name of an object is "abc ", and
the name passed here is "abc", then the object will not be found because of
the trailing space.
When using UF_OBJ_cycle_by_name, features are only returned if they are the only
object with that name. If there is any possibility that there could be objects
with the same name (that are not features), then call UF_OBJ_cycle_by_by_name_and_type
using UF_feature_type in order to find the named features.
Please refer to the example
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_OBJ_cycle_by_name(
const char * name ,/* <I>
Name of objects on which to cycle
*/
tag_t * object /* <I/O>
On input the object found by the last call to this routine.
Begin the cycle by passing in object = NULL_TAG
On output, the next object of the given name. Outputs a
NULL_TAG when the cycle is finished.
*/
);
/******************************************************************************
Returns the objects status, UF_OBJ_DELETED, UF_OBJ_TEMPORARY, UF_OBJ_CONDEMNED,
and UF_OBJ_ALIVE. This function should only be used to get information on objects
within the part, not the part itself.
NOTE: You are strongly advised to avoid doing anything to non-alive
objects unless you are familiar with their use. NX may delete or reuse
these objects at any time. Some of these objects do not get filed with
the part.
Return:
Returns 1 of 4 statuses
UF_OBJ_DELETED
UF_OBJ_TEMPORARY
UF_OBJ_CONDEMNED
UF_OBJ_ALIVE
Environment: Internal and External
See Also:
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_ask_status(
tag_t object /* <I>
The object for which you are asking status
*/
);/**/
/*****************************************************************************
Returns a logical indicating whether tagged NX object is displayable,
and therefore possesses attributes of color, width, font, and layer.
Although an object possesses these displayable attributes, it
does not mean that the object is ever actually displayed in the graphics
window in an interactive NX session. Some objects possess
these characteristics for purposes internal to NX.
Return:
Returns a logical which indicates whether object is
displayable
Environment: Internal and External
See Also:
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_is_displayable(
tag_t object_id, /* <I>
Object identifier of object to query
*/
logical *is_displayable /* <O>
TRUE = This object is displayable
FALSE = This object is not displayable
*/
);
/*****************************************************************************
Determines whether the given tagged NX object is a transferable or not.
You can potentially export a transferable object using
UF_PART_export or UF_PART_export_with_options, or transfer to a
new component using UF_ASSEM_create_component_part.
Although a particular object may return as being transferable, there is
no guarantee that the objects of that type will be transferred. For
example, if an object of a transferable type depends upon an object
which is not transferable, then the original object will not be transferred.
Environment: Internal and External
See Also:
UF_PART_export
UF_PART_export_with_options
UF_ASSEM_create_component_part
Please refer to the example
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_is_transferable(
tag_t object_id, /* <I>
Object identifier of object to query
*/
logical *is_transferable /* <O>
TRUE = This object is transferable
FALSE = This object is not transferable
*/
);
/******************************************************************************
Returns the object type and subtype of a tagged NX object.
The majority of these objects are listed in the uf_object_types.h
header file.
In addition to the objects listed in uf_object_types.h, there are other
NX objects uniquely identified by a tag. Among these objects
are expressions and parts. These objects, which are not listed in the
uf_object_types.h header file, produce the type UF_OBJ_EXPR_TYPE and
UF_OBJ_PART_TYPE with a subtype of 0.
The types and subtypes this function returns for expressions
and parts are not useful in any other Open API routines.
These types are provided only to allow you to determine the class of a
NX object through its identifier (i.e. its tag) which can assist
you in determining the other Open API routines that you can use
in conjunction with the object. For a more detailed discussion of
classes of objects and the Open API routines available to these
objects, please see the Open API Programmer's Guide, "The
NX Object Model".
Environment: Internal and External
See Also:
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_ask_type_and_subtype(
tag_t object_id ,/* <I>
Object identifier of object to query
*/
int * type ,/* <O>
Type of object
*/
int * subtype /* <O>
Subtype of object
*/
);
/******************************************************************************
Returns the extended object type of a tagged NX object. (extended object types have
values over 256). The majority of these objects are listed in the uf_object_types.h
header file.
In addition to the objects listed in uf_object_types.h, there are other
NX objects uniquely identified by a tag. Among these objects
are expressions and parts. These objects, which are not listed in the
uf_object_types.h header file, produce the type UF_OBJ_EXPR_TYPE and
UF_OBJ_PART_TYPE with a subtype of 0.
The types and subtypes this function returns for expressions
and parts are not useful in any other Open API routines.
These types are provided only to allow you to determine the class of a
NX object through its identifier (i.e. its tag) which can assist
you in determining the other Open API routines that you can use
in conjunction with the object. For a more detailed discussion of
classes of objects and the Open API routines available to these
objects, please see the Open API Programmer's Guide, "The
NX Object Model".
The difference between the type returned by UF_OBJ_ask_type_and_subtype and this routine is,
UF_OBJ_ask_type_and_subtype returns UF_extended_type or UF_extended_displayable_type for
all the extended type objects except for some types like parts and expressions.
Whereas this routine returns the object's real type.
Environment: Internal and External
See Also:
UF_OBJ_ask_type_and_subtype
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_ask_extended_type_and_subtype(
tag_t object_id ,/* <I>
Object identifier of object to query
*/
int * type ,/* <O>
Type of object
*/
int * subtype /* <O>
Subtype of object
*/
);
/******************************************************************************
Finds the name of the specified object. If the object you query is not of an
object type listed in uf_object_types.h or if the object has no name, an
error code returns and name is set to the empty string, "". Note that the
name output for an object of type UF_occ_instance_type is not necessarily the
instance name; the instance name can be accessed using
UF_ASSEM_ask_component_data.
Environment: Internal and External
See Also:
History:
******************************************************************************/
/* */
extern UFUNEXPORT int UF_OBJ_ask_name(
tag_t object_id ,/* <I>
Object identifier of object to inquire upon.
*/
char *name /* <O>
Name of object
*/
);
/******************************************************************************
Sets the name of a object. You can only set the name of an object which has
an object type defined in the uf_object_types.h header file. Note that the
name set for an object of type UF_occ_instance_type is not the instance name;
the instance name can be set using UF_ASSEM_rename_instance.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_name (
tag_t object_id ,/* <I>
Object identifier of object whose name is to be set.
*/
const char * name /* <I>
Name to assign to object. The length of the name is
limited to UF_OBJ_NAME_LEN characters.
*/
);
/******************************************************************************
Sets the origin of an object name. This origin is only used as the location
to display the name when name display is enabled with
UF_DISP_set_name_display_status. This routine will return an error if the
object is not named.
Environment: Internal and External
See Also:
UF_DISP_set_name_display_status
UF_OBJ_ask_name_origin
History: Originally released in V17.0
******************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_name_origin(
tag_t object_id ,/* <I>
Object identifier of object whose name origin is to be set.
*/
double origin[3] /* <I>
Origin in absolute coordinates where the name is to be
displayed
*/
);
/******************************************************************************
Returns the name origin of the specified object. If the object you query is
not of an object type listed in uf_object_types.h or if the object has no name,
an error code returns and the origin is set to (0,0,0).
Environment: Internal and External
See Also:
UF_OBJ_set_name_origin
History: Originally released in V17.0
******************************************************************************/
extern UFUNEXPORT int UF_OBJ_ask_name_origin(
tag_t object_id ,/* <I>
Object identifier of object to inquire upon.
*/
double origin[3] /* <O>
Origin in absolute coordinates where the name of the
object will be displayed.
*/
);
/******************************************************************************
Deletes the name from the specified object. Only objects with an object
type listed in uf_object_types.h can have their names deleted.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUNEXPORT int UF_OBJ_delete_name(
tag_t object_id /* <I>
Object identifier of object whose name is to be
deleted.
*/
);
/******************************************************************************
Returns the display properties (layer, color, blank status, line width,
and font) for an object.
Environment: Internal and External
See Also:
For structure see UF_OBJ_disp_props_t
History:
******************************************************************************/
extern UFUNEXPORT int UF_OBJ_ask_display_properties (
tag_t object_id ,/* <I>
Object identifier of object to query
*/
UF_OBJ_disp_props_p_t disp_props /* <O>
Display properties of object of inquiry
*/
);
/******************************************************************************
Modifies the layer of an object. Use UF_OBJ_ask_display_properties to
determine the object's current layer.
If you attempt to change the layer of an object which is on a
reserved layer (greater than UF_LAYER_MAX_LAYER, or zero), the request
will be ignored.
If you attempt to change the layer of an object which is on a user-accessible
layer (UF_LAYER_MIN_LAYER <= layer <= UF_LAYER_MAX_LAYER) to a reserved layer,
the request will be ignored, except that objects of type RM_view_type
and RM_cs2_vertex_type may be moved to layer 0, which is where these
object types belong, so that parts where these object types were erroneously
moved off of layer 0 may be repaired.
Environment: Internal and External
See Also:
UF_OBJ_set_layer_allow_hidden
UF_OBJ_ask_display_properties
History: In V18.0 attempts to move change the layer of objects on
reserved layers will be ignored.
******************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_layer(
tag_t object_id ,/* <I>
Object identifier of object whose layer is to be
changed.
*/
int layer /* <I>
layer to assign.
*/
);
/******************************************************************************
Modifies the color of an object. Use UF_OBJ_ask_display_properties to
determine the object's current color.
Note: There must be a work part present before calling this function.
Environment: Internal and External
See Also:
See the string defined color constants in the types and symbols .
UF_OBJ_ask_display_properties
History:
******************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_color(
tag_t object_id ,/* <I>
Object identifier of object whose color is to be
changed.
*/
int color /* <I>
Color to assign. Must be one of the following values [1-216]
*/
);
/******************************************************************************
Modifies the blank status of an object. Use UF_OBJ_ask_display_properties to
determine the object's current blank status.
If the object is a sketch or a group, all members of the sketch or
group will have their blank status modified. For groups, this includes
all members of any sub-groups.
Environment: Internal and External
See Also:
UF_OBJ_ask_display_properties
History: V18.0 Comments about sketches and groups added
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_blank_status(
tag_t object_id ,/* <I>
Object identifier of object whose blank status is to
be changed.
*/
int blank_status /* <I>
Blank status to assign. Use one of the following
string defined constants:
UF_OBJ_NOT_BLANKED
UF_OBJ_BLANKED
*/
);
/******************************************************************************
Modifies the line_width of an object. Use UF_OBJ_ask_display_properties to
determine the object's current line width.
Environment: Internal and External
See Also:
UF_OBJ_ask_display_properties
See the string defined line-width constants in the types and symbols .
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_line_width(
tag_t object_id ,/* <I>
Object identifier of object whose line_width is to be
changed.
*/
int line_width /* <I>
line_width to assign.
*/
);
/******************************************************************************
Deletes an array of objects. This is considerably faster than deleting the
objects one at a time. This routine should always be used when more than
one object is to be deleted.
Do not attempt to delete objects while cycling the database in a looping
structure. Problems can occur when trying to read the next object and delete
objects in a looping structure. To delete objects, we recommend that you:
Save the objects in an array and then perform the delete function after you
have completed the cycling by calling UF_OBJ_delete_array_of_objects.
A return value of zero does not guarantee that all of the objects were
deleted. To determine if an particular object was deleted, use
UF_OBJ_ask_status. If statuses is NULL, then the return code from this
function will be 0 if the return code from UF_OBJ_delete_object would
have been zero for all the objects. A non-zero status can either mean
that an individual object could not be deleted, or that some other
fatal error occurred. If statuses is not null, then the individual
delete status for each object is returned in the statuses array. The
return code from the function will be non-zero if some more global
failure occurred.
Environment: Internal and External
See Also:
UF_OBJ_delete_object
History: Originally released in V16.0
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_delete_array_of_objects(
int num_objects, /* <I>
The count of the objects in the object_id array.
*/
tag_t object_id[], /* <I>
Array of object identifiers to be deleted.
*/
int **statuses /* <IOF>
This should be the address of pointer. If it is NULL,
then individual status for the delete operation on each
object will not be given. If it is non-NULL, then
an array will be allocated, and the individual status for each
object placed in this array. The status for
individual objects can be:
0 - object was passed on to the delete algorithm
UF_OBJ_object_can_not_be_deleted
UF_OBJ_err_bad_parameter_number_1
This status will be the same as what would have been returned
had the single object been passed to UF_OBJ_delete_object.
A value of 0 does not necessarily mean that the object was
deleted, this can only be determined by calling
UF_OBJ_ask_status. If a non-NULL pointer is passed in,
then the user must free this returned status array by
using UF_free.
*/
);
/******************************************************************************
Deletes an object. A return value of zero does not guarantee that an object is
deleted. To determine if an object is deleted, use UF_OBJ_ask_status.
It is not allowed to delete the current WCS, if you try, an error will be
returned.
Do not attempt to delete objects while cycling the database in a looping
structure. Problems can occur when trying to read the next object and delete
objects in a looping structure. To delete objects, we recommend:
Save the objects in an array and then perform the delete function using
UF_OBJ_delete_array_of_objects after you have completed the cycling.
If you have multiple objects to delete, you should use the routine
UF_OBJECT_delete_array_of_objects, as it will be much faster.
Note: If a type-specific function exists for the type of object being
deleted, please use that type-specific function instead of this general
use function. For example, to delete a view use UF_VIEW_delete, to
delete a drawing use UF_DRAW_delete_drawing, etc.
Environment: Internal and External
See Also:
UF_OBJ_ask_status
UF_OBJ_delete_array_of_objects
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_delete_object(
tag_t object_id /* <I>
Object identifier of object to delete
*/
);
/******************************************************************************
Modifies the font of an object. Use UF_OBJ_ask_display_properties to
determine the object's current font.
Environment: Internal and External
See Also:
UF_OBJ_ask_display_properties
See the string defined font constants in in the types and symbols
History:
****************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_font(
tag_t object_id ,/* <I>
Object identifier of object whose font is to be
changed.
*/
int font /* <I>
font to assign.
*/
);
/***************************************************************************
Reverses the blank status of all displayable objects on selectable
layers. Uses the work view layer mask.
Environment: Internal and External
See Also:
History:
****************************************************************************/
extern UFUNEXPORT int UF_OBJ_reverse_blank_all( void );
/*****************************************************************************
*
* Color, Line Font and Width Settings
*
*****************************************************************************
*
* Thse functions provide access to specific color, line font, and width
* object creation settings for specific object type and subtype combinations.
* Some of these specific color, line font and width type/subtype/property
* settings may be shared by other type/subtype/property combinations.
*
* The following sets of type/subtype/property combinations share
* specific object creation settings (NOTE: sets are delimited by blank
* lines):
* Type Subtype Property
* ---- ------- -------------------------
* RM_general_object_type UF_all_subtype UF_OBJ_no_property
*
* UF_point_type UF_all_subtype UF_OBJ_no_property
*
* UF_line_type UF_all_subtype UF_OBJ_no_property
*
* UF_circle_type UF_all_subtype UF_OBJ_no_property
*
* UF_conic_type UF_all_subtype UF_OBJ_no_property
*
* UF_spline_type UF_all_subtype UF_OBJ_no_property
*
* UF_coordinate_system_type UF_all_subtype UF_OBJ_no_property
*
* UF_solid_type UF_all_subtype UF_OBJ_solid_body_property
* UF_solid_type UF_all_subtype UF_OBJ_sheet_body_property
*
* UF_plane_type UF_all_subtype UF_OBJ_no_property
* UF_datum_axis_type UF_all_subtype UF_OBJ_no_property
* UF_datum_plane_type UF_all_subtype UF_OBJ_no_property
*
* UF_drafting_entity_type UF_draft_note_subtype UF_OBJ_no_property
* UF_draft_label_subtype
*
* UF_drafting_entity_type UF_draft_id_symbol_subtype UF_OBJ_no_property
*
* UF_drafting_entity_type UF_draft_fpt_subtype UF_OBJ_no_property
*
* UF_drafting_entity_type UF_draft_cntrline_subtype UF_OBJ_no_property
* UF_draft_linear_cntrln_subtype
* UF_draft_full_cir_cntrln_subtype
* UF_draft_part_cir_cntrln_subtype
* UF_draft_full_blt_circle_subtype
* UF_draft_part_blt_circle_subtype
* UF_draft_offset_cntrpt_subtype
* UF_draft_cyl_cntrln_subtype
* UF_draft_sym_cntrln_subtype
*
* UF_drafting_entity_type UF_draft_crosshatch_subtype UF_OBJ_no_property
* UF_draft_area_fill_subtype
* UF_draft_solid_fill_subtype
*
* UF_drafting_entity_type UF_draft_intersection_subtype UF_OBJ_no_property
*
* UF_drafting_entity_type UF_draft_target_point_subtype UF_OBJ_no_property
*
* UF_drafting_entity_type UF_draft_user_defined_subtype UF_OBJ_no_property
*
* UF_drafting_entity_type UF_draft_assorted_parts_subtype UF_OBJ_no_property
* UF_dimension_type UF_all_subtype UF_OBJ_no_property
*
* Notes:
*
* 1. RM_general_object_type refers to all types without specific object
* settings. This setting is directly accessible through the
* UF_OBJ_ask_def_cre_settings & UF_OBJ_set_def_cre_<color or
* line_font or width> functions.
*
* 2. The UF_all_subtype subtype indicates that the settings are valid
* for all subtypes of the type.
*
* 3. UF_plane_type, UF_datum_axis_type and UF_datum_plane_type all share
* the same object creation settings. For example, if UF_plane_type's
* color is set to blue, UF_datum_axis_type's and UF_datum_plane_type's
* color will also be set to blue.
*
* 4. Asking for the color, line font and width object creation settings of
* (UF_drafting_entity_type, UF_draft_assorted_parts_subtype) or
* (UF_dimension_type, UF_all_subtype) will return the color, line font
* and width object creation settings for a Dimension. However,
* setting the color, line font and width object creation settings of
* (UF_drafting_entity_type, UF_draft_assorted_parts_subtype) or
* (UF_dimension_type, UF_all_subtype) will set the color, line font and
* width object creation settings for dimensions as well as
* extension lines 1 & 2, arrow lines 1 & 2, and arrowheads 1 & 2.
*
****************************************************************************/
/*****************************************************************************
Reads the work part's color, line font, and width object creation
settings for the type and subtype specified. If the type is an invalid
object type or if no object creation settings exist for the type and
subtype combination, then an error is returned. This routine uses the
settings structure UF_OBJ_cre_settings_s .
Environment: Internal and External
See Also:
UF_OBJ_cre_settings_t
For information on type, subtype and properties click here.
History:
****************************************************************************/
extern UFUNEXPORT int UF_OBJ_ask_cre_settings(
const int type ,/* <I>
type to ask settings of
*/
const int subtype ,/* <I>
Subtype of type to ask settings of
*/
const int property ,/* <I>
Property of type/subtype to ask settings of
*/
UF_OBJ_cre_settings_p_t settings /* <O>
Color, line font and width object creation
settings for the specified type and subtype.
*/
);
/*****************************************************************************
Set the specified type and subtype's color object creation setting in the
work part. If the type is not a valid object type or if no object creation
settings exist for the type and subtype combination then an error is
returned.
Environment: Internal and External
See Also:
See the string defined color constants in the types and symbols
For information on type, subtype and properties click here.
History:
****************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_cre_color(
const int type ,/* <I>
Type to set color of
*/
const int subtype ,/* <I>
Subtype to set color of
*/
const int property ,/* <I>
Property of type/subtype to set color of
*/
const int color /* <I>
Color for types new object creation
*/
);
/*****************************************************************************
Set the specified type and subtype's line font object creation setting in
the work part. If the type is not a valid object type or if no object
creation settings exist for the type and subtype combination then an
error is returned.
Environment: Internal and External
See Also:
See the line_font values in the types and symbols
For information on type, subtype and properties click here.
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_cre_line_font(
const int type ,/* <I>
Type to set line font of
*/
const int subtype ,/* <I>
Subtype to set line font of
*/
const int property ,/* <I>
Property of type/subtype to set line font of
*/
const int line_font /* <I>
Type's new object creation line font
*/
);
/*****************************************************************************
Set the specified type and subtype's width object creation setting in
the work part. If the type is not a valid object type or if no object
creation settings exist for the type and subtype combination then an
error is returned.
Environment: Internal and External
See Also:
See the width constants in the types and symbols
For information on type, subtype and properties click here.
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_cre_width(
const int type ,/* <I>
Type to set width of
*/
const int subtype ,/* <I>
Subtype to set width of
*/
const int property ,/* <I>
Property of type/subtype to set width of
*/
const int width /* <I>
Type's new object creation width
*/
);
/*****************************************************************************
Reads the work part's default color, line font, and width object
creation settings. This routine uses the settings structure
UF_OBJ_cre_settings_s.
Environment: Internal and External
See Also:
UF_OBJ_cre_settings_t
History:
****************************************************************************/
extern UFUNEXPORT int UF_OBJ_ask_def_cre_settings(
UF_OBJ_cre_settings_p_t settings /* <O>
Default color, line font and width object
creation settings for the specified type
and subtype.
*/
);
/*****************************************************************************
Sets the default color object creation setting. Does not work for sheet bodies
or solid bodies. Use UF_OBJ_set_cre_color_to_def or UF_OBJ_set_cre_color for
these specific object types.
Environment: Internal and External
See Also:
See the color string constants in the types and symbols
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_def_cre_color(
const int color /* <I>
New default object creation color
*/
);
/*****************************************************************************
Sets the default line_font object creation setting.
Environment: Internal and External
See Also:
See the line_font in the types and symbols
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_def_cre_line_font(
const int line_font /* <I>
New default object creation line_font
*/
);
/*****************************************************************************
Sets the default width object creation setting.
Environment: Internal and External
See Also:
See the width constants in the types and symbols
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_def_cre_width(
const int width /* <I>
New default object creation width
*/
);
/*****************************************************************************
Query if the work part's type/subtype color setting is using the default
color setting.
Environment: Internal and External
See Also:
For information on type, subtype and properties click here.
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_is_def_cre_color(
const int type ,/* <I>
Type to query
*/
const int subtype ,/* <I>
Subtype to query
*/
const int property ,/* <I>
Property of type/subtype to query
*/
logical * is_default /* <O>
TRUE = Color is set to default
FALSE = Color is not set to default
*/
);
/*****************************************************************************
Query if the work part's type/subtype line font setting is using the
default line font setting.
Environment: Internal and External
See Also:
For information on type, subtype and properties click here.
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_is_def_cre_line_font(
const int type ,/* <I>
Type to query
*/
const int subtype ,/* <I>
Subtype to query
*/
const int property ,/* <I>
Property of type/subtype to query
*/
logical * is_default /* <O>
TRUE = Line font is set to default
FALSE = Line font is not set to default
*/
);
/*****************************************************************************
Query if the work part's type/subtype line width setting is using the
default line width setting.
Environment: Internal and External
See Also:
For information on type, subtype and properties click here.
History:
****************************************************************************/
extern UFUNEXPORT int UF_OBJ_is_def_cre_width(
const int type ,/* <I>
Type to query
*/
const int subtype ,/* <I>
Subtype to query
*/
const int property ,/* <I>
Property of type/subtype to query
*/
logical * is_default /* <O>
TRUE = Line width is set to default
FALSE = Line width is not set to default
*/
);
/*****************************************************************************
Make the work part's type/subtype color setting use the default color
setting.
Environment: Internal and External
See Also:
For information on type, subtype and properties click here.
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_cre_color_to_def(
const int type ,/* <I>
Type to set color of
*/
const int subtype ,/* <I>
Subtype to set color of
*/
const int property /* <I>
Property of type/subtype to set color of
*/
);
/*****************************************************************************
Make the work part's type/subtype line font setting use the default
line font setting.
Environment: Internal and External
See Also:
For information on type, subtype and properties click here.
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_cre_line_font_to_def(
const int type ,/* <I>
Type to set line font of
*/
const int subtype ,/* <I>
Subtype to set line font of
*/
const int property /* <I>
Property of type/subtype to set line font of
*/
);
/*****************************************************************************
Make the work part's type/subtype width setting use the default width
setting.
Environment: Internal and External
See Also:
For information on type, subtype and properties click here.
History:
*****************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_cre_width_to_def(
const int type ,/* <I>
Type to set width of
*/
const int subtype ,/* <I>
Subtype to set width of
*/
const int property /* <I>
Property of type/subtype to set width of
*/
);
/*****************************************************************************
Returns the version of the part in which the given object was created
and the version in which it was last modified. The version numbers
returned are from 1 to the highest version number of the part, unless
there is an error, in which case the version numbers are set to 0. The
UF_PART_<xxxx> routines which deal with part save histories can be
used to obtain information about the versions of a part.
Environment: Internal and External
See Also:
UF_PART_ask_nth_history
UF_PART_ask_num_histories
UF_PART_ask_part_history
UF_PART_clear_history_list
UF_PART_create_history_list
UF_PART_delete_history_list
For example please refer to the example
History:
****************************************************************************/
extern UFUNEXPORT int UF_OBJ_ask_cre_mod_versions(
tag_t object ,/* <I>
Object Identifier
*/
int *creation_version,/* <O>
Object's creation version
*/
int *lastmod_version /* <O>
Object's last modification version
*/
);
/****************************************************************************
Sets the partial shading attribute for a solid face or for all faces in a
solid body.
Environment: Internal and External
See Also:
History:
****************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_partially_shaded(
tag_t object ,/* <I>
Object identifier of solid face or body to set
attributes for
*/
logical shaded /* <I>
Shaded status of the solid face
TRUE = set shading
FALSE = unset shading
*/
);
/****************************************************************************
Returns the partially shaded status for a single solid face.
Environment: Internal and External
See Also:
History:
****************************************************************************/
extern UFUNEXPORT int UF_OBJ_ask_partially_shaded(
tag_t object ,/* <I>
Object identifier of solid face to read attribute from
*/
logical * shaded /* <O>
Shaded status of the solid face
TRUE = shading is on
FALSE = shading is off
*/
);
/*****************************************************************************
Asks the translucency of faces, facets and bodies.
Environment: Internal and External
See Also:
History: Introduced in NX 2.0.2
****************************************************************************/
extern UFUNEXPORT int UF_OBJ_ask_translucency
(
tag_t object ,/* <I>
The object for which you are asking the translucency
It must be of one of the following types:
UF_solid_type, with one of these subtypes:
UF_solid_body_type
UF_solid_face_type
UF_faceted_model_type
UF_component_type
*/
UF_OBJ_translucency_p_t translucency /* <O>
percent translucent 0 - 100 */
);
/****************************************************************************
Sets the translucency of faces, facets and solid/sheet bodies.
Environment: Internal and External
See Also:
History: Introduced in NX 2.0.2
***************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_translucency
(
tag_t object ,/* <I>
The object for which you are setting the translucency
It must be of one of the following types:
UF_solid_type, with one of these subtypes:
UF_solid_body_type
UF_solid_face_type
UF_faceted_model_type
UF_component_type
*/
UF_OBJ_translucency_t translucency /* <I>
percent translucent 0 - 100 */
);
/*****************************************************************************
Queries if an object is a promoted object. Returns TRUE if object is a
promotion.
Environment: Internal and External
See Also:
History:
**************************************************************************/
extern UFUNEXPORT logical UF_OBJ_is_object_a_promotion (
tag_t object /* <I>
Tag of object to query
*/
);/* */
/****************************************************************************
Sets the face analysis attribute of a face. If the attribute is TRUE, the
face is displayed using analysis data in face analysis views. The
parameters defining the details of the display are specified by
UF_DISP_set_srfanl_params.
Environment: Internal
See Also:
UF_DISP_set_srfanl_params
History:
****************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_face_analysis(
tag_t face ,/* <I>
Object identifier of the face
*/
logical srfanl /* <I>
Shaded status of the face
TRUE = Display with analysis data in face analysis
views.
FALSE = Display without analysis data
*/
);
/****************************************************************************
Asks the face analysis attribute of a face. If the attribute is TRUE, the
face is displayed using analysis data in face analysis views. The
parameters defining the details of the display are specified by
UF_DISP_set_srfanl_params.
Environment: Internal
See Also:
UF_DISP_set_srfanl_params
History:
****************************************************************************/
extern UFUNEXPORT int UF_OBJ_ask_face_analysis(
tag_t face ,/* <I>
Object identifier
*/
logical * srfanl /* <O>
Face analysis data flag:
TRUE = Face is displayed with face analysis data
in face analysis views
FALSE = off
*/
);
/****************************************************************************
Replaces the geometry of the n'th element of the target object array with
the geometry of the n'th element of the source object array. Neither object
can be an occurrence but both objects may belong to the same component part
in an assembly. Both objects must be alive (see UF_OBJ_ask_status)
and both objects must be distinct and belong to the same part.
The target objects get added to the update list and any references to
these objects are maintained.
The source objects get added to the delete list.
Users must call UF_MODL_update() at the appropriate time to update
the target objects, delete the source objects and
propagate the changes to the model.
The type and subtype of each pair of objects must be valid for the routine
but they are not required to be the same. It is expected that the source
object is a newly created object with no extra user defined
attributes attached, and that it is not referenced by other objects.
Only valid geometry can exist in the objects, which consists of the
following (all subtypes are valid):
UF_point_type
UF_line_type
UF_circle_type
UF_conic_type
UF_spline_type
The display details [layer, color, line font and width, blank and
highlight status] and all user defined attributes, including names of
the target objects are all maintained. Links and references to the
target objects are preserved.
The reference set of the source objects are copied to the respective
target objects. If a source object is of a different type than the
corresponding target object, any occurrences existing based on the
target object are deleted and recreated by this routine.
Environment: Internal and External
See Also: UF_OBJ_replace_object_data
History:
***************************************************************************/
extern UFUNEXPORT int UF_OBJ_replace_object_array_data(
int num_objects, /* <I>
Number of objects whose geometry is to be replaced
*/
tag_t *target_objects,/* <I>
Target objects whose geometry is to be replaced
*/
tag_t *source_objects /* <I>
Source objects whose geometry is to be used as
replacements for target_objects
*/
);
/****************************************************************************
Replaces the geometry of the target object with the
geometry of the source object. Neither object can be an
occurrence but both objects may belong to the same component part
in an assembly. Both objects must be alive (see UF_OBJ_ask_status)
and both objects must be distinct and belong to the same part.
The target object gets updated and any references to this
object are maintained. The source object gets deleted.
The type and subtype of each object must be valid for the routine but
they are not required to be the same. It is expected that the source object
is a newly created object with no extra user defined attributes attached,
and that it is not referenced by other objects.
Only valid geometry can exist in either object which consists of the
following (all subtypes are valid):
UF_point_type
UF_line_type
UF_circle_type
UF_conic_type
UF_spline_type
The display details [layer, color, line font and width, blank and
highlight status] and all user defined attributes, including name of
the target object are all maintained. Links and references to the target
object are preserved. The reference set of the source object is copied to
the target object. If the source object is a different type than the
target object, any occurrences existing based on the target object are
deleted and recreated by this routine.
NOTE: This routine will update the model. If this is not desirable,
see UF_OBJ_replace_object_array_data()
Environment: Internal and External
See Also: UF_OBJ_replace_object_array_data
History:
***************************************************************************/
extern UFUNEXPORT int UF_OBJ_replace_object_data(
tag_t orig_obj ,/* <I>
Target object whose geometry is to be replaced.
*/
tag_t new_obj /* <I>
Source object whose geometry is to be used as a
replacement for orig_obj.
*/
);
/****************************************************************************
Cycles objects in the specified part by name and object type. Note that
the name of an object of type UF_occ_instance_type is not necessarily the
instance name.
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
Environment: Internal and External
See Also:
History: This function was originally released in V15.0.
****************************************************************************/
extern UFUNEXPORT int UF_OBJ_cycle_by_name_and_type(
tag_t part_tag ,/* <I>
Tag of part in which to cycle.
*/
const char * name ,/* <I>
Name of objects on which to cycle.
*/
int type ,/* <I>
Object type on which to cycle (see uf_object_types.h)
*/
logical use_occ ,/* <I>
Occurrence filter:
TRUE = include occurrences
FALSE = exclude occurrrences
*/
tag_t * object /* <I/O>
On input the object found by the last call to this routine.
Begin the cycle by passing in object = NULL_TAG
On output, the next object of the given name. Outputs a
NULL_TAG when the cycle is finished.
*/
);
/****************************************************************************
Cycles objects in the specified part by name and object type. Note that
the name of an object of type UF_occ_instance_type is not necessarily the
instance name.
This works like UF_OBJ_cycle_by_name_and_type.
The difference between this routine and UF_OBJ_cycle_by_name_and_type is that
UF_OBJ_cycle_by_name_and_type returns all the extended objects (extended object
types have values over 256) if either UF_extended_type or UF_extended_displayable_type
is passed in as type. Whereas this routine does not return any objects for those two types
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
Environment: Internal and External
See Also:
UF_OBJ_cycle_by_name_and_type
History: This function was originally released in V15.0.
****************************************************************************/
extern UFUNEXPORT int UF_OBJ_cycle_by_name_and_type_extended(
tag_t part_tag ,/* <I>
Tag of part in which to cycle.
*/
const char * name ,/* <I>
Name of objects on which to cycle.
*/
int type ,/* <I>
Object type on which to cycle (see uf_object_types.h)
*/
logical use_occ ,/* <I>
Occurrence filter:
TRUE = include occurrences
FALSE = exclude occurrrences
*/
tag_t * object /* <I/O>
On input the object found by the last call to this routine.
Begin the cycle by passing in object = NULL_TAG
On output, the next object of the given name. Outputs a
NULL_TAG when the cycle is finished.
*/
);
/**********************************************************************
Returns the tag of the part which contains the specified object_in_part.
Environment: Internal and External
See Also:
History:
*********************************************************************/
extern UFUNEXPORT int UF_OBJ_ask_owning_part(
tag_t object_in_part ,/* <I>
Tag of object for which the part is required.
*/
tag_t * part_tag /* <O>
part containing object_in_part
*/
);
/*
******************************************************************************
******************************************************************************
***** WARNING: The routines that follow will be soon be obsoleted *****
***** Do not use them! Use their indicated replacements. *****
******************************************************************************
******************************************************************************
*/
/* uf5025 read part file data and set default object -- replaced by default
creation routines above */
extern UFUNEXPORT void FTN(uf5025)(int *ia1, int *ia2,
int *ia3, int *ia4);
/* uf5026 temporarily modify object defaults -- replaced by default creation
routines above */
extern UFUNEXPORT void FTN(uf5026)(const int *ip1, const int *ip2,
const int *ip3, const int *ip4,
const int *ip5);
/* uc5027 read object name -- replaced by UF_OBJ_ask_name */
extern UFUNEXPORT int uc5027(tag_t np1, char cr2[ UF_OBJ_NAME_BUFSIZE ] /* <O> */, int *ir3);
/* uc5028 find named object -- replaced by UF_OBJ_cycle_by_name */
extern UFUNEXPORT int uc5028(const char *cp1 /* <I> */, int ip2, tag_t *nr3);
/* uc5029 add/modify object name -- replaced by UF_OBJ_set_name */
extern UFUNEXPORT int uc5029(tag_t np1, const char *cp2 /* <I> */, int ip3);
/* uc502a read object font -- NO REPLACEMENT (use
UF_OBJ_ask_display_properties) */
extern UFUNEXPORT int uc502a(tag_t np1, char cr2[31 ] /* <O> */);
/* uc502e temporarily modify object defaults -- NO REPLACEMENT (use default
creation routines above) */
extern UFUNEXPORT int uc502e(int ip1, int ip2, int ip3, int ip4, const char *cp5 /* <I> */);
/* uc502m edit object font -- NO REPLACEMENT (use UF_OBJ_set_font) */
extern UFUNEXPORT int uc502m(tag_t np1, const char *cp2 /* <I> */);
/* uc502n read part file data and set default object -- NO REPLACEMENT (use
default creation routines
above) */
extern UFUNEXPORT int uc502n(int *ia1, int *ia2, int *ia3, char ca4[ UF_OBJ_NAME_BUFSIZE ]/* <I/O> */);
/* uc502r read current font definition file name -- NO REPLACEMENT */
extern UFUNEXPORT int uc502r(int ip1, char ca2[ MAX_FSPEC_BUFSIZE]/* <I/O> */);
/* uc5203 cycle by object name -- replaced by UF_OBJ_cycle_by_name */
extern UFUNEXPORT void uc5203(tag_t *na1, const char *cp2 /* <I> */, int ip3);
/* UF_OBJ_reset_defaults -- replaced by default routines above */
extern UFUNEXPORT int UF_OBJ_reset_defaults(
int default_color, /* <I> */
int default_layer, /* <I> */
int default_width, /* <I> */
int default_font /* <I> */
);
/* UF_OBJ_return_prev_defaults -- replaced by default routines above */
extern UFUNEXPORT int UF_OBJ_return_prev_defaults(void);
/* UF_OBJ_modify_defaults -- replaced by default routines above */
extern UFUNEXPORT int UF_OBJ_modify_defaults(
int default_color, /* <I> */
int default_layer, /* <I> */
int default_width, /* <I> */
int default_font /* <I> */
);
/******************************************************************************
Modifies the layer of an object. Use UF_OBJ_ask_display_properties to
determine the object's current layer.
This function allows movement to and from the hidden layers.
Environment: Internal and External
See Also:
UF_OBJ_set_layer
UF_OBJ_ask_display_properties
History: Original release was in NX 3.0.3
******************************************************************************/
extern UFUNEXPORT int UF_OBJ_set_layer_allow_hidden(
tag_t object_id ,/* <I>
Object identifier of object whose layer is to be
changed.
*/
int layer /* <I>
layer to assign.
*/
);
#undef EXPORTLIBRARY
#endif /* UF_OBJ_INCLUDED */