UF_DISP_activate_grid (view source)
Defined in: uf_disp.h
Overview
This causes the grid to be display immediately instead of waiting for a
system determined regeneration (at more opportune time). However, trying
to activate a grid in the wrong context will not work. For example, a drawing
grid cannot be displayed in the Modeling application context.
product_context - either UF_DISP_SKETCH_GRID for sketcher application,
or UF_DISP_DRAWING_GRID for drawing,
or UF_DISP_SHED_GRID for True Shading display,
or UF_DISP_MODEL_GRID for others (or default).
Environment
Internal and External
See Also
History
Originally released in V19.0
Required License(s)
gateway
void UF_DISP_activate_grid
(
UF_DISP_grid_context_t product_context
)
UF_DISP_grid_context_t | product_context | Input | either UF_DISP_SKETCH_GRID or UF_DISP_DRAWING_GRID or UF_DISP_MODEL_GRID or UF_DISP_SHED_GRID |
UF_DISP_add_item_to_display (view source)
Defined in: uf_disp_ugopenint.h
Overview
Adds an object to the display. You can use this routine to update the
display of a new or modified object, if UF_DISP_set_display has been
used to turn off the display update.
Environment
Internal
Required License(s)
gateway
int UF_DISP_add_item_to_display
(
tag_t object_id
)
tag_t | object_id | Input | Object identifier of the object to be added to display |
UF_DISP_ask_closest_color (view source)
Defined in: uf_disp.h
Overview
Determines the color in the Color Table Object (CTO) "closest" to
the given color values, based on the specified Color Comparison
Method. The index of the closest color is returned.
UF_DISP_CCM_EUCLIDEAN_DISTANCE - this method returns the
color which is the least Euclidean distance away from the given color
in the RGB color cube.
Note that the background color is not considered as a candidate.
There must be a part loaded when this function is called.
Environment
Internal
See Also
Required License(s)
gateway
int UF_DISP_ask_closest_color
(
int clr_model,
double clr_values [ 3 ] ,
int clr_cmp_mtd,
int * clr_num
)
int | clr_model | Input | The color model of the values in clr_values; the following constants are defined in uf_disp.h: UF_DISP_rgb_model UF_DISP_hsv_model UF_DISP_hls_model |
double | clr_values [ 3 ] | Input | Three doubles representing the color, where the meaning and range of each value depends on the color model specified: rgb: clr_values[0]: 0.0 <= red <= 1.0 clr_values[1]: 0.0 <=green <= 1.0 clr_values[2]: 0.0 <= blue <= 1.0 hsv: clr_values[0]: 0.0 <= hue <= 360.0 clr_values[1]: 0.0 <= saturation <= 1.0 clr_values[2]: 0.0 <= value <= 1.0 hls: clr_values[0]: 0.0 <= hue <= 360.0 clr_values[2]: 0.0 <= light <= 1.0 clr_values[1]: 0.0 <= saturation <= 1.0 |
int | clr_cmp_mtd | Input | The Color Comparison Method currently only UF_DISP_CCM_EUCLIDEAN_DISTANCE is defined. |
int * | clr_num | Output | The number of the closest color. Range: 1 .. (# color records in CTO) - 1 Note: the background color is not considered as a candidate. |
UF_DISP_ask_closest_color_in_displayed_part (view source)
Defined in: uf_disp.h
Overview
Returns the index of the color in the color table of the currently
displayed part that is most similar to the color indicated by the
given color name symbol.
If the specified part cannot be found, then the closest color in
the default color definition file (CDF) specified by the customer
defaults file is returned. If no such file exists, then the closest
color in the system color table is returned.
Return
Zero is returned upon successful execution.
Any other return code indicates an error.
Environment
Internal and External
See Also
History
Originally released in NX3.
Required License(s)
gateway
int UF_DISP_ask_closest_color_in_displayed_part
(
UF_DISP_color_name_t color_name,
int * color_index
)
UF_DISP_color_name_t | color_name | Input | symbol for color name |
int * | color_index | Output | color index of most similar color |
UF_DISP_ask_closest_color_in_part (view source)
Defined in: uf_disp.h
Overview
Returns the index of the color in the color table of the specified
part that is most similar to the color indicated by the given color
name symbol. Parameter object_in_part identifies the part; the
parameter can be set to the part tag or the tag of an object in the
part.
If the specified part cannot be found, then the closest color in
the default color definition file (CDF) specified by the customer
defaults file is returned. If no such file exists, then the closest
color in the system color table is returned.
Return
Zero is returned upon successful execution.
Any other return code indicates an error.
Environment
Internal and External
See Also
History
Originally released in NX3.
Required License(s)
gateway
int UF_DISP_ask_closest_color_in_part
(
tag_t object_in_part,
UF_DISP_color_name_t color_name,
int * color_index
)
tag_t | object_in_part | Input | object in part of interest |
UF_DISP_color_name_t | color_name | Input | symbol for color name |
int * | color_index | Output | color index of most similar color |
UF_DISP_ask_color (view source)
Defined in: uf_disp.h
Overview
Obtains the name and values of the specified color from the Color
Table object (CTO) of the Display part. The color values are given
using the specified color model.
Note that the maximum value permitted for clr_num is the number of
records presently in the CTO, minus 1. The number of CTO records
may be obtained by calling UF_DISP_ask_color_count. There must be
a part loaded when this function is called.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_DISP_ask_color
(
int clr_num,
int clr_model,
char * * clr_name,
double clr_values [ 3 ]
)
int | clr_num | Input | The number of the color whose name and value are to be returned; Range: 0 .. (# color records in CTO) - 1 Note: 0 is for the background color |
int | clr_model | Input | The color model of the values in clr_values: UF_DISP_rgb_model UF_DISP_hsv_model UF_DISP_hls_model |
char * * | clr_name | Output to UF_*free* | A pointer to the name of the color. This must be freed by the caller using UF_free |
double | clr_values [ 3 ] | Output | Three doubles representing the color, where the meaning and range of each value depends on the color model specified: rgb: clr_values[0]: 0.0 <= red <= 1.0 clr_values[1]: 0.0 <=green <= 1.0 clr_values[2]: 0.0 <= blue <= 1.0 hsv: clr_values[0]: 0.0 <= hue <= 360.0 clr_values[1]: 0.0 <= saturation <= 1.0 clr_values[2]: 0.0 <= value <= 1.0 hls: clr_values[0]: 0.0 <= hue <= 360.0 clr_values[2]: 0.0 <= light <= 1.0 clr_values[1]: 0.0 <= saturation <= 1.0 |
UF_DISP_ask_color_count (view source)
Defined in: uf_disp.h
Overview
Returns the actual number of records currently in the Color Table
object of the Display part, including the record for the background
color. There must be a part loaded when this function is called.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_DISP_ask_color_count
(
int * count
)
int * | count | Output | number of records in the color table object (includes background color) |
UF_DISP_ask_current_grid_context (view source)
Defined in: uf_disp.h
Overview
This function returns the current application for task environment
return - either UF_DISP_SKETCH_GRID for sketcher application,
or UF_DISP_DRAWING_GRID for drawing,
or UF_DISP_SHED_GRID for True Shading display,
or UF_DISP_MODEL_GRID for others (or default).
or UF_DISP_NULL_GRID if no grid is setup yet
Environment
Internal and External
See Also
History
Originally released in V19.0
Required License(s)
gateway
UF_DISP_grid_context_t UF_DISP_ask_current_grid_context
(
void
)
UF_DISP_ask_currently_selected_material (view source)
Defined in: uf_disp.h
Overview
This function returns ERROR_OK or zero if either
a material in the Materials in Part Palette is selected or
a material in the Materials Library is selected depending which was selected lastly.
If material selected is from the Materials in Part palette, then both material_tag and
material_full_archive_name will be returned. If the material selected is from
the Materials library, then only material_full_archive_name will be returned.
The function also returns the material source of UF_DISP_material_source_t type.
This can be used to determine which of UF_DISP_ask_work_part_material_lwa_user_area_data
or UF_DISP_ask_library_material_lwa_user_area_data to call to find the
LWA (LightWork Archive) user area data.
If no material is found selected, non-zero is returned.
This function applies to materials of current renderer type.
Environment
Internal only
History
This function is created for NX604.
Required License(s)
gateway
int UF_DISP_ask_currently_selected_material
(
UF_DISP_material_source_t * material_source,
tag_t * material_tag,
char material_full_archive_name [ MAX_FSPEC_BUFSIZE ]
)
UF_DISP_material_source_t * | material_source | Output | UF_DISP_lw_material_in_Materials_Library or UF_DISP_lw_material_in_Materials_in_Part_Palette |
tag_t * | material_tag | Output | The tag of material that is currently selected in the Materials in Part Palette |
char | material_full_archive_name [ MAX_FSPEC_BUFSIZE ] | Output | The full_arachive_name of the material currently selected in the Materials in part palette or the Materials Library |
UF_DISP_ask_display (view source)
Defined in: uf_disp.h
Overview
Queries the display status. You can use UF_DISP_ask_display to find out
the current state of the graphics display.
Environment
Internal
History
Released in V16.0
Required License(s)
gateway
int UF_DISP_ask_display
(
int * display_code
)
int * | display_code | Output | display code: UF_DISP_SUPPRESS_DISPLAY- set display off UF_DISP_UNSUPPRESS_DISPLAY- set display on |
UF_DISP_ask_display_context (view source)
Defined in: uf_disp.h
Overview
Inquires the context pointer and returns information about display,
selection, fit, and attention point information in the output structure.
This function can be called prior to displaying geometry, after
geometry is displayed, or both. This routine may only be called from a
UDO registered callback routine. The context argument passed into this
routine will be passed from NX to the UDO callback routine.
NOTE: All values in the inquiry structure are set to NULL or FALSE by this function
except for the following:
If this routine is being called from the attention point callback the
is_attn_pt_valid field is set to TRUE.
If this routine is being called from the fit callback only the view_tag is set.
If this routine is being called from the display callback,
the view_tag, is_draw_open_disp, is_view_mode_valid, and view_mode fields
are set.
Environment
Internal and External
See Also
History
Modified in V17 to return the view tag
Required License(s)
gateway
int UF_DISP_ask_display_context
(
void * context,
UF_DISP_inquire_p_t inquiry
)
void * | context | Input | The private context pointer obtained from the callback. |
UF_DISP_inquire_p_t | inquiry | Output | The inquiry structure. |
UF_DISP_ask_drawing_display (view source)
Defined in: uf_disp.h
Overview
Returns the data that affects drawing monochrome display.
This routine MUST be called to populate the data structure, before
UF_DISP_set_drawing_display is called.
Please reference ufd_disp.c to review a sample execution of this function.
Return
UF_err_program_not_initialized
Environment
Internal and External
See Also
History
None
Required License(s)
gateway
int UF_DISP_ask_drawing_display
(
UF_DISP_drawing_display_data_p_t drawing_display
)
UF_DISP_ask_geometry_of_material (view source)
Defined in: uf_disp.h
Overview
This function returns a list of geometry object tags that are associated to
the given material tag.
The object_tags are limited to these types: UF_solid_type, UF_solid_face_subtype
and UF_faceted_model_type.
This function supports both types of materials.
Environment
Internal
See Also
History
This function is created for NX7.5 QRM.
Required License(s)
gateway
int UF_DISP_ask_geometry_of_material
(
const tag_t material_tag,
int * object_count,
tag_p_t * object_tags
)
const tag_t | material_tag | Input | The tag of material that is assigned to the returned objects. |
int * | object_count | Output | Number of objects found |
tag_p_t * | object_tags | Output to UF_*free* | A pointer to a list of geometry object tags associated to the given material. |
UF_DISP_ask_grid_parameters (view source)
Defined in: uf_disp.h
Overview
Queries the information about the grid in the designated application
context. The 'product_context' variable must be set.
product_context - either UF_DISP_SKETCH_GRID for sketcher application,
or UF_DISP_DRAWING_GRID for drawing,
or UF_DISP_SHED_GRID for True Shading display,
or UF_DISP_MODEL_GRID for others (or default).
Environment
Internal and External
See Also
History
Originally released in V19.0
Required License(s)
gateway
void UF_DISP_ask_grid_parameters
(
UF_DISP_grid_context_t product_context,
UF_DISP_grid_p_t output_grid
)
UF_DISP_ask_library_material_lwa_user_area_data (view source)
Defined in: uf_disp.h
Overview
This function returns the LWA user area data based on the material_full_archive_name and the
specification_attribute_string_key.
If the specified data is found in the LWA user area data, ERROR_OK or 0 is returned.
This function only supports Author based materials and libraries.
Environment
Internal only
History
This function is created for NX604.
Required License(s)
gateway
int UF_DISP_ask_library_material_lwa_user_area_data
(
char * material_full_archive_name,
const char * attribute_string_key,
const char * * attribute_data
)
char * | material_full_archive_name | Input | the full archive_name of the material to get lwa user area data |
const char * | attribute_string_key | Input | key to identify which data in the lwa user data area to get |
const char * * | attribute_data | Output | return the user area data specified by the attribute_string_key |
UF_DISP_ask_material (view source)
Defined in: uf_disp.h
Overview
This function returns the material tag and name of the material assigned to
the object defined by object_tag.
The object_tag is limited to these types: UF_solid_type, UF_solid_face_subtype
and UF_faceted_model_type.
This function supports both types of materials, but will only work on the materials of
the current renderer type.
For example, if you are using the Author RTS renderer(vs. Iray+ RTS renderer), then this API
will apply to Author type materials.
Environment
Internal and External
See Also
History
This function is created for NX3 QRM.
Required License(s)
gateway
int UF_DISP_ask_material
(
const tag_t object_tag,
tag_p_t material_tag,
char material_name [ UF_SF_MAX_MAT_NAME_BUFSIZE ]
)
const tag_t | object_tag | Input | The tag of the object. |
tag_p_t | material_tag | Output | The tag of material that is assigned to the specified object. |
char | material_name [ UF_SF_MAX_MAT_NAME_BUFSIZE ] | Output | The name of the material |
UF_DISP_ask_model_bounds (view source)
Defined in: uf_disp.h
Overview
Returns the model bounds of the work part. Each part should contain
exactly one "model bounds object" which ideally contains a 3D box in
absolute space inside of which is all of the geometry of the work part.
NOTE: In general, the model bounds returned by this function are
NOT accurate, as NX does not usually update the model bounds as
objects are created, modified, and deleted. This function is intended
for use by certain NX applications such as translators which know that
their application has earlier computed model bounds which are still
known to be valid.
Environment
Internal and External
Required License(s)
gateway
int UF_DISP_ask_model_bounds
(
const tag_t model_bounds_obj,
double model_bounds [ 6 ]
)
const tag_t | model_bounds_obj | Input | The tag of the Model Bounds object of the work part. Use UF_DISP_ask_model_bounds_tag to find this tag. |
double | model_bounds [ 6 ] | Output | The model bounds of the work part. The six values are (Minimum_X, Maximum_X, Minimum_Y, Maximum_Y, Minimum_Z, Maximum_Z) |
UF_DISP_ask_model_bounds_tag (view source)
Defined in: uf_disp.h
Overview
Returns the model bounds tag of the work part. Each part should
contain exactly one "model bounds object" which ideally contains a
3D box in absolute space inside of which is all of the geometry of the
work part.
Environment
Internal and External
Required License(s)
gateway
int UF_DISP_ask_model_bounds_tag
(
tag_t * model_bounds_object
)
tag_t * | model_bounds_object | Output | The tag of the Model Bounds object of the work part. If the work part has no model bounds object (which is an abnormal condition), NULL_TAG is returned. |
UF_DISP_ask_name_display_status (view source)
Defined in: uf_disp.h
Overview
Returns the current name display setting.
Environment
Internal and External
Required License(s)
gateway
int UF_DISP_ask_name_display_status
(
int * current_status
)
int * | current_status | Output | Name Display Status: UF_DISP_NAME_DISPLAY_OFF UF_DISP_NAME_DISPLAY_ON |
UF_DISP_ask_name_view_status (view source)
Defined in: uf_disp.h
Overview
Returns the current name display view setting. The constant
UF_DISP_NAMES_IN_VIEW_OF_DEFN is the view which was the
work view when the object was defined.
Environment
Internal and External
Required License(s)
gateway
int UF_DISP_ask_name_view_status
(
int * current_status
)
int * | current_status | Output | View Status 0 = UF_DISP_NAMES_IN_WORK_VIEW 1 = UF_DISP_NAMES_IN_VIEW_OF_DEFN |
UF_DISP_ask_srfanl_params (view source)
Defined in: uf_disp.h
Overview
Reads the face analysis display parameters into the supplied
UF_DISP_srfanl_data_t structure. This routine uses a pointer to the
structure UF_DISP_srfanl_data_s.
Environment
Internal
Required License(s)
gateway
int UF_DISP_ask_srfanl_params
(
UF_DISP_srfanl_data_t * params
)
UF_DISP_ask_system_parameters (view source)
Defined in: uf_disp.h
Overview
Reads system display parameters. This routine uses a pointer to the
structure UF_DISP_system_params_s.
To access parameters related to shaded face edges, please use
UF_VIEW_ask_shaded_edge_options instead.
Environment
Internal and External
See Also
History
V12.0 light_source_angles field removed from the structure
V13.0 Added show_shaded_face_edges and hidden_shaded_face_edges
to the structure
V19.0 Added fields use_face_edges_color
face_edges_color
hidden_geometry_color
random_color_displayed
random_color_object_type
Required License(s)
gateway
int UF_DISP_ask_system_parameters
(
UF_DISP_system_params_p_t system_parameters
)
UF_DISP_ask_texture_space_info (view source)
Defined in: uf_disp.h
Overview
This function returns the texture space information required for the
specified material.
For certain material texture (e.g., logos), texture space information is
required to describe how to place the texture on a body so the texture image
or pattern will appear correctly on the model (orientation, position and
scale). If texture space information is not found for the material
(e.g., for non-textured materials, such as metals), ts_info_defined will
be set to 0 and no texture space information will be returned.
This function only supports Author based materials.
Environment
Internal and External
See Also
History
This function is created for NX3 QRM.
Required License(s)
gateway
int UF_DISP_ask_texture_space_info
(
tag_t material_tag,
UF_DISP_texture_space_info_t * ts_info_ptr,
int * ts_info_defined
)
tag_t | material_tag | Input | tag of material to request texture space information for. |
UF_DISP_texture_space_info_t * | ts_info_ptr | Output | texture space information |
int * | ts_info_defined | Output | value of 1 is returned if texture space information is returned |
UF_DISP_ask_work_part_material_lwa_user_area_data (view source)
Defined in: uf_disp.h
Overview
This function returns the LWA user area data based on the material tag and the
specification_attribute_string_key.
If the specified data is found from the LWA user area data, ERROR_OK or 0 is returned.
This function only supports Author based materials.
Environment
Internal only
History
This function is created for NX604.
Required License(s)
gateway
int UF_DISP_ask_work_part_material_lwa_user_area_data
(
tag_t material_tag,
const char * attribute_string_key,
const char * * attribute_data
)
tag_t | material_tag | Input | the tag of the material to get the lwa user area data |
const char * | attribute_string_key | Input | key to identify which data in the lwa user data area to get NOTE max key length is 31 |
const char * * | attribute_data | Output | return the user area data specified by the attribute_string_key |
UF_DISP_ask_work_plane_emphasis (view source)
Defined in: uf_disp.h
Overview
Queries the current work plane emphasis setting. When work plane emphasis
is on, objects that do not lie on the work plane appear de-emphasized, in
which the object color is blended with the De-emphasis Blend Color according
to the De-emphasis Blend Percentage. A de-emphasized object is unselectable
unless the work plane emphasis selection filter is overridden. Work plane
emphasis is a session dependent value; it is not saved with any part.
Environment
Internal and External
See Also
History
Original release was in V13.0.
Required License(s)
gateway
int UF_DISP_ask_work_plane_emphasis
(
int * emphasis
)
int * | emphasis | Output | Emphasis setting. Must be one of: UF_DISP_WORK_PLANE_EMPHASIS_ON, or UF_DISP_WORK_PLANE_EMPHASIS_OFF |
UF_DISP_ask_work_plane_sel (view source)
Defined in: uf_disp.h
Overview
Queries the value of the selection override for work plane emphasis.
When work plane emphasis is enabled and the selection override is
equal to UF_DISP_SELECT_WORK_DIMMED, no objects are
filtered out of selection because they are off the work plane.
When work plane emphasis is enabled and the selection override is
equal to UF_DISP_NO_SELECT_WORK_DIMMED, no objects
dimmed for work plane emphasis are selectable.
When work plane emphasis is disabled, the selection override setting
has no affect although it can be changed. The selection override
setting takes effect once work plane emphasis is enabled.
The work plane emphasis selection override is a session dependent
value; it is not saved with any part.
Environment
Internal and External
See Also
History
Original release was in V13.0.
Required License(s)
gateway
int UF_DISP_ask_work_plane_sel
(
int * override
)
int * | override | Output | Emphasis selection override setting. Must be either: UF_DISP_SELECT_WORK_DIMMED, or UF_DISP_NO_SELECT_WORK_DIMMED |
UF_DISP_assign_material (view source)
Defined in: uf_disp.h
Overview
This function assigns the material to object
NOTE object types accepted include: UF_solid_type, UF_solid_face_subtype
and UF_faceted_model_type.
This function supports assigning of both types of materials (Iray+ and Author).
Environment
Internal and external
See Also
History
This function is created for NX3 QRM.
Required License(s)
gateway
int UF_DISP_assign_material
(
const tag_t material_tag,
const tag_t object_tag
)
const tag_t | material_tag | Input | The tag of the material to assign to object |
const tag_t | object_tag | Input | The tag of object to assign the material to |
UF_DISP_batch_shade (view source)
Defined in: uf_disp.h
Overview
Creates a shaded image using the capabilities of NX Photo and saves
that image as a TIFF, GIF, or JPEG file. You specify the image type
by including the appropriate file extension in the save_filename
parameter. Use any one of the following file extensions:
.tif - TIFF
.gif - GIF
.jpg - JPEG
For example, specifying "test.jpg" for the filename parameter
creates a JPEG file.
The batch shade function shades the active view using the light
sources, backgrounds, foregrounds, materials and textures that were
setup using interactive NX. If the current layout is a drawing then
this function will return without creating an output file.
If using a shade method of UF_DISP_high_quality, UF_DISP_preview,
UF_DISP_photo_real or UF_DISP_raytrace then a Studio Render license
is required. If this license is not available then the method will
default back to UF_DISP_phong.
Please note this API generates output shaded image file using Lightworks Author renderer and
supports Lightworks Author materials and textures. IrayPlus materials won't be processed.
Please set NX_RTS_IRAY=0 before executing NX Open utilities using this API.
Environment
Internal and External
See Also
History
This function was modified in V14.0 to also produce GIF
and JPEG files
Required License(s)
gateway
int UF_DISP_batch_shade
(
char* filename,
int x_size,
int y_size,
UF_DISP_shade_method_t method
)
char* | filename | Input | Name of output TIFF, GIF, or JPEG file |
int | x_size | Input | X size of output in pixels |
int | y_size | Input | Y size of output in pixels |
UF_DISP_shade_method_t | method | Input | Type of shade to produce. Either: UF_DISP_flat, UF_DISP_gouraud, UF_DISP_phong, UF_DISP_high_quality, UF_DISP_preview, UF_DISP_photo_real, or UF_DISP_raytrace |
UF_DISP_batch_shade_options (view source)
Defined in: uf_disp.h
Overview
Creates a shaded image using the capabilities of NX Photo and saves
that image as a TIFF, GIF, or JPEG file. You specify the image type
by including the appropriate file extension in the save_filename
parameter. Use any one of the following file extensions:
.tif - TIFF
.gif - GIF
.jpg - JPEG
For example, specifying "test.jpg" for the filename parameter
creates a JPEG file.
The batch shade function shades the active view using the light
sources, backgrounds, foregrounds, materials and textures that were
setup using interactive NX. If the current layout is a drawing then
this function will return without creating an output file.
This function allows setting of some options for the shading process.
If using a shade method of UF_DISP_high_quality, UF_DISP_preview,
UF_DISP_photo_real or UF_DISP_raytrace then a Studio Render license
is required. If this license is not available then the method will
default back to UF_DISP_phong.
Please note this API generates output shaded image file using Lightworks Author renderer and
supports Lightworks Author materials and textures. IrayPlus materials won't be processed.
Please set NX_RTS_IRAY=0 before executing NX Open utilities using this API.
Environment
Internal and External
History
This function was first released in NX3.0.3
Required License(s)
gateway
int UF_DISP_batch_shade_options
(
char* filename,
int x_size,
int y_size,
UF_DISP_shade_method_t method,
UF_DISP_shade_options_p_t options
)
char* | filename | Input | Name of output TIFF, GIF, or JPEG file |
int | x_size | Input | X size of output in pixels |
int | y_size | Input | Y size of output in pixels |
UF_DISP_shade_method_t | method | Input | Type of shade to produce. Either: UF_DISP_flat, UF_DISP_gouraud, UF_DISP_phong, UF_DISP_high_quality, UF_DISP_preview, UF_DISP_photo_real, or UF_DISP_raytrace |
UF_DISP_shade_options_p_t | options | Input | Options to control the shading process. |
UF_DISP_compute_model_bounds (view source)
Defined in: uf_disp.h
Overview
Computes the model bounds for the work part. The model bounds
defines a box in Absolute coordinates which contains all of the
potentially displayable geometry of the part. The sides of the box are
parallel to the axes of the absolute coordinate system. Objects which
are not currently displayable, because they are blanked or on an
invisible layer, are still included within the model bounds.
If there are no displayable objects in the part, bounds_computed will
be FALSE, and model_bounds will contain default bounds, which are
the size of the current graphics in X and Y, with Z the same as the
smaller of X and Y.
NOTE: This function is of limited value for most NX Open API
application developers. It is intended to be used by certain NX
applications such as translators.
Environment
Internal and External
Required License(s)
gateway
int UF_DISP_compute_model_bounds
(
logical * bounds_computed,
double model_bounds [ 6 ]
)
logical * | bounds_computed | Output | TRUE if there are some displayable objects in the work part, so that normal model bounds were computed. FALSE if the work part has no displayable objects |
double | model_bounds [ 6 ] | Output | The model bounds for the work part. This is a box in absolute space, whose sides are parallel to the axes of the absolute coordinate system. The six values of the array are the Minimum_X, Maximum_X, Minimum_Y, Maximum_Y, Minimum_Z and Maximum_Z of the box. If bounds_computed is FALSE, default bounds are returned. The default bounds are roughly the size of the current graphics window. |
UF_DISP_conehead (view source)
Defined in: uf_disp_ugopenint.h
Overview
Displays a temporary conehead vector with either the base of the staff,
the arrow tip or the base of the arrow head at the reference point
in the specified view.
Return
void
Environment
Internal
See Also
Required License(s)
gateway
void UF_DISP_conehead
(
int display_flag,
double coord [ 3 ] ,
double vector [ 3 ] ,
int anchor_flag
)
int | display_flag | Input | Display views to draw the conehead vector in. UF_DISP_ALL_VIEWS_BUT_DRAWING UF_DISP_VIEW_OF_LAST_CURSOR UF_DISP_ALL_ACTIVE_VIEWS UF_DISP_WORK_VIEW_ONLY >0 = View sequence number |
double | coord [ 3 ] | Input | 3D absolute coordinates of anchor. |
double | vector [ 3 ] | Input | 3D vector which gives conehead direction |
int | anchor_flag | Input | Denotes the anchor point 0 = Anchor point at base of staff 1 = Anchor point at tip of arrowhead 2 = Anchor point at base of arrowhead |
UF_DISP_copy_LWA_archive_material_to_work_part (view source)
Defined in: uf_disp.h
Overview
This function copies a material specified by the material_name input argument from the currently
opened Lightworks LWA archive material library to the work part.
NOTE: this API will not work on CgFX materials.
Returns
0 = Success
-1 = Failed to find an opened LWA archive materials library
-2 = Failed to import named material.
Not -1,-2, 0 = Error code
Standard UF Error Codes:
UF_err_program_not_initialized
UF_err_bad_parameter_number_1: problem found with material_name argument
UF_err_part_not_loaded: need to have an opened work part.
This function only supports Author based materials and libraries(lwa).
Environment
Internal and external
See Also
History
This function is created for NX8.5.3
Required License(s)
gateway
int UF_DISP_copy_LWA_archive_material_to_work_part
(
const char* material_name,
tag_p_t material_tag
)
const char* | material_name | Input | The name of material in the currently opened archive material library to copy to the work part. |
tag_p_t | material_tag | Output | The tag of the copied material. |
UF_DISP_copy_material (view source)
Defined in: uf_disp.h
Overview
This function creates a new material based on an existing material
attributes defined by the given material tag.
This function supports copying of both type of materials(Iray+ and Author).
Environment
Internal and External
See Also
History
This function is created for NX3 QRM.
Required License(s)
gateway
int UF_DISP_copy_material
(
const tag_t material_tag,
tag_t * new_material_tag,
char new_material_name [ MAX_FSPEC_BUFSIZE ]
)
const tag_t | material_tag | Input | The tag of material that the new material is copied from. |
tag_t * | new_material_tag | Output | new material tag |
char | new_material_name [ MAX_FSPEC_BUFSIZE ] | Output | The name of the newly copied material |
UF_DISP_create_animation (view source)
Defined in: uf_disp.h
Overview
Allows the batch creation of an MPEG movie based on an existing
animation saved in the opened part. An Animation can be created
using the Create Animation Dialog. See the NX Gateway Online
help for details on creating an animation name and frames.
Note that only animations of "Define Key Frames" type are supported.
The Default animation is "Define Trajectory Curves" type. To create
a "Define Key Frames" type animation, the user needs to select
"Define Key Frames" prior to selecting Add/Copy when creating a new
animation.
Returns
0 = Success
-1 = Unable to find data for "animation_name"
-2 = General error creating MPEG data
not -1,-2, 0 = Error code
Standard UF Error Codes
Environment
Internal and External
History
Original release was in V13.0.
Required License(s)
gateway
int UF_DISP_create_animation
(
char * filename,
char * animation_name,
int first_frame,
int last_frame
)
char * | filename | Input | Name of output file for MPEG data |
char * | animation_name | Input | Name of a Key Frame camera pan in the part |
int | first_frame | Input | Initial frame to generate (usually 0) |
int | last_frame | Input | Final frame to generate |
UF_DISP_create_framed_image (view source)
Defined in: uf_disp_ugopenint.h
Overview
Creates an image file with the file type and rectangular frame you
specify using the image currently displayed in the graphics window.
Export a PNG/JPEG/TIFF/GIF/XWD/BMP full window or rectangular area image
Full window image: set width and height to zero
Rectangular area image: set width, height greater than zero and set
upper left point window coordinate
Return
Return code:
= 0 No error
= not 0 Error code, including:
UF_DISP_err_failed_to_create_image_file
Standard UF error codes
Environment
Internal
History
Original release was in V15.0.
Required License(s)
gateway
int UF_DISP_create_framed_image
(
char* filename,
UF_DISP_image_format_t format,
UF_DISP_background_color_t color,
int upper_left_corner [ 2 ] ,
int width,
int height
)
char* | filename | Input | Name of output image file |
UF_DISP_image_format_t | format | Input | Image type to produce: UF_DISP_PNG UF_DISP_JPEG UF_DISP_TIFF UF_DISP_COMPRESSED_TIFF UF_DISP_GIF UF_DISP_XWD (Only on UNIX workstations) UF_DISP_BMP (Only on Windows workstations) |
UF_DISP_background_color_t | color | Input | Back ground color: UF_DISP_ORIGINAL - original background color UF_DISP_WHITE - white background color. |
int | upper_left_corner [ 2 ] | Input | The Image's upper left corner in the window. Set both x and y to 0 (zero) for a full screen image. upper_left_corner[0] = x position upper_left_corner[1] = y position |
int | width | Input | Image width in pixels. Set to 0 (zero) for full screen image. |
int | height | Input | Image height in pixels. Set to 0 (zero) for full screen image. |
UF_DISP_create_image (view source)
Defined in: uf_disp_ugopenint.h
Overview
Export a PNG/JPEG/TIFF/GIF/XWD/BMP full window area image
Creates an image file with the file type you specify using the image
currently displayed in the graphics window.
Return
Return code:
= 0 No error
= not 0 Error code, including:
UF_DISP_err_failed_to_create_image_file
Standard UF error codes
Environment
Internal
See Also
History
Original release was in V13.0.
Required License(s)
gateway
int UF_DISP_create_image
(
char* filename,
UF_DISP_image_format_t format,
UF_DISP_background_color_t color
)
char* | filename | Input | Name of output image file |
UF_DISP_image_format_t | format | Input | Image type to produce: UF_DISP_PNG UF_DISP_JPEG UF_DISP_TIFF UF_DISP_COMPRESSED_TIFF UF_DISP_GIF UF_DISP_XWD (Only on UNIX workstations) UF_DISP_BMP (Only on Windows workstations) |
UF_DISP_background_color_t | color | Input | Back ground color: UF_DISP_ORIGINAL UF_DISP_WHITE |
UF_DISP_deactivate_grid (view source)
Defined in: uf_disp.h
Overview
This is mainly called when existing from a 'task' environment (eg. Sketcher)
This causes the grid to be removed from display. In general, if switching
from one application to another this call is not necessary because the DSS
subsystem manages all this. However, in a task environment, existing the
environment doesn't always cause display regeneration. Therefore, it is a
good 'house keeping' practice to call this when another grid is expected to
be restored when existing from the current task environment.
product_context - either UF_DISP_SKETCH_GRID for sketcher application,
or UF_DISP_DRAWING_GRID for drawing,
or UF_DISP_SHED_GRID for True Shading display,
or UF_DISP_MODEL_GRID for others (or default).
restore_prev_context_grid - TRUE to assure a proper display regeneration
FALSE, if you don't care
Environment
Internal and External
See Also
History
Originally released in V19.0
Required License(s)
gateway
void UF_DISP_deactivate_grid
(
UF_DISP_grid_context_t product_context,
logical restore_prev_context_grid
)
UF_DISP_grid_context_t | product_context | Input | either UF_DISP_SKETCH_GRID or UF_DISP_DRAWING_GRID or UF_DISP_MODEL_GRID or UF_DISP_SHED_GRID |
logical | restore_prev_context_grid | Input | either TRUE or FALSE |
UF_DISP_delete_material (view source)
Defined in: uf_disp.h
Overview
This function deletes the material specified by the material_tag.
This function supports deletion of both types of materials (Iray+ and Author).
Environment
Internal and external
See Also
History
This function is created for NX3 QRM.
Required License(s)
gateway
int UF_DISP_delete_material
(
const tag_t material_tag
)
const tag_t | material_tag | Input | The tag of material to be deleted |
UF_DISP_display_arc (view source)
Defined in: uf_disp.h
Overview
Displays a User Defined Object arc. The arc is drawn from the start
angle to the end angle in a counter clockwise manner. This routine
may only be called from a UDO registered callback routine. The
context argument passed into this routine will be passed from NX
to the UDO callback routine.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_DISP_display_arc
(
double matrix [ 9 ] ,
double start_angle,
double end_angle,
double arc_center [ 3 ] ,
double radius,
void * context
)
double | matrix [ 9 ] | Input | A matrix for the CSYS in which the arc exists. Use UF_MTX3_initialize to create a matrix from X and Y vectors |
double | start_angle | Input | Start angle expressed in radians |
double | end_angle | Input | End angle expressed in radians. The start angle must be less than the end angle and the difference between the two must be less than 2 PI |
double | arc_center [ 3 ] | Input | Coordinates in arc coordinates system CSYS |
double | radius | Input | Radius from the arc_center |
void * | context | Input / Output | A private context pointer obtained from the callback |
UF_DISP_display_circle (view source)
Defined in: uf_disp.h
Overview
Displays a User Defined Object circle which can be solid filled. This
routine may only be called from a UDO registered callback routine. The
context argument passed into this routine will be passed from NX
to the UDO callback routine.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_DISP_display_circle
(
double matrix [ 9 ] ,
double circle_center [ 3 ] ,
double radius,
logical filled,
void * context
)
double | matrix [ 9 ] | Input | A matrix for the CSYS in which the circle exists. Use UF_MTX3_initialize to create a matrix from X and Y vectors. |
double | circle_center [ 3 ] | Input | Circle's center coordinates (x, y, and z) from the CSYS in which the circle exists (see the matrix[9] argument). |
double | radius | Input | Radius from the circle_center |
logical | filled | Input | TRUE = Solid fill the circle's interior FALSE = Circle's interior not filled |
void * | context | Input / Output | A private context pointer obtained from the callback. |
UF_DISP_display_facets (view source)
Defined in: uf_disp.h
Overview
Displays User Defined Object facets. This routine may only be called from a
UDO registered callback routine. The context argument passed into this
routine will be passed from NX to the UDO callback routine.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_DISP_display_facets
(
UF_DISP_facet_p_t facets,
int num_vertices,
int num_facets,
UF_DISP_facet_type_t type_of_facet,
void * context
)
UF_DISP_facet_p_t | facets | Input | An array of facets. |
int | num_vertices | Input | The number of vertices in one facet. |
int | num_facets | Input | The number of facets in the facet array. |
UF_DISP_facet_type_t | type_of_facet | Input | The format of the facet in the facet array. |
void * | context | Input / Output | A private context pointer obtained from the callback. |
UF_DISP_display_ogp_arc (view source)
Defined in: uf_disp_ugopenint.h
Overview
This function defines an arc to be rendered in the specified view. The
"ogp" in the name indicates that the arc will be drawn as an Overlay
Graphics primitive (please see the Overview to this section); as such, it
neither creates, nor is directly associated with, an NX object.
The arc is drawn in a positive angular direction ("counterclockwise")
from the start angle to the end angle.
The orientation matrix must be ortho-normal. (If necessary, use
UF_MTX3_initialize to create the matrix from X and Y vectors.)
This function returns an error if the absolute value of the difference
between the start and end angle is greater than two pi (plus the system
tolerance). An error is also returned if the start angle is greater than
the end angle.
UF_DISP_display_ogp_ functions are intended to be used
exclusively from motion callback functions. Please see the discussion
and example provided with UF_UI_specify_screen_position.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_DISP_display_ogp_arc
(
tag_t view_tag,
double orientation [ 9 ] ,
double start_angle,
double end_angle,
double center [ 3 ] ,
double radius
)
tag_t | view_tag | Input | Tag of the view in which the arc is to be rendered |
double | orientation [ 9 ] | Input | The rotation matrix of the arc (relative to the Work Part Absolute Coordinate System). The matrix must be ortho-normal. If necessary, use UF_MTX3_initialize to create the matrix from X and Y vectors. |
double | start_angle | Input | Start angle in radians; the zero degree vector is the positive x-axis of the space described by the orientation matrix. |
double | end_angle | Input | End angle in radians; the zero degree vector is the positive x-axis of the space described by the orientation matrix. |
double | center [ 3 ] | Input | The arc center in the coordinate system of the arc (as defined by "orientation" above). |
double | radius | Input | The radius of the arc (Work Part Absolute units) |
UF_DISP_display_ogp_circle (view source)
Defined in: uf_disp_ugopenint.h
Overview
This function defines a circle to be rendered in the specified view.
The "ogp" in the name indicates that the arc will be drawn as an
Overlay Graphics primitive (please see the Overview to this section); as
such, it neither creates, nor is directly associated with, an NX
object. The orientation matrix must be ortho-normal. (If necessary, use
UF_MTX3_initialize to create the matrix from X and Y vectors.)
UF_DISP_display_ogp_ functions are intended to be used
exclusively from motion callback functions. Please see the discussion
and example provided with UF_UI_specify_screen_position.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_DISP_display_ogp_circle
(
tag_t view_tag,
double orientation [ 9 ] ,
double center [ 3 ] ,
double radius
)
tag_t | view_tag | Input | Tag of the view in which the circle is to be rendered |
double | orientation [ 9 ] | Input | The rotation matrix of the circle (relative to the Work Part Absolute Coordinate System). The matrix must be ortho-normal. If necessary, use UF_MTX3_initialize to create the matrix from X and Y vectors. |
double | center [ 3 ] | Input | The circle center in the coordinate system of the arc (as defined by "orientation" above). |
double | radius | Input | The radius of the circle (Work Part Absolute units) |
UF_DISP_display_ogp_line (view source)
Defined in: uf_disp_ugopenint.h
Overview
This function defines a simple line to be rendered in the specified
view. The "ogp" in the name indicates that the line is drawn as an
Overlay Graphics primitive (please see the Overview to this section); as
such, it neither creates, nor is directly associated with, an NX
object. UF_DISP_display_ogp_ functions are intended to be used
exclusively from motion callback functions. Please see the discussion
and example provided with UF_UI_specify_screen_position.
Environment
Internal Only
See Also
Required License(s)
gateway
int UF_DISP_display_ogp_line
(
tag_t view_tag,
double pos1 [ 3 ] ,
double pos2 [ 3 ]
)
tag_t | view_tag | Input | Tag of the view in which the line is to be rendered |
double | pos1 [ 3 ] | Input | 1st endpoint (Work Part Abs Coords) |
double | pos2 [ 3 ] | Input | 2nd endpoint (Work Part Abs Coords) |
UF_DISP_display_ogp_polyline (view source)
Defined in: uf_disp_ugopenint.h
Overview
This function defines a polyline to be rendered in the specified view.
The "ogp" in the name indicates that the polyline will be drawn as an
Overlay Graphics primitive (please see the Overview to this section); as
such, it neither creates, nor is directly associated with, an NX
object. UF_DISP_display_ogp_ functions are intended to be used
exclusively from motion callback functions. Please see the discussion
and example provided with UF_UI_specify_screen_position.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_DISP_display_ogp_polyline
(
tag_t view_tag,
double pos_array [ ] [ 3 ] ,
int pos_count
)
tag_t | view_tag | Input | Tag of the view in which the polyline is to be rendered |
double | pos_array [ ] [ 3 ] | Input | Array of positions [pos_count][3] each position is an (x,y,z) triplet in Work Part Absolute Coordinates. |
int | pos_count | Input | count of positions in pos_array |
UF_DISP_display_points (view source)
Defined in: uf_disp.h
Overview
Displays User Defined Object points. This routine may only be called from
a UDO registered callback routine. The context argument passed into this
routine will be passed from NX to the UDO callback routine.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_DISP_display_points
(
double * points,
int num_points,
UF_DISP_poly_marker_t marker_type,
void * context
)
double * | points | Input | num_points An array of point coordinates. |
int | num_points | Input | The number of points in the points array. |
UF_DISP_poly_marker_t | marker_type | Input | The type of marker to be displayed. |
void * | context | Input / Output | A private context pointer obtained from the callback. |
UF_DISP_display_polygon (view source)
Defined in: uf_disp.h
Overview
Displays a closed User Defined Object polygon and may be solid
filled. The polygon must be planar and convex when using the filled option.
This routine may only be called from a UDO registered callback routine.
The context argument passed into this routine will be passed from
NX to the UDO callback routine.
NOTE: A polygon is convex if a line joining any two interior
points of the polygon lies completely inside the polygon
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_DISP_display_polygon
(
double * points,
int num_points,
logical filled,
void * context
)
double * | points | Input | num_points An array of coordinates resulting in a closed polygon. |
int | num_points | Input | The number of points in the points array. |
logical | filled | Input | TRUE = Solid fill polygon's interior. FALSE = Do not fill polygon's interior |
void * | context | Input / Output | A private context pointer obtained from the callback. |
UF_DISP_display_polyline (view source)
Defined in: uf_disp.h
Overview
Displays a User Defined Object polyline which is a connected set of
line segments. This routine may only be called from a UDO registered
callback routine. The context argument passed into this routine will be
passed from NX to the UDO callback routine.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_DISP_display_polyline
(
double * poly_points,
int num_points,
void * context
)
double * | poly_points | Input | An array of absolute coordinates which represent a connected set of line segments. |
int | num_points | Input | The number of points in the poly_points array. |
void * | context | Input / Output | A private context pointer obtained from the callback. |
UF_DISP_display_rpo_dimensions (view source)
Defined in: uf_disp_ugopenint.h
Overview
Displays all or some rpo dimensions which belong to the specified
feature. The dimensions are specified indirectly by an array of
expression tags. If the count of the array is -1 then the array is
ignored and all rpo dimensions of the feature are displayed. If the
count is 0 then nothing is displayed. The display is temporary and can
be removed by a display refresh operation. The background color can
also be used to erase the dimensions but it may leave gaps on the
display. There must be a part loaded when this function is called. Any
specified expression which does not tie directly to a dimension of the
specified feature is considered invalid.
Environment
Internal
Required License(s)
gateway
int UF_DISP_display_rpo_dimensions
(
tag_t feature_tag,
int exp_count,
tag_t* exp_tags,
int view_option,
int color_option,
int color
)
tag_t | feature_tag | Input | Tag of the feature to which the dimensions belong |
int | exp_count | Input | >=0 = Number of expression tags in exp_tags array -1 = all rpo dimensions of the feature |
tag_t* | exp_tags | Input | exp_count Array of expression tags of which the dimensions need to be displayed.(is ignored if count <=0) |
int | view_option | Input | Option for the view, the constants are in uf_disp.h: UF_DISP_ALL_VIEWS_BUT_DRAWING UF_DISP_VIEW_OF_LAST_CURSOR UF_DISP_ALL_ACTIVE_VIEWS UF_DISP_WORK_VIEW_ONLY |
int | color_option | Input | Option for the color, the constants are in uf_disp.h: UF_DISP_USE_SYSTEM_COLOR UF_DISP_USE_BACKGROUND_COLOR UF_DISP_USE_ORIGINAL_COLOR UF_DISP_USE_SPECIFIED_COLOR |
int | color | Input | Color used to display the dimensions if color_option= UF_DISP_USE_SPECIFIED_COLOR. Use the color constants listed in uf_obj.h. |
UF_DISP_display_sket_dimensions (view source)
Defined in: uf_disp_ugopenint.h
Overview
Displays all or some sketch dimensions which belong to a specified
sketch. The dimensions are specified indirectly by an array of
expression tags. If the count of the array is -1 then the array is
ignored and all dimensions of the sketch are displayed. If the count is
0 then nothing is displayed. The display is temporary and can be
removed by a display refresh operation. The background color can
also be used to erase the dimensions but it may leave gaps on the
display. There must be a part loaded when this function is called. Any
specified expression which does not tie directly to a dimension of the
specified feature is considered invalid.
Environment
Internal
Required License(s)
gateway
int UF_DISP_display_sket_dimensions
(
tag_t sketch_tag,
int exp_count,
tag_t* exp_tags,
int view_option,
int color_option,
int color
)
tag_t | sketch_tag | Input | Tag of the sketch to which the dimensions belong |
int | exp_count | Input | >= 0 = Number of expression tags in exp_tags array -1 = all dimensions of the sketch |
tag_t* | exp_tags | Input | exp_count Array of expression tags of which the dimensions need to be displayed. (is ignored if count <= 0) |
int | view_option | Input | Option for the view, the constants are in uf_disp.h: UF_DISP_ALL_VIEWS_BUT_DRAWING UF_DISP_VIEW_OF_LAST_CURSOR UF_DISP_ALL_ACTIVE_VIEWS UF_DISP_WORK_VIEW_ONLY |
int | color_option | Input | Option for the color, the constants are in uf_disp.h: UF_DISP_USE_SYSTEM_COLOR UF_DISP_USE_BACKGROUND_COLOR UF_DISP_USE_ORIGINAL_COLOR UF_DISP_USE_SPECIFIED_COLOR |
int | color | Input | Color used to display the dimensions if color_option= UF_DISP_USE_SPECIFIED_COLOR. Use the color constants listed in uf_obj.h. |
UF_DISP_display_temporary_arc (view source)
Defined in: uf_disp.h
Overview
Displays a temporary arc. A display refresh erases temporary
geometry. The start angle must be less than the end angle and the
absolute value of the difference must be less than two pi.
Environment
Internal
See Also
Required License(s)
gateway
int UF_DISP_display_temporary_arc
(
tag_t view_tag,
UF_DISP_view_type_t which_views,
double matrix [ 9 ] ,
double start_angle,
double end_angle,
double arc_center [ 3 ] ,
double radius,
UF_OBJ_disp_props_t * attrib
)
tag_t | view_tag | Input | The tag of the view in which to display the temporary arc. |
UF_DISP_view_type_t | which_views | Input | The view mode to use. |
double | matrix [ 9 ] | Input | A matrix for the CSYS in which the arc exists. Use UF_MTX3_initialize to create a matrix from X and Y vectors. |
double | start_angle | Input | Start angle in radians |
double | end_angle | Input | End angle in radians. |
double | arc_center [ 3 ] | Input | Coordinates are with respect to the CSYS of the matrix in the work part. |
double | radius | Input | Radius from the arc center. |
UF_OBJ_disp_props_t * | attrib | Input | The color, font, and width elements of the structure should be set to: attrib->color = color index attrib->font = 1 for solid 2-7, user defined 0 use system default attrib->line_width = line width values in uf_obj.h -1 use the default width |
UF_DISP_display_temporary_line (view source)
Defined in: uf_disp.h
Overview
Displays a temporary line. A display refresh erases temporary geometry.
Environment
Internal
See Also
Required License(s)
gateway
int UF_DISP_display_temporary_line
(
tag_t view_tag,
UF_DISP_view_type_t which_views,
double start_line [ 3 ] ,
double end_line [ 3 ] ,
UF_OBJ_disp_props_t * attrib
)
tag_t | view_tag | Input | The tag of the view in which the temporary line is to display. |
UF_DISP_view_type_t | which_views | Input | The view mode to use |
double | start_line [ 3 ] | Input | The absolute coordinates of the start point of the line. |
double | end_line [ 3 ] | Input | The absolute coordinates of the work part of the end point of the line. |
UF_OBJ_disp_props_t * | attrib | Input | The color, font, and width elements of the structure should be set to: attrib->color = color index attrib->font = 1 for solid 2-7, user defined 0 use system default attrib->line_width = line width values in uf_obj.h -1 use the default width |
UF_DISP_display_temporary_point (view source)
Defined in: uf_disp.h
Overview
Displays a temporary marker. A display refresh erases temporary
geometry.
Environment
Internal
See Also
Required License(s)
gateway
int UF_DISP_display_temporary_point
(
tag_t view_tag,
UF_DISP_view_type_t which_views,
double markerpos [ 3 ] ,
UF_OBJ_disp_props_t * color,
UF_DISP_poly_marker_t marker_type
)
tag_t | view_tag | Input | The tag of the view in which to display the temporary maker. |
UF_DISP_view_type_t | which_views | Input | The view mode to use. |
double | markerpos [ 3 ] | Input | The marker position in absolute coordinates of the work part |
UF_OBJ_disp_props_t * | color | Input | The color element of the structure. All other elements of the structure are ignored. If color->color = 0, then the system default color is used. |
UF_DISP_poly_marker_t | marker_type | Input | The marker type |
UF_DISP_display_temporary_text (view source)
Defined in: uf_disp.h
Overview
Displays temporary text. A display refresh erases temporary text. The
text is entered in an array and each newline is specified by entering
the '\n' character in the text. The text must be null terminated.
The text is displayed parallel to the screen. The size of the text
is in the given size (or the system default size) on the screen, and
remains at the same size regardless of the view scale.
Environment
Internal
See Also
History
V18.0 Add comments.
Required License(s)
gateway
int UF_DISP_display_temporary_text
(
tag_t view_tag,
UF_DISP_view_type_t which_views,
char text [ ] ,
double text_coord [ 3 ] ,
UF_DISP_text_ref_t ref_point,
UF_OBJ_disp_props_t * color,
double char_size,
int hardware
)
tag_t | view_tag | Input | The tag of the view in which to display the temporary text. |
UF_DISP_view_type_t | which_views | Input | The view mode to use. |
char | text [ ] | Input | Lines of text |
double | text_coord [ 3 ] | Input | Position of text box reference point in absolute coordinates of the displayed part. |
UF_DISP_text_ref_t | ref_point | Input | Reference point of text box |
UF_OBJ_disp_props_t * | color | Input | The color element of the structure. All other elements of the structure are ignored. If color->color = 0, then the system default color is used. |
double | char_size | Input | The character size in part units (Metric or inches). Used only if software text is used. If <= 0, then uses system default. |
int | hardware | Input | hardware/software flag: 0 = Use hardware font 1 = Use software font |
UF_DISP_display_text (view source)
Defined in: uf_disp.h
Overview
Displays User Defined Object text which rotates with the view. The
text is entered in an array and each newline is specified by entering
the '\n' character in the text. The text must be null terminated. For
example, "Hello \n World!". This routine may only be called from a
UDO registered callback routine. The context argument passed into this
routine will be passed from NX to the UDO callback routine.
The text is drawn using the character size found in the Annotations
Preference dialog, under Lettering, General. This size may be changed
by UF_DRF_set_preferences, setting mpr[4] to the desired size.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_DISP_display_text
(
char text [ ] ,
double text_coord [ 3 ] ,
UF_DISP_text_ref_t ref_point,
void * context
)
char | text [ ] | Input | Lines of text |
double | text_coord [ 3 ] | Input | Position of text box reference point in absolute coordinates. |
UF_DISP_text_ref_t | ref_point | Input | Reference point of text box |
void * | context | Input / Output | A private context pointer obtained from the callback. |
UF_DISP_export_windows_metafile (view source)
Defined in: uf_disp.h
Overview
Creates a Windows Enhanced Metafile of the image in the
NX graphics window. This function is available only
on Windows NT. Calling it on any other platform will result
in an error being returned. There are options to export the
Enhanced Metafile to the clipboard or to a device context. This is
similar to exporting a plot file or a CGM file of the current display.
Any views which are in Shaded, Partially Shaded, or in Face Analysis
mode are treated as if they were in Wireframe mode.
The Enhanced Metafile will be created using part colors and a single
(standard thin) line width value.
The size of the image in the generated Enhanced Metafile is the same
as that of the current graphics window. Therefore, you may wish to
resize the graphics window to the desired size prior to invoking this
function. When in External mode, the size of the graphics window is
the size the last time the part was saved.
The output Enhanced Metafile does not include the Work Coordinate
System, the grid, nor any temporary display.
You can only use the UF_DISP_WMF_TO_CLIPBOARD option
when in Internal mode. If you use this option in External mode, this
function returns an error code.
Environment
Internal and External
History
Original release was in V14.0.
Required License(s)
gateway
int UF_DISP_export_windows_metafile
(
UF_DISP_wmf_output_t output_type,
char * file_spec
)
UF_DISP_wmf_output_t | output_type | Input | Specifies where the output Enhanced Metafile should be written: UF_DISP_WMF_TO_CLIPBOARD writes directly to the Windows clipboard. This is not available in external NX Open programs. UF_DISP_WMF_TO_FILE uses the following file_spec to output the metafile data to. |
char * | file_spec | Input | The file specification of the file to create. This parameter is used only when the output_type is UF_DISP_WMF_TO_FILE. This file specification must be at most MAX_FSPEC_SIZE characters. |
UF_DISP_get_conehead_attrb (view source)
Defined in: uf_disp_ugopenint.h
Overview
Gets the current attribute settings with which the conehead vector
displays by a call to UF_DISP_conehead. You can then obtain the
values of the fields of the UF_DISP_conehead_attrb_s structure (see
the example below).
Return
void
Environment
Internal
See Also
Required License(s)
gateway
void UF_DISP_get_conehead_attrb
(
UF_DISP_conehead_attrb_s * attributes
)
UF_DISP_j3d_free_geometry (view source)
Defined in: uf_disp.h
Overview
Cleans up the data returned from UF_DISP_j3d_geometry
Environment
Internal and External
See Also
None
History
None
Required License(s)
gateway
int UF_DISP_j3d_free_geometry
(
int num_entities,
UF_DISP_j3d_entity_p_t entity_list
)
UF_DISP_j3d_geometry (view source)
Defined in: uf_disp.h
Overview
Creates polygon and vector data for the geometry of a part file.
The output polygon data is triangle strips for polygon data and
vectors for curves.
wireframe - a boolean value where if the value is 1, then solids
and sheets will be returned as wireframe vector data
for the edges of the body. If the value is 0, then
solids and sheets will be returned as triangle strip
polygon data.
num_entities - returns the number of elements in the entity_list
entitiy_list - An array of display data structures
Environment
Internal and External
See Also
None
History
None
Required License(s)
gateway
int UF_DISP_j3d_geometry
(
int wireframe,
int * num_entities,
UF_DISP_j3d_entity_p_t * entity_list
)
UF_DISP_labeled_conehead (view source)
Defined in: uf_disp_ugopenint.h
Overview
Displays a temporary, labeled conehead vector with either the base of
the staff, the arrow tip or the base of the arrowhead at the reference
point in the specified view(s). A label will be placed at the cone's tip.
Environment
Internal
Return
void
Required License(s)
gateway
void UF_DISP_labeled_conehead
(
int display_flag,
double coord [ 3 ] ,
double vector [ 3 ] ,
int anchor_flag,
char * label
)
int | display_flag | Input | Display views to draw the conehead vector in. UF_DISP_ALL_VIEWS_BUT_DRAWING UF_DISP_VIEW_OF_LAST_CURSOR UF_DISP_ALL_ACTIVE_VIEWS UF_DISP_WORK_VIEW_ONLY >0 = View sequence number |
double | coord [ 3 ] | Input | 3D absolute coordinates of anchor or reference point in absolute space. |
double | vector [ 3 ] | Input | 3D vector which gives conehead direction in absolute space. |
int | anchor_flag | Input | Denotes the anchor point's location: 0 = Anchor point at base of staff 1 = Anchor point at tip of arrowhead 2 = Anchor point at base of arrowhead |
char * | label | Input | Labels the conehead at its tip. |
UF_DISP_load_color_table (view source)
Defined in: uf_disp_ugopenint.h
Overview
Downloads the color table to the graphics display, so that all geometry
displayed in the graphics window will now use the current contents of
the Color Table object (of the Display part); this is equivalent to
selecting Apply from the color palette dialog in interactive
NX. There must be a part loaded before calling this function.
Environment
Internal
See Also
Required License(s)
gateway
int UF_DISP_load_color_table
(
void
)
UF_DISP_make_display_up_to_date (view source)
Defined in: uf_disp.h
Overview
Ensures that previously invoked display operations are complete.
Function UF_DISP_make_display_up_to_date should be called only by
NX Open API programs that directly invoke Windows, MFC, or Motif
functions to display dialogs. This function is unneeded when
NX Open dialogs are used.
When NX Open functions perform display operations, the display
operations can be buffered. NX Open dialog logic ensures that
the buffered operations are completed at appropriate times. If
an NX Open API program bypasses NX Open dialog logic, the program
might need to explicitly invoke UF_DISP_make_display_up_to_date
to complete buffered operations. The function should be called
immediately before invoking Windows, MFC, or Motif functions to
display dialogs.
Return
Zero is returned upon successful execution.
Any other return code indicates an error.
Environment
Internal
History
Originally released in V17.0.2
Required License(s)
gateway
int UF_DISP_make_display_up_to_date
(
void
)
UF_DISP_open_LWA_archive_materials_library (view source)
Defined in: uf_disp.h
Overview
This function opens the Lightworks LWA archive material library specified by the input argument lwa_material_library_name
Returns
0 = Success
-1 = Failed to initialize Lightworks session_manager
-2 = Failed to open the specified lwa material archive library file
not -1,-2, 0 = Error code
Standard UF Error Codes
UF_err_program_not_initialized
UF_err_bad_parameter_number_1: problem found with lwa_archive_library_name , file does not exist.
UF_err_part_not_loaded: need to have an opened work part.
This function only supports Author based materials and libraries(lwa).
Environment
Internal and external
See Also
History
This function is created for NX8.5.3
Required License(s)
gateway
int UF_DISP_open_LWA_archive_materials_library
(
const char* lwa_archive_library_name
)
const char* | lwa_archive_library_name | Input | The name including full path of the LWA archive material library to be opened. |
UF_DISP_print_window_ug_image (view source)
Defined in: uf_disp_ugopenint.h
Overview
Prints the contents of the graphics window to the default printer.
This function is available only on Windows workstations and returns
an error if called on a non-Windows workstation.
Environment
Internal
History
Originally released in V16.0.
Second parameter redefined in V18.0.
Required License(s)
gateway
int UF_DISP_print_window_ug_image
(
int format,
int color_usage
)
int | format | Input | Specifies the format of the printed image. 0: A vector-format image is printed. 1: A raster-format (bitmap) image is printed. If only wireframe views are displayed, then a vector-format image is printed even if the format parameter is set to 1. |
int | color_usage | Input | Specifies how color is used in the printed image. 0: If a vector image is printed, line color is determined by the setting of the Black Lines Only option in the File->Print dialog. If a raster image is printed, the image background is the same as the background of the graphics window. 1: If a vector image is printed, line color is determined by the setting of the Black Lines Only option in the File->Print dialog. If a raster image is printed, the image background is white. 2: If a vector image is printed, lines are printed in color (or shades of gray on a monochrome printer). If a raster image is printed, the image background is the same as the background of the graphics window. 3: If a vector image is printed, all lines are printed in black. If a raster image is printed, the image background is white. |
UF_DISP_refresh (view source)
Defined in: uf_disp.h
Overview
Performs an entire display refresh.
Return
void
Environment
Internal
Required License(s)
gateway
void UF_DISP_refresh
(
void
)
UF_DISP_regenerate_display (view source)
Defined in: uf_disp.h
Overview
Regenerates the display.
Environment
Internal
Required License(s)
gateway
int UF_DISP_regenerate_display
(
void
)
UF_DISP_regenerate_view (view source)
Defined in: uf_disp.h
Overview
Regenerates the display of a single view . The view must be currently
displayed. If you specify an inactive view (i.e. a view on a layout or a
drawing which is not displayed), an error occurs. Use
UF_VIEW_ask_tag_of_view_name to find the view_tag.
Environment
Internal
See Also
Required License(s)
gateway
int UF_DISP_regenerate_view
(
tag_t view_tag
)
tag_t | view_tag | Input | The tag of the view to regenerate |
UF_DISP_remove_material_assignment (view source)
Defined in: uf_disp.h
Overview
This function applies "None" material to a geometry identified by the input object tag argument.
This removes all the material texture links to the object.
It does not remove the materials or textures from the part.
Returns
0 = Success
Standard UF Error Codes:
UF_err_program_not_initialized
UF_err_bad_parameter_number_1: problem found with object_tag
UF_err_part_not_loaded
This function aplies to materials of current renderer type.
This means if user is in Iray+ renderer mode, then only materials of Iray+ type will be removed.
Environment
Internal and external
See Also
History
This function is created for NX8.5.3
Required License(s)
gateway
int UF_DISP_remove_material_assignment
(
tag_t object_tag
)
tag_t | object_tag | Input | The tag of the geometry object to remove the material from. |
UF_DISP_reset_conehead_attrb (view source)
Defined in: uf_disp_ugopenint.h
Overview
Resets the conehead attributes to the default values.
Return
void
Environment
Internal
Required License(s)
gateway
void UF_DISP_reset_conehead_attrb
(
void
)
UF_DISP_set_color (view source)
Defined in: uf_disp.h
Overview
Modifies the name and values of the specified color in the Color Table
object (CTO) of the Display part. The color values are given using
the specified color model.
Note that the maximum value permitted for clr_num is the number of
records presently in the CTO, minus 1. The number of CTO records
may be obtained by calling UF_DISP_ask_color_count. There must be
a part loaded when this function is called.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_DISP_set_color
(
int clr_num,
int clr_model,
char * clr_name,
double clr_values [ 3 ]
)
int | clr_num | Input | The number of the color whose name and value are to be returned; Range: 0 .. (# color records in CTO) - 1 Note: 0 is for the background color |
int | clr_model | Input | The color model of the values in clr_values: UF_DISP_rgb_model UF_DISP_hsv_model UF_DISP_hls_model |
char * | clr_name | Input | The name of the color; the character array must be null terminated. The length must not exceed UF_DISP_MAX_NAME_SIZE, as defined in uf_disp.h ignored if clr_num == 0 |
double | clr_values [ 3 ] | Input | Three doubles representing the color, where the meaning and range of each value depends on the color model specified: rgb: clr_values[0]: 0.0 <= red <= 1.0 clr_values[1]: 0.0 <=green <= 1.0 clr_values[2]: 0.0 <= blue <= 1.0 hsv: clr_values[0]: 0.0 <= hue <= 360.0 clr_values[1]: 0.0 <= saturation <= 1.0 clr_values[2]: 0.0 <= value <= 1.0 hls: clr_values[0]: 0.0 <= hue <= 360.0 clr_values[2]: 0.0 <= light <= 1.0 clr_values[1]: 0.0 <= saturation <= 1.0 |
UF_DISP_set_conehead_attrb (view source)
Defined in: uf_disp_ugopenint.h
Overview
Allows changes to the current attribute settings with which the
conehead vector displays by a call to UF_DISP_conehead.
Note that it is best to get the current attribute settings and then
adjust the ones you need, as shown in the example.
Return
void
Environment
Internal
See Also
Required License(s)
gateway
void UF_DISP_set_conehead_attrb
(
UF_DISP_conehead_attrb_s * attributes
)
UF_DISP_set_display (view source)
Defined in: uf_disp.h
Overview
Sets the display status. You can use UF_DISP_set_display to turn
off the graphics display before executing a long series of graphics
intensive operations such as manipulations of views, layouts, or
drawings. You must call UF_DISP_regenerate_display to update the
display after turning it back on.
Note that there are limitations to this function in conjunction with
layout and drawing changes. If you open a layout or drawing, the
display will change to show the outlines of the views in the layout
or drawing, even though the suppress state is enabled; the contents
of the views will not be shown however.
Environment
Internal
Required License(s)
gateway
int UF_DISP_set_display
(
int display_code
)
int | display_code | Input | display code: UF_DISP_SUPPRESS_DISPLAY- set display off UF_DISP_UNSUPPRESS_DISPLAY- set display on |
UF_DISP_set_drawing_display (view source)
Defined in: uf_disp.h
Overview
Update the data that affects drawing monochrome display.
The routine UF_DISP_ask_drawing_display MUST be called to
populate the data structure, before this routine is called.
Please reference ufd_disp.c to review a sample execution of this function.
Return
UF_err_program_not_initialized, UF_err_bad_parameter_number_1
Environment
Internal and External
See Also
History
None
Required License(s)
gateway
int UF_DISP_set_drawing_display
(
UF_DISP_drawing_display_data_p_t drawing_display
)
UF_DISP_set_grid_parameters (view source)
Defined in: uf_disp.h
Overview
Sets up the information for the grid in the designated application
context. Any field not set will have a default value provided.
product_context - either UF_DISP_SKETCH_GRID for sketcher application,
or UF_DISP_DRAWING_GRID for drawing,
or UF_DISP_SHED_GRID for True Shading display,
or UF_DISP_MODEL_GRID for others (or default).
Environment
Internal and External
See Also
History
Originally released in V19.0
Required License(s)
gateway
void UF_DISP_set_grid_parameters
(
UF_DISP_grid_context_t product_context,
UF_DISP_grid_p_t input_grid
)
UF_DISP_grid_context_t | product_context | Input | either UF_DISP_SKETCH_GRID or UF_DISP_DRAWING_GRID or UF_DISP_MODEL_GRID or UF_DISP_SHED_GRID |
UF_DISP_grid_p_t | input_grid | Input | a polulated grid structure |
UF_DISP_set_highlight (view source)
Defined in: uf_disp.h
Overview
Turns object/feature highlight on or off.
Environment
Internal
Required License(s)
gateway
int UF_DISP_set_highlight
(
tag_t object_id,
int action_switch
)
tag_t | object_id | Input | Object/Feature identifier |
int | action_switch | Input | Action Switch 0 = Turn Highlight Off 1 = Turn Highlight On |
UF_DISP_set_highlights (view source)
Defined in: uf_disp.h
Overview
Turns object/feature highlight on or off.
Environment
Internal
History
This function was first released in NX 7.5.5
Required License(s)
gateway
int UF_DISP_set_highlights
(
int object_count,
tag_p_t object_list,
int action_switch
)
int | object_count | Input | The number of objects in the object_list |
tag_p_t | object_list | Input | object list to set highlights |
int | action_switch | Input | Action Switch 0 = Turn Highlight Off 1 = Turn Highlight On |
UF_DISP_set_model_bounds (view source)
Defined in: uf_disp.h
Overview
Stores the given model bounds into the one and only model bounds
object for the work part. The given tag must be that of the model
bounds object.
NOTE: This function is of limited value for most NX Open API
application developers. It is intended to be used by certain NX
applications such as translators.
Environment
Internal and External
Required License(s)
gateway
int UF_DISP_set_model_bounds
(
const tag_t model_bounds_object,
const double model_bounds [ 6 ]
)
const tag_t | model_bounds_object | Input | The tag of the Model Bounds object of the work part. You will have received this from a prior call to UF_DISP_ask_model_bounds_tag |
const double | model_bounds [ 6 ] | Input | The model bounds of the current work part. The six values are (Minimum_X, Maximum_X, Minimum_Y, Maximum_Y, Minimum_Z, Maximum_Z). You probably have determined these bounds in a prior call to UF_DISP_compute_model_bounds. |
UF_DISP_set_name_display_status (view source)
Defined in: uf_disp.h
Overview
Sets the name display status for objects. Names are created with
UF_OBJ_set_name, and the location where they are displayed is set with
UF_OBJ_set_name_origin.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_DISP_set_name_display_status
(
const int new_status
)
const int | new_status | Input | Name display status: UF_DISP_NAME_DISPLAY_OFF UF_DISP_NAME_DISPLAY_ON |
UF_DISP_set_name_view_status (view source)
Defined in: uf_disp.h
Overview
Sets the name display view status. The constant
UF_DISP_NAMES_IN_VIEW_OF_DEFN is the view which is the work
view when the object is defined.
Environment
Internal and External
Required License(s)
gateway
int UF_DISP_set_name_view_status
(
const int new_status
)
const int | new_status | Input | Name display view status: UF_DISP_NAMES_IN_WORK_VIEW UF_DISP_NAMES_IN_VIEW_OF_DEFN UF_DISP_NAMES_IN_ALL_VIEWS |
UF_DISP_set_srfanl_params (view source)
Defined in: uf_disp.h
Overview
Sets the face analysis display parameters. This routine uses a pointer
to the structure UF_DISP_srfanl_data_s.
Environment
Internal
See Also
Required License(s)
gateway
int UF_DISP_set_srfanl_params
(
UF_DISP_srfanl_data_t * params
)
UF_DISP_set_system_parameters (view source)
Defined in: uf_disp.h
Overview
Environment
Internal and External
History
V12.0 light_source_angles field removed from the structure
V13.0 Added show_shaded_face_edges and hidden_shaded_face_edges
to the structure
V19.0 Added fields use_face_edges_color
face_edges_color
hidden_geometry_color
random_color_displayed
random_color_object_type
Required License(s)
gateway
int UF_DISP_set_system_parameters
(
UF_DISP_system_params_p_t system_parameters
)
UF_DISP_set_texture_space_info (view source)
Defined in: uf_disp.h
Overview
This function allows user to set new texture space information of the material.
This function only supports Author based materials.
Environment
Internal and External
See Also
History
This function is created for NX3 QRM.
Required License(s)
gateway
int UF_DISP_set_texture_space_info
(
const tag_t material_tag,
UF_DISP_texture_space_info_t * ts_info_ptr
)
UF_DISP_set_work_plane_emphasis (view source)
Defined in: uf_disp.h
Overview
Sets work plane emphasis on or off. When work plane emphasis is on,
objects that do not lie on the work plane appear de-emphasized, in
which the object color is blended with the De-emphasis Blend Color
according to the De-emphasis Blend Percentage. A de-emphasized object
is unselectable unless the work plane emphasis selection filter is
overridden. Work plane emphasis is a session dependent value; it is
not saved with any part.
Environment
Internal and External
See Also
History
Original release was in V13.0.
Required License(s)
gateway
int UF_DISP_set_work_plane_emphasis
(
int emphasis
)
int | emphasis | Input | Emphasis setting. Must be either: UF_DISP_WORK_PLANE_EMPHASIS_ON, or UF_DISP_WORK_PLANE_EMPHASIS_OFF |
UF_DISP_set_work_plane_sel (view source)
Defined in: uf_disp.h
Overview
Sets (or unsets) the work plane emphasis selection override.
When work plane emphasis is enabled and the selection override is
set to UF_DISP_SELECT_WORK_DIMMED, no objects are filtered
out of selection because they are off the work plane.
When work plane emphasis is enabled and the selection override is
set to UF_DISP_NO_SELECT_WORK_DIMMED, no objects
dimmed for work plane emphasis are selectable.
When work plane emphasis is disabled, the selection override setting
has no affect although it can be changed. The selection override
setting takes effect once work plane emphasis is enabled.
The work plane emphasis selection override is a session dependent
value; it is not saved with any part.
Environment
Internal and External
See Also
History
Original release was in V13.0.
Required License(s)
gateway
int UF_DISP_set_work_plane_sel
(
int override
)
int | override | Input | Emphasis selection override setting. Must be either: UF_DISP_SELECT_WORK_DIMMED, or UF_DISP_NO_SELECT_WORK_DIMMED |
UF_DISP_update_material_display_of_geometry (view source)
Defined in: uf_disp.h
Overview
This function updates the display of the given geometry objects
in Studio rendering style.
The display of UF_solid_type, UF_solid_face_subtype and UF_faceted_model_type
are updated. All other object types are ignored.
This function supports materials update of current renderer type.
Environment
Internal
See Also
History
This function is created for NX7.5.2 QRM.
Required License(s)
gateway
int UF_DISP_update_material_display_of_geometry
(
const int object_count,
const tag_p_t object_list
)
const int | object_count | Input | The number of objects in the object_list |
const tag_p_t | object_list | Input | The tags of objects with material applied to |