uc5027 (view source)
Defined in: uf_obj.h
Overview
uc5027 read object name -- replaced by UF_OBJ_ask_name
Required License(s)
gateway
int uc5027
(
tag_t np1,
char cr2 [ UF_OBJ_NAME_BUFSIZE ] ,
int * ir3
)
tag_t | np1 | Output | |
char | cr2 [ UF_OBJ_NAME_BUFSIZE ] | | |
int * | ir3 | | |
uc5028 (view source)
Defined in: uf_obj.h
Overview
uc5028 find named object -- replaced by UF_OBJ_cycle_by_name
Required License(s)
gateway
int uc5028
(
const char * cp1,
int ip2,
tag_t * nr3
)
const char * | cp1 | Input | |
int | ip2 | Input | |
tag_t * | nr3 | | |
uc5029 (view source)
Defined in: uf_obj.h
Overview
uc5029 add/modify object name -- replaced by UF_OBJ_set_name
Required License(s)
gateway
int uc5029
(
tag_t np1,
const char * cp2,
int ip3
)
tag_t | np1 | Input | |
const char * | cp2 | | |
int | ip3 | | |
uc502a (view source)
Defined in: uf_obj.h
Overview
uc502a read object font -- NO REPLACEMENT (use
UF_OBJ_ask_display_properties)
Required License(s)
gateway
int uc502a
(
tag_t np1,
char cr2 [ 31 ]
)
tag_t | np1 | Output | |
char | cr2 [ 31 ] | | |
uc502e (view source)
Defined in: uf_obj.h
Overview
uc502e temporarily modify object defaults -- NO REPLACEMENT (use default
creation routines above)
Required License(s)
gateway
int uc502e
(
int ip1,
int ip2,
int ip3,
int ip4,
const char * cp5
)
int | ip1 | | |
int | ip2 | | |
int | ip3 | | |
int | ip4 | Input | |
const char * | cp5 | | |
uc502m (view source)
Defined in: uf_obj.h
Overview
uc502m edit object font -- NO REPLACEMENT (use UF_OBJ_set_font)
Required License(s)
gateway
int uc502m
(
tag_t np1,
const char * cp2
)
tag_t | np1 | Input | |
const char * | cp2 | | |
uc502n (view source)
Defined in: uf_obj.h
Overview
uc502n read part file data and set default object -- NO REPLACEMENT (use
default creation routines
above)
Required License(s)
gateway
int uc502n
(
int * ia1,
int * ia2,
int * ia3,
char ca4 [ UF_OBJ_NAME_BUFSIZE ]
)
int * | ia1 | | |
int * | ia2 | | |
int * | ia3 | Input / Output | |
char | ca4 [ UF_OBJ_NAME_BUFSIZE ] | | |
uc502r (view source)
Defined in: uf_obj.h
Overview
uc502r read current font definition file name -- NO REPLACEMENT
Required License(s)
gateway
int uc502r
(
int ip1,
char ca2 [ MAX_FSPEC_BUFSIZE ]
)
int | ip1 | Input / Output | |
char | ca2 [ MAX_FSPEC_BUFSIZE ] | | |
uc5203 (view source)
Defined in: uf_obj.h
Overview
uc5203 cycle by object name -- replaced by UF_OBJ_cycle_by_name
Required License(s)
gateway
void uc5203
(
tag_t * na1,
const char * cp2,
int ip3
)
tag_t * | na1 | Input | |
const char * | cp2 | | |
int | ip3 | | |
uf5025 (view source)
Defined in: uf_obj.h
Overview
uf5025 read part file data and set default object -- replaced by default
creation routines above
Required License(s)
gateway
void uf5025
(
int * ia1,
int * ia2,
int * ia3,
int * ia4
)
int * | ia1 | | |
int * | ia2 | | |
int * | ia3 | | |
int * | ia4 | | |
uf5026 (view source)
Defined in: uf_obj.h
Overview
uf5026 temporarily modify object defaults -- replaced by default creation
routines above
Required License(s)
gateway
void uf5026
(
const int * ip1,
const int * ip2,
const int * ip3,
const int * ip4,
const int * ip5
)
const int * | ip1 | | |
const int * | ip2 | | |
const int * | ip3 | | |
const int * | ip4 | | |
const int * | ip5 | | |
UF_OBJ_ask_cre_mod_versions (view source)
Defined in: uf_obj.h
Overview
Returns the version of the part in which the given object was created
and the version in which it was last modified. The version numbers
returned are from 1 to the highest version number of the part, unless
there is an error, in which case the version numbers are set to 0. The
UF_PART_<xxxx> routines which deal with part save histories can be
used to obtain information about the versions of a part.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_ask_cre_mod_versions
(
tag_t object,
int * creation_version,
int * lastmod_version
)
tag_t | object | Input | Object Identifier |
int * | creation_version | Output | Object's creation version |
int * | lastmod_version | Output | Object's last modification version |
UF_OBJ_ask_cre_settings (view source)
Defined in: uf_obj.h
Overview
Reads the work part's color, line font, and width object creation
settings for the type and subtype specified. If the type is an invalid
object type or if no object creation settings exist for the type and
subtype combination, then an error is returned. This routine uses the
settings structure UF_OBJ_cre_settings_s .
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_ask_cre_settings
(
const int type,
const int subtype,
const int property,
UF_OBJ_cre_settings_p_t settings
)
const int | type | Input | type to ask settings of |
const int | subtype | Input | Subtype of type to ask settings of |
const int | property | Input | Property of type/subtype to ask settings of |
UF_OBJ_cre_settings_p_t | settings | Output | Color, line font and width object creation settings for the specified type and subtype. |
UF_OBJ_ask_def_cre_settings (view source)
Defined in: uf_obj.h
Overview
Reads the work part's default color, line font, and width object
creation settings. This routine uses the settings structure
UF_OBJ_cre_settings_s.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_ask_def_cre_settings
(
UF_OBJ_cre_settings_p_t settings
)
UF_OBJ_cre_settings_p_t | settings | Output | Default color, line font and width object creation settings for the specified type and subtype. |
UF_OBJ_ask_display_properties (view source)
Defined in: uf_obj.h
Overview
Returns the display properties (layer, color, blank status, line width,
and font) for an object.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_ask_display_properties
(
tag_t object_id,
UF_OBJ_disp_props_p_t disp_props
)
tag_t | object_id | Input | Object identifier of object to query |
UF_OBJ_disp_props_p_t | disp_props | Output | Display properties of object of inquiry |
UF_OBJ_ask_extended_type_and_subtype (view source)
Defined in: uf_obj.h
Overview
Returns the extended object type of a tagged NX object. (extended object types have
values over 256). The majority of these objects are listed in the uf_object_types.h
header file.
In addition to the objects listed in uf_object_types.h, there are other
NX objects uniquely identified by a tag. Among these objects
are expressions and parts. These objects, which are not listed in the
uf_object_types.h header file, produce the type UF_OBJ_EXPR_TYPE and
UF_OBJ_PART_TYPE with a subtype of 0.
The types and subtypes this function returns for expressions
and parts are not useful in any other Open API routines.
These types are provided only to allow you to determine the class of a
NX object through its identifier (i.e. its tag) which can assist
you in determining the other Open API routines that you can use
in conjunction with the object. For a more detailed discussion of
classes of objects and the Open API routines available to these
objects, please see the Open API Programmer's Guide, "The
NX Object Model".
The difference between the type returned by UF_OBJ_ask_type_and_subtype and this routine is,
UF_OBJ_ask_type_and_subtype returns UF_extended_type or UF_extended_displayable_type for
all the extended type objects except for some types like parts and expressions.
Whereas this routine returns the object's real type.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_ask_extended_type_and_subtype
(
tag_t object_id,
int * type,
int * subtype
)
tag_t | object_id | Input | Object identifier of object to query |
int * | type | Output | Type of object |
int * | subtype | Output | Subtype of object |
UF_OBJ_ask_face_analysis (view source)
Defined in: uf_obj.h
Overview
Asks the face analysis attribute of a face. If the attribute is TRUE, the
face is displayed using analysis data in face analysis views. The
parameters defining the details of the display are specified by
UF_DISP_set_srfanl_params.
Environment
Internal
See Also
Required License(s)
gateway
int UF_OBJ_ask_face_analysis
(
tag_t face,
logical * srfanl
)
tag_t | face | Input | Object identifier |
logical * | srfanl | Output | Face analysis data flag: TRUE = Face is displayed with face analysis data in face analysis views FALSE = off |
UF_OBJ_ask_name (view source)
Defined in: uf_obj.h
Overview
Required License(s)
gateway
int UF_OBJ_ask_name
(
tag_t object_id,
char * name
)
tag_t | object_id | Input | Object identifier of object to inquire upon. |
char * | name | Output | Name of object |
UF_OBJ_ask_name_origin (view source)
Defined in: uf_obj.h
Overview
Returns the name origin of the specified object. If the object you query is
not of an object type listed in uf_object_types.h or if the object has no name,
an error code returns and the origin is set to (0,0,0).
Environment
Internal and External
See Also
History
Originally released in V17.0
Required License(s)
gateway
int UF_OBJ_ask_name_origin
(
tag_t object_id,
double origin [ 3 ]
)
tag_t | object_id | Input | Object identifier of object to inquire upon. |
double | origin [ 3 ] | Output | Origin in absolute coordinates where the name of the object will be displayed. |
UF_OBJ_ask_owning_part (view source)
Defined in: uf_obj.h
Overview
Returns the tag of the part which contains the specified object_in_part.
Environment
Internal and External
Required License(s)
gateway
int UF_OBJ_ask_owning_part
(
tag_t object_in_part,
tag_t * part_tag
)
tag_t | object_in_part | Input | Tag of object for which the part is required. |
tag_t * | part_tag | Output | part containing object_in_part |
UF_OBJ_ask_partially_shaded (view source)
Defined in: uf_obj.h
Overview
Returns the partially shaded status for a single solid face.
Environment
Internal and External
Required License(s)
gateway
int UF_OBJ_ask_partially_shaded
(
tag_t object,
logical * shaded
)
tag_t | object | Input | Object identifier of solid face to read attribute from |
logical * | shaded | Output | Shaded status of the solid face TRUE = shading is on FALSE = shading is off |
UF_OBJ_ask_status (view source)
Defined in: uf_obj.h
Overview
Returns the objects status, UF_OBJ_DELETED, UF_OBJ_TEMPORARY, UF_OBJ_CONDEMNED,
and UF_OBJ_ALIVE. This function should only be used to get information on objects
within the part, not the part itself.
NOTE: You are strongly advised to avoid doing anything to non-alive
objects unless you are familiar with their use. NX may delete or reuse
these objects at any time. Some of these objects do not get filed with
the part.
Return
Returns 1 of 4 statuses
UF_OBJ_DELETED
UF_OBJ_TEMPORARY
UF_OBJ_CONDEMNED
UF_OBJ_ALIVE
Environment
Internal and External
Required License(s)
gateway
int UF_OBJ_ask_status
(
tag_t object
)
tag_t | object | Input | The object for which you are asking status |
UF_OBJ_ask_translucency (view source)
Defined in: uf_obj.h
Overview
Asks the translucency of faces, facets and bodies.
Environment
Internal and External
History
Introduced in NX 2.0.2
Required License(s)
gateway
int UF_OBJ_ask_translucency
(
tag_t object,
UF_OBJ_translucency_p_t translucency
)
tag_t | object | Input | The object for which you are asking the translucency It must be of one of the following types: UF_solid_type, with one of these subtypes: UF_solid_body_type UF_solid_face_type UF_faceted_model_type UF_component_type |
UF_OBJ_translucency_p_t | translucency | Output | percent translucent 0 - 100 |
UF_OBJ_ask_type_and_subtype (view source)
Defined in: uf_obj.h
Overview
Returns the object type and subtype of a tagged NX object.
The majority of these objects are listed in the uf_object_types.h
header file.
In addition to the objects listed in uf_object_types.h, there are other
NX objects uniquely identified by a tag. Among these objects
are expressions and parts. These objects, which are not listed in the
uf_object_types.h header file, produce the type UF_OBJ_EXPR_TYPE and
UF_OBJ_PART_TYPE with a subtype of 0.
The types and subtypes this function returns for expressions
and parts are not useful in any other Open API routines.
These types are provided only to allow you to determine the class of a
NX object through its identifier (i.e. its tag) which can assist
you in determining the other Open API routines that you can use
in conjunction with the object. For a more detailed discussion of
classes of objects and the Open API routines available to these
objects, please see the Open API Programmer's Guide, "The
NX Object Model".
Environment
Internal and External
Required License(s)
gateway
int UF_OBJ_ask_type_and_subtype
(
tag_t object_id,
int * type,
int * subtype
)
tag_t | object_id | Input | Object identifier of object to query |
int * | type | Output | Type of object |
int * | subtype | Output | Subtype of object |
UF_OBJ_cycle_all (view source)
Defined in: uf_obj.h
Overview
Returns all objects in a given part on all layers regardless of their
current status or displayability. This includes temporary (system created) objects.
It does not return expressions.
This function returns the tag of the object that was found. To continue
cycling, pass the returned object in as the second argument to this
function.
NOTE: You are strongly advised to avoid doing anything to non-alive
objects unless you are familiar with their use. NX may delete or reuse
these objects at any time. Some of these objects do not get filed with
the part.
NOTE: This routine is invalid for partially loaded parts. If you call this
function using a partially loaded part, it returns a NULL_TAG from
the beginning of the cycle.
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
Return
This function returns the object identifier of the next object.
The cycle is completed when a NULL_TAG is returned
Environment
Internal and External
See Also
Required License(s)
gateway
tag_t UF_OBJ_cycle_all
(
tag_t part_tag,
tag_t object
)
tag_t | part_tag | Input | Tag of part you wish to cycle |
tag_t | object | Input | Begin the cycle by passing in object = NULL_TAG |
UF_OBJ_cycle_by_name (view source)
Defined in: uf_obj.h
Overview
Cycle the objects of a given name in current work part. Note that the name of
an object of type UF_occ_instance_type is not necessarily the instance name.
Note that the name must match exactly. If the name of an object is "abc ", and
the name passed here is "abc", then the object will not be found because of
the trailing space.
When using UF_OBJ_cycle_by_name, features are only returned if they are the only
object with that name. If there is any possibility that there could be objects
with the same name (that are not features), then call UF_OBJ_cycle_by_by_name_and_type
using UF_feature_type in order to find the named features.
Please refer to the
example
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
Environment
Internal and External
Required License(s)
gateway
int UF_OBJ_cycle_by_name
(
const char * name,
tag_t * object
)
const char * | name | Input | Name of objects on which to cycle |
tag_t * | object | Input / Output | On input the object found by the last call to this routine. Begin the cycle by passing in object = NULL_TAG On output, the next object of the given name. Outputs a NULL_TAG when the cycle is finished. |
UF_OBJ_cycle_by_name_and_type (view source)
Defined in: uf_obj.h
Overview
Cycles objects in the specified part by name and object type. Note that
the name of an object of type UF_occ_instance_type is not necessarily the
instance name.
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
Environment
Internal and External
History
This function was originally released in V15.0.
Required License(s)
gateway
int UF_OBJ_cycle_by_name_and_type
(
tag_t part_tag,
const char * name,
int type,
logical use_occ,
tag_t * object
)
tag_t | part_tag | Input | Tag of part in which to cycle. |
const char * | name | Input | Name of objects on which to cycle. |
int | type | Input | Object type on which to cycle (see uf_object_types.h) |
logical | use_occ | Input | Occurrence filter: TRUE = include occurrences FALSE = exclude occurrrences |
tag_t * | object | Input / Output | On input the object found by the last call to this routine. Begin the cycle by passing in object = NULL_TAG On output, the next object of the given name. Outputs a NULL_TAG when the cycle is finished. |
UF_OBJ_cycle_by_name_and_type_extended (view source)
Defined in: uf_obj.h
Overview
Cycles objects in the specified part by name and object type. Note that
the name of an object of type UF_occ_instance_type is not necessarily the
instance name.
This works like UF_OBJ_cycle_by_name_and_type.
The difference between this routine and UF_OBJ_cycle_by_name_and_type is that
UF_OBJ_cycle_by_name_and_type returns all the extended objects (extended object
types have values over 256) if either UF_extended_type or UF_extended_displayable_type
is passed in as type. Whereas this routine does not return any objects for those two types
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
Environment
Internal and External
See Also
History
This function was originally released in V15.0.
Required License(s)
gateway
int UF_OBJ_cycle_by_name_and_type_extended
(
tag_t part_tag,
const char * name,
int type,
logical use_occ,
tag_t * object
)
tag_t | part_tag | Input | Tag of part in which to cycle. |
const char * | name | Input | Name of objects on which to cycle. |
int | type | Input | Object type on which to cycle (see uf_object_types.h) |
logical | use_occ | Input | Occurrence filter: TRUE = include occurrences FALSE = exclude occurrrences |
tag_t * | object | Input / Output | On input the object found by the last call to this routine. Begin the cycle by passing in object = NULL_TAG On output, the next object of the given name. Outputs a NULL_TAG when the cycle is finished. |
UF_OBJ_cycle_objs_in_part (view source)
Defined in: uf_obj.h
Overview
Returns all objects in the part of the specified types on all layers (including
layers not writable or viewable) regardless of their current state of displayability.
This routine does not return expressions, condemned objects, temporary (system created)
objects, or sleepy objects. An object that is asleep is one that has been removed from
the model. For example, if you blend an edge, then the edge is asleep. The WCS will not
be returned unless it has been saved.
NOTE: This routine cycles the features in a part when the type
specified is UF_feature_type.
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
Environment
Internal and External
See Also
For example please refer to the
example
Required License(s)
gateway
int UF_OBJ_cycle_objs_in_part
(
tag_t part_tag,
int type,
tag_t * object
)
tag_t | part_tag | Input | Tag of part you wish to cycle |
int | type | Input | Type of object on which to cycle |
tag_t * | object | Input / Output | On input the object found by the last call to this routine. if this routine has not been called yet, then set object=NULL_TAG to start cycling. On output the next object of the type specified. If there is no object, and the cycling is complete a NULL_TAG is returned. |
UF_OBJ_cycle_objs_in_part1 (view source)
Defined in: uf_obj.h
Overview
Returns all objects in the part of the specified types that are found on layers
1 thru 256 regardless of their current state of displayability. This routine does not
return expressions, condemned objects, temporary (system created) objects, or sleepy objects. An object that is asleep is one that has been removed from the model.
For example, if you blend an edge, then the edge is asleep. The WCS will not
be returned unless it has been saved.
NOTE: This routine cycles the features in a part when the type
specified is UF_feature_type.
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
Environment
Internal and External
See Also
For example please refer to the
example
History
NX10.0.0
Required License(s)
gateway
int UF_OBJ_cycle_objs_in_part1
(
tag_t part_tag,
int type,
tag_t * object
)
tag_t | part_tag | Input | Tag of part you wish to cycle |
int | type | Input | Type of object on which to cycle |
tag_t * | object | Input / Output | On input the object found by the last call to this routine. if this routine has not been called yet, then set object=NULL_TAG to start cycling. On output the next object of the type specified. If there is no object, and the cycling is complete a NULL_TAG is returned. |
UF_OBJ_cycle_typed_objs_in_part (view source)
Defined in: uf_obj.h
Overview
This routine has been added to deal with extended object types (extended object types have
values over 256).
Returns all objects in the part of the specified types on all layers
regardless of their current state of displayability. This routine does not
return expressions, condemned objects, temporary (system created) objects, or sleepy objects.
An object that is asleep is one that has been removed from the model.
For example, if you blend an edge, then the edge is asleep. The WCS will not
be returned unless it has been saved.
Although this works like UF_OBJ_cycle_objs_in_part, there is a difference.
When type is UF_extended_type, this routine (UF_OBJ_cycle_typed_objs_in_part) will not returns any objects.
Whereas UF_OBJ_cycle_objs_in_part will return all the objects with extended entity types for type UF_extended_type.
For more details on how UF_OBJ_cycle_objs_in_part works, please see comment for UF_OBJ_cycle_objs_in_part
NOTE: This routine cycles the features in a part when the type
specified is UF_feature_type.
Do not attempt to delete objects when cycling the database in a loop. Problems
can occur when trying to read the next object when the current object has been
deleted. To delete objects, save an array with the objects in it, and then
when you have completed cycling, use UF_OBJ_delete_array_of_objects to delete
the saved array of objects.
See Also
Required License(s)
gateway
int UF_OBJ_cycle_typed_objs_in_part
(
tag_t part_tag,
int type,
tag_t * object
)
tag_t | part_tag | Input | Tag of part you wish to cycle |
int | type | Input | Type of object on which to cycle |
tag_t * | object | Input / Output | On input the object found by the last call to this routine. if this routine has not been called yet, then set object=NULL_TAG to start cycling. On output the next object of the type specified. If there is no object, and the cycling is complete a NULL_TAG is returned. |
UF_OBJ_delete_array_of_objects (view source)
Defined in: uf_obj.h
Overview
Deletes an array of objects. This is considerably faster than deleting the
objects one at a time. This routine should always be used when more than
one object is to be deleted.
Do not attempt to delete objects while cycling the database in a looping
structure. Problems can occur when trying to read the next object and delete
objects in a looping structure. To delete objects, we recommend that you:
Save the objects in an array and then perform the delete function after you
have completed the cycling by calling UF_OBJ_delete_array_of_objects.
A return value of zero does not guarantee that all of the objects were
deleted. To determine if an particular object was deleted, use
UF_OBJ_ask_status. If statuses is NULL, then the return code from this
function will be 0 if the return code from UF_OBJ_delete_object would
have been zero for all the objects. A non-zero status can either mean
that an individual object could not be deleted, or that some other
fatal error occurred. If statuses is not null, then the individual
delete status for each object is returned in the statuses array. The
return code from the function will be non-zero if some more global
failure occurred.
Environment
Internal and External
See Also
History
Originally released in V16.0
Required License(s)
gateway
int UF_OBJ_delete_array_of_objects
(
int num_objects,
tag_t object_id [ ] ,
int * * statuses
)
int | num_objects | Input | The count of the objects in the object_id array. |
tag_t | object_id [ ] | Input | Array of object identifiers to be deleted. |
int * * | statuses | Input / Output to UF_*free* | This should be the address of pointer. If it is NULL, then individual status for the delete operation on each object will not be given. If it is non-NULL, then an array will be allocated, and the individual status for each object placed in this array. The status for individual objects can be: 0 - object was passed on to the delete algorithm UF_OBJ_object_can_not_be_deleted UF_OBJ_err_bad_parameter_number_1 This status will be the same as what would have been returned had the single object been passed to UF_OBJ_delete_object. A value of 0 does not necessarily mean that the object was deleted, this can only be determined by calling UF_OBJ_ask_status. If a non-NULL pointer is passed in, then the user must free this returned status array by using UF_free. |
UF_OBJ_delete_name (view source)
Defined in: uf_obj.h
Overview
Deletes the name from the specified object. Only objects with an object
type listed in uf_object_types.h can have their names deleted.
Environment
Internal and External
Required License(s)
gateway
int UF_OBJ_delete_name
(
tag_t object_id
)
tag_t | object_id | Input | Object identifier of object whose name is to be deleted. |
UF_OBJ_delete_object (view source)
Defined in: uf_obj.h
Overview
Deletes an object. A return value of zero does not guarantee that an object is
deleted. To determine if an object is deleted, use UF_OBJ_ask_status.
It is not allowed to delete the current WCS, if you try, an error will be
returned.
Do not attempt to delete objects while cycling the database in a looping
structure. Problems can occur when trying to read the next object and delete
objects in a looping structure. To delete objects, we recommend:
Save the objects in an array and then perform the delete function using
UF_OBJ_delete_array_of_objects after you have completed the cycling.
If you have multiple objects to delete, you should use the routine
UF_OBJECT_delete_array_of_objects, as it will be much faster.
Note: If a type-specific function exists for the type of object being
deleted, please use that type-specific function instead of this general
use function. For example, to delete a view use UF_VIEW_delete, to
delete a drawing use UF_DRAW_delete_drawing, etc.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_delete_object
(
tag_t object_id
)
tag_t | object_id | Input | Object identifier of object to delete |
UF_OBJ_is_def_cre_color (view source)
Defined in: uf_obj.h
Overview
Query if the work part's type/subtype color setting is using the default
color setting.
Environment
Internal and External
See Also
For information on type, subtype and properties
click here.
Required License(s)
gateway
int UF_OBJ_is_def_cre_color
(
const int type,
const int subtype,
const int property,
logical * is_default
)
const int | type | Input | Type to query |
const int | subtype | Input | Subtype to query |
const int | property | Input | Property of type/subtype to query |
logical * | is_default | Output | TRUE = Color is set to default FALSE = Color is not set to default |
UF_OBJ_is_def_cre_line_font (view source)
Defined in: uf_obj.h
Overview
Query if the work part's type/subtype line font setting is using the
default line font setting.
Environment
Internal and External
See Also
For information on type, subtype and properties
click here.
Required License(s)
gateway
int UF_OBJ_is_def_cre_line_font
(
const int type,
const int subtype,
const int property,
logical * is_default
)
const int | type | Input | Type to query |
const int | subtype | Input | Subtype to query |
const int | property | Input | Property of type/subtype to query |
logical * | is_default | Output | TRUE = Line font is set to default FALSE = Line font is not set to default |
UF_OBJ_is_def_cre_width (view source)
Defined in: uf_obj.h
Overview
Query if the work part's type/subtype line width setting is using the
default line width setting.
Environment
Internal and External
See Also
For information on type, subtype and properties
click here.
Required License(s)
gateway
int UF_OBJ_is_def_cre_width
(
const int type,
const int subtype,
const int property,
logical * is_default
)
const int | type | Input | Type to query |
const int | subtype | Input | Subtype to query |
const int | property | Input | Property of type/subtype to query |
logical * | is_default | Output | TRUE = Line width is set to default FALSE = Line width is not set to default |
UF_OBJ_is_displayable (view source)
Defined in: uf_obj.h
Overview
Returns a logical indicating whether tagged NX object is displayable,
and therefore possesses attributes of color, width, font, and layer.
Although an object possesses these displayable attributes, it
does not mean that the object is ever actually displayed in the graphics
window in an interactive NX session. Some objects possess
these characteristics for purposes internal to NX.
Return
Returns a logical which indicates whether object is
displayable
Environment
Internal and External
Required License(s)
gateway
int UF_OBJ_is_displayable
(
tag_t object_id,
logical * is_displayable
)
tag_t | object_id | Input | Object identifier of object to query |
logical * | is_displayable | Output | TRUE = This object is displayable FALSE = This object is not displayable |
UF_OBJ_is_object_a_promotion (view source)
Defined in: uf_obj.h
Overview
Queries if an object is a promoted object. Returns TRUE if object is a
promotion.
Environment
Internal and External
Required License(s)
gateway
logical UF_OBJ_is_object_a_promotion
(
tag_t object
)
tag_t | object | Input | Tag of object to query |
UF_OBJ_is_transferable (view source)
Defined in: uf_obj.h
Overview
Determines whether the given tagged NX object is a transferable or not.
You can potentially export a transferable object using
UF_PART_export or UF_PART_export_with_options, or transfer to a
new component using UF_ASSEM_create_component_part.
Although a particular object may return as being transferable, there is
no guarantee that the objects of that type will be transferred. For
example, if an object of a transferable type depends upon an object
which is not transferable, then the original object will not be transferred.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_is_transferable
(
tag_t object_id,
logical * is_transferable
)
tag_t | object_id | Input | Object identifier of object to query |
logical * | is_transferable | Output | TRUE = This object is transferable FALSE = This object is not transferable |
UF_OBJ_modify_defaults (view source)
Defined in: uf_obj.h
Overview
UF_OBJ_modify_defaults -- replaced by default routines above
Required License(s)
gateway
int UF_OBJ_modify_defaults
(
int default_color,
int default_layer,
int default_width,
int default_font
)
int | default_color | Input | |
int | default_layer | Input | |
int | default_width | Input | |
int | default_font | Input | |
UF_OBJ_replace_object_array_data (view source)
Defined in: uf_obj.h
Overview
Replaces the geometry of the n'th element of the target object array with
the geometry of the n'th element of the source object array. Neither object
can be an occurrence but both objects may belong to the same component part
in an assembly. Both objects must be alive (see UF_OBJ_ask_status)
and both objects must be distinct and belong to the same part.
The target objects get added to the update list and any references to
these objects are maintained.
The source objects get added to the delete list.
Users must call UF_MODL_update() at the appropriate time to update
the target objects, delete the source objects and
propagate the changes to the model.
The type and subtype of each pair of objects must be valid for the routine
but they are not required to be the same. It is expected that the source
object is a newly created object with no extra user defined
attributes attached, and that it is not referenced by other objects.
Only valid geometry can exist in the objects, which consists of the
following (all subtypes are valid):
UF_point_type
UF_line_type
UF_circle_type
UF_conic_type
UF_spline_type
The display details [layer, color, line font and width, blank and
highlight status] and all user defined attributes, including names of
the target objects are all maintained. Links and references to the
target objects are preserved.
The reference set of the source objects are copied to the respective
target objects. If a source object is of a different type than the
corresponding target object, any occurrences existing based on the
target object are deleted and recreated by this routine.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_replace_object_array_data
(
int num_objects,
tag_t * target_objects,
tag_t * source_objects
)
int | num_objects | Input | Number of objects whose geometry is to be replaced |
tag_t * | target_objects | Input | Target objects whose geometry is to be replaced |
tag_t * | source_objects | Input | Source objects whose geometry is to be used as replacements for target_objects |
UF_OBJ_replace_object_data (view source)
Defined in: uf_obj.h
Overview
Replaces the geometry of the target object with the
geometry of the source object. Neither object can be an
occurrence but both objects may belong to the same component part
in an assembly. Both objects must be alive (see UF_OBJ_ask_status)
and both objects must be distinct and belong to the same part.
The target object gets updated and any references to this
object are maintained. The source object gets deleted.
The type and subtype of each object must be valid for the routine but
they are not required to be the same. It is expected that the source object
is a newly created object with no extra user defined attributes attached,
and that it is not referenced by other objects.
Only valid geometry can exist in either object which consists of the
following (all subtypes are valid):
UF_point_type
UF_line_type
UF_circle_type
UF_conic_type
UF_spline_type
The display details [layer, color, line font and width, blank and
highlight status] and all user defined attributes, including name of
the target object are all maintained. Links and references to the target
object are preserved. The reference set of the source object is copied to
the target object. If the source object is a different type than the
target object, any occurrences existing based on the target object are
deleted and recreated by this routine.
NOTE: This routine will update the model. If this is not desirable,
see UF_OBJ_replace_object_array_data()
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_replace_object_data
(
tag_t orig_obj,
tag_t new_obj
)
tag_t | orig_obj | Input | Target object whose geometry is to be replaced. |
tag_t | new_obj | Input | Source object whose geometry is to be used as a replacement for orig_obj. |
UF_OBJ_reset_defaults (view source)
Defined in: uf_obj.h
Overview
UF_OBJ_reset_defaults -- replaced by default routines above
Required License(s)
gateway
int UF_OBJ_reset_defaults
(
int default_color,
int default_layer,
int default_width,
int default_font
)
int | default_color | Input | |
int | default_layer | Input | |
int | default_width | Input | |
int | default_font | Input | |
UF_OBJ_return_prev_defaults (view source)
Defined in: uf_obj.h
Overview
UF_OBJ_return_prev_defaults -- replaced by default routines above
Required License(s)
gateway
int UF_OBJ_return_prev_defaults
(
void
)
UF_OBJ_reverse_blank_all (view source)
Defined in: uf_obj.h
Overview
Reverses the blank status of all displayable objects on selectable
layers. Uses the work view layer mask.
Environment
Internal and External
Required License(s)
gateway
int UF_OBJ_reverse_blank_all
(
void
)
UF_OBJ_set_blank_status (view source)
Defined in: uf_obj.h
Overview
Modifies the blank status of an object. Use UF_OBJ_ask_display_properties to
determine the object's current blank status.
If the object is a sketch or a group, all members of the sketch or
group will have their blank status modified. For groups, this includes
all members of any sub-groups.
Environment
Internal and External
See Also
History
V18.0 Comments about sketches and groups added
Required License(s)
gateway
int UF_OBJ_set_blank_status
(
tag_t object_id,
int blank_status
)
tag_t | object_id | Input | Object identifier of object whose blank status is to be changed. |
int | blank_status | Input | Blank status to assign. Use one of the following string defined constants: UF_OBJ_NOT_BLANKED UF_OBJ_BLANKED |
UF_OBJ_set_color (view source)
Defined in: uf_obj.h
Overview
Modifies the color of an object. Use UF_OBJ_ask_display_properties to
determine the object's current color.
Note: There must be a work part present before calling this function.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_set_color
(
tag_t object_id,
int color
)
tag_t | object_id | Input | Object identifier of object whose color is to be changed. |
int | color | Input | Color to assign. Must be one of the following values [1-216] |
UF_OBJ_set_cre_color (view source)
Defined in: uf_obj.h
Overview
Set the specified type and subtype's color object creation setting in the
work part. If the type is not a valid object type or if no object creation
settings exist for the type and subtype combination then an error is
returned.
Environment
Internal and External
See Also
See the string defined color constants in the
types and symbols
For information on type, subtype and properties
click here.
Required License(s)
gateway
int UF_OBJ_set_cre_color
(
const int type,
const int subtype,
const int property,
const int color
)
const int | type | Input | Type to set color of |
const int | subtype | Input | Subtype to set color of |
const int | property | Input | Property of type/subtype to set color of |
const int | color | Input | Color for types new object creation |
UF_OBJ_set_cre_color_to_def (view source)
Defined in: uf_obj.h
Overview
Make the work part's type/subtype color setting use the default color
setting.
Environment
Internal and External
See Also
For information on type, subtype and properties
click here.
Required License(s)
gateway
int UF_OBJ_set_cre_color_to_def
(
const int type,
const int subtype,
const int property
)
const int | type | Input | Type to set color of |
const int | subtype | Input | Subtype to set color of |
const int | property | Input | Property of type/subtype to set color of |
UF_OBJ_set_cre_line_font (view source)
Defined in: uf_obj.h
Overview
Set the specified type and subtype's line font object creation setting in
the work part. If the type is not a valid object type or if no object
creation settings exist for the type and subtype combination then an
error is returned.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_set_cre_line_font
(
const int type,
const int subtype,
const int property,
const int line_font
)
const int | type | Input | Type to set line font of |
const int | subtype | Input | Subtype to set line font of |
const int | property | Input | Property of type/subtype to set line font of |
const int | line_font | Input | Type's new object creation line font |
UF_OBJ_set_cre_line_font_to_def (view source)
Defined in: uf_obj.h
Overview
Make the work part's type/subtype line font setting use the default
line font setting.
Environment
Internal and External
See Also
For information on type, subtype and properties
click here.
Required License(s)
gateway
int UF_OBJ_set_cre_line_font_to_def
(
const int type,
const int subtype,
const int property
)
const int | type | Input | Type to set line font of |
const int | subtype | Input | Subtype to set line font of |
const int | property | Input | Property of type/subtype to set line font of |
UF_OBJ_set_cre_width (view source)
Defined in: uf_obj.h
Overview
Set the specified type and subtype's width object creation setting in
the work part. If the type is not a valid object type or if no object
creation settings exist for the type and subtype combination then an
error is returned.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_set_cre_width
(
const int type,
const int subtype,
const int property,
const int width
)
const int | type | Input | Type to set width of |
const int | subtype | Input | Subtype to set width of |
const int | property | Input | Property of type/subtype to set width of |
const int | width | Input | Type's new object creation width |
UF_OBJ_set_cre_width_to_def (view source)
Defined in: uf_obj.h
Overview
Make the work part's type/subtype width setting use the default width
setting.
Environment
Internal and External
See Also
For information on type, subtype and properties
click here.
Required License(s)
gateway
int UF_OBJ_set_cre_width_to_def
(
const int type,
const int subtype,
const int property
)
const int | type | Input | Type to set width of |
const int | subtype | Input | Subtype to set width of |
const int | property | Input | Property of type/subtype to set width of |
UF_OBJ_set_def_cre_color (view source)
Defined in: uf_obj.h
Overview
Sets the default color object creation setting. Does not work for sheet bodies
or solid bodies. Use UF_OBJ_set_cre_color_to_def or UF_OBJ_set_cre_color for
these specific object types.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_set_def_cre_color
(
const int color
)
const int | color | Input | New default object creation color |
UF_OBJ_set_def_cre_line_font (view source)
Defined in: uf_obj.h
Overview
Sets the default line_font object creation setting.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_set_def_cre_line_font
(
const int line_font
)
const int | line_font | Input | New default object creation line_font |
UF_OBJ_set_def_cre_width (view source)
Defined in: uf_obj.h
Overview
Sets the default width object creation setting.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_set_def_cre_width
(
const int width
)
const int | width | Input | New default object creation width |
UF_OBJ_set_face_analysis (view source)
Defined in: uf_obj.h
Overview
Sets the face analysis attribute of a face. If the attribute is TRUE, the
face is displayed using analysis data in face analysis views. The
parameters defining the details of the display are specified by
UF_DISP_set_srfanl_params.
Environment
Internal
See Also
Required License(s)
gateway
int UF_OBJ_set_face_analysis
(
tag_t face,
logical srfanl
)
tag_t | face | Input | Object identifier of the face |
logical | srfanl | Input | Shaded status of the face TRUE = Display with analysis data in face analysis views. FALSE = Display without analysis data |
UF_OBJ_set_font (view source)
Defined in: uf_obj.h
Overview
Modifies the font of an object. Use UF_OBJ_ask_display_properties to
determine the object's current font.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_set_font
(
tag_t object_id,
int font
)
tag_t | object_id | Input | Object identifier of object whose font is to be changed. |
int | font | Input | font to assign. |
UF_OBJ_set_layer (view source)
Defined in: uf_obj.h
Overview
Modifies the layer of an object. Use UF_OBJ_ask_display_properties to
determine the object's current layer.
If you attempt to change the layer of an object which is on a
reserved layer (greater than UF_LAYER_MAX_LAYER, or zero), the request
will be ignored.
If you attempt to change the layer of an object which is on a user-accessible
layer (UF_LAYER_MIN_LAYER <= layer <= UF_LAYER_MAX_LAYER) to a reserved layer,
the request will be ignored, except that objects of type RM_view_type
and RM_cs2_vertex_type may be moved to layer 0, which is where these
object types belong, so that parts where these object types were erroneously
moved off of layer 0 may be repaired.
Environment
Internal and External
See Also
History
In V18.0 attempts to move change the layer of objects on
reserved layers will be ignored.
Required License(s)
gateway
int UF_OBJ_set_layer
(
tag_t object_id,
int layer
)
tag_t | object_id | Input | Object identifier of object whose layer is to be changed. |
int | layer | Input | layer to assign. |
UF_OBJ_set_layer_allow_hidden (view source)
Defined in: uf_obj.h
Overview
Modifies the layer of an object. Use UF_OBJ_ask_display_properties to
determine the object's current layer.
This function allows movement to and from the hidden layers.
Environment
Internal and External
See Also
History
Original release was in NX 3.0.3
Required License(s)
gateway
int UF_OBJ_set_layer_allow_hidden
(
tag_t object_id,
int layer
)
tag_t | object_id | Input | Object identifier of object whose layer is to be changed. |
int | layer | Input | layer to assign. |
UF_OBJ_set_line_width (view source)
Defined in: uf_obj.h
Overview
Modifies the line_width of an object. Use UF_OBJ_ask_display_properties to
determine the object's current line width.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_OBJ_set_line_width
(
tag_t object_id,
int line_width
)
tag_t | object_id | Input | Object identifier of object whose line_width is to be changed. |
int | line_width | Input | line_width to assign. |
UF_OBJ_set_name (view source)
Defined in: uf_obj.h
Overview
Sets the name of a object. You can only set the name of an object which has
an object type defined in the uf_object_types.h header file. Note that the
name set for an object of type UF_occ_instance_type is not the instance name;
the instance name can be set using UF_ASSEM_rename_instance.
Environment
Internal and External
Required License(s)
gateway
int UF_OBJ_set_name
(
tag_t object_id,
const char * name
)
tag_t | object_id | Input | Object identifier of object whose name is to be set. |
const char * | name | Input | Name to assign to object. The length of the name is limited to UF_OBJ_NAME_LEN characters. |
UF_OBJ_set_name_origin (view source)
Defined in: uf_obj.h
Overview
Sets the origin of an object name. This origin is only used as the location
to display the name when name display is enabled with
UF_DISP_set_name_display_status. This routine will return an error if the
object is not named.
Environment
Internal and External
See Also
History
Originally released in V17.0
Required License(s)
gateway
int UF_OBJ_set_name_origin
(
tag_t object_id,
double origin [ 3 ]
)
tag_t | object_id | Input | Object identifier of object whose name origin is to be set. |
double | origin [ 3 ] | Input | Origin in absolute coordinates where the name is to be displayed |
UF_OBJ_set_partially_shaded (view source)
Defined in: uf_obj.h
Overview
Sets the partial shading attribute for a solid face or for all faces in a
solid body.
Environment
Internal and External
Required License(s)
gateway
int UF_OBJ_set_partially_shaded
(
tag_t object,
logical shaded
)
tag_t | object | Input | Object identifier of solid face or body to set attributes for |
logical | shaded | Input | Shaded status of the solid face TRUE = set shading FALSE = unset shading |
UF_OBJ_set_translucency (view source)
Defined in: uf_obj.h
Overview
Sets the translucency of faces, facets and solid/sheet bodies.
Environment
Internal and External
History
Introduced in NX 2.0.2
Required License(s)
gateway
int UF_OBJ_set_translucency
(
tag_t object,
UF_OBJ_translucency_t translucency
)
tag_t | object | Input | The object for which you are setting the translucency It must be of one of the following types: UF_solid_type, with one of these subtypes: UF_solid_body_type UF_solid_face_type UF_faceted_model_type UF_component_type |
UF_OBJ_translucency_t | translucency | Input | percent translucent 0 - 100 |