public static class QuickQuotationBuilder.InsertGroupMaterials extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CR12
insert group material is Cr12
|
static int |
_CR12MO_V
insert group material is Cr12MoV
|
static QuickQuotationBuilder.InsertGroupMaterials |
CR12
insert group material is Cr12
|
static QuickQuotationBuilder.InsertGroupMaterials |
CR12MO_V
insert group material is Cr12MoV
|
Modifier and Type | Method and Description |
---|---|
static QuickQuotationBuilder.InsertGroupMaterials |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static QuickQuotationBuilder.InsertGroupMaterials |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static QuickQuotationBuilder.InsertGroupMaterials[] |
values()
Returns an array that contains the values for this enum.
|
public static final QuickQuotationBuilder.InsertGroupMaterials CR12
public static final QuickQuotationBuilder.InsertGroupMaterials CR12MO_V
public static final int _CR12
public static final int _CR12MO_V
public static QuickQuotationBuilder.InsertGroupMaterials valueOf(int value)
public static QuickQuotationBuilder.InsertGroupMaterials valueOf(String name)
public static QuickQuotationBuilder.InsertGroupMaterials[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.