public static class QuickQuotationBuilder.DesignTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ADDITIONAL_DIE
The design is a additional die
|
static int |
_CHANGEOVER
the design is a changeover
|
static int |
_NEW_DESIGN
the design is a new design
|
static QuickQuotationBuilder.DesignTypes |
ADDITIONAL_DIE
The design is a additional die
|
static QuickQuotationBuilder.DesignTypes |
CHANGEOVER
the design is a changeover
|
static QuickQuotationBuilder.DesignTypes |
NEW_DESIGN
the design is a new design
|
Modifier and Type | Method and Description |
---|---|
static QuickQuotationBuilder.DesignTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static QuickQuotationBuilder.DesignTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static QuickQuotationBuilder.DesignTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final QuickQuotationBuilder.DesignTypes NEW_DESIGN
public static final QuickQuotationBuilder.DesignTypes CHANGEOVER
public static final QuickQuotationBuilder.DesignTypes ADDITIONAL_DIE
public static final int _NEW_DESIGN
public static final int _CHANGEOVER
public static final int _ADDITIONAL_DIE
public static QuickQuotationBuilder.DesignTypes valueOf(int value)
public static QuickQuotationBuilder.DesignTypes valueOf(String name)
public static QuickQuotationBuilder.DesignTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.