public static class MWMoldedPartValidationBuilder.CalculateOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EDIT_REGIONS_ONLY
edit properties of region faces only
|
static int |
_KEEP_EXISTING
calculate and keep existing properties on the faces
|
static int |
_RESET_ALL
calculate and replace all properties for region faces
|
static MWMoldedPartValidationBuilder.CalculateOption |
EDIT_REGIONS_ONLY
edit properties of region faces only
|
static MWMoldedPartValidationBuilder.CalculateOption |
KEEP_EXISTING
calculate and keep existing properties on the faces
|
static MWMoldedPartValidationBuilder.CalculateOption |
RESET_ALL
calculate and replace all properties for region faces
|
Modifier and Type | Method and Description |
---|---|
static MWMoldedPartValidationBuilder.CalculateOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MWMoldedPartValidationBuilder.CalculateOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MWMoldedPartValidationBuilder.CalculateOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final MWMoldedPartValidationBuilder.CalculateOption KEEP_EXISTING
public static final MWMoldedPartValidationBuilder.CalculateOption EDIT_REGIONS_ONLY
public static final MWMoldedPartValidationBuilder.CalculateOption RESET_ALL
public static final int _KEEP_EXISTING
public static final int _EDIT_REGIONS_ONLY
public static final int _RESET_ALL
public static MWMoldedPartValidationBuilder.CalculateOption valueOf(int value)
public static MWMoldedPartValidationBuilder.CalculateOption valueOf(String name)
public static MWMoldedPartValidationBuilder.CalculateOption[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.