public static class MWMoldedPartValidationBuilder.AssignToRegion extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CAVITY_REGION
assign selected region faces to the Cavity region
|
static int |
_CORE_REGION
assign selected region faces to the Core region
|
static MWMoldedPartValidationBuilder.AssignToRegion |
CAVITY_REGION
assign selected region faces to the Cavity region
|
static MWMoldedPartValidationBuilder.AssignToRegion |
CORE_REGION
assign selected region faces to the Core region
|
Modifier and Type | Method and Description |
---|---|
static MWMoldedPartValidationBuilder.AssignToRegion |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MWMoldedPartValidationBuilder.AssignToRegion |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MWMoldedPartValidationBuilder.AssignToRegion[] |
values()
Returns an array that contains the values for this enum.
|
public static final MWMoldedPartValidationBuilder.AssignToRegion CAVITY_REGION
public static final MWMoldedPartValidationBuilder.AssignToRegion CORE_REGION
public static final int _CAVITY_REGION
public static final int _CORE_REGION
public static MWMoldedPartValidationBuilder.AssignToRegion valueOf(int value)
public static MWMoldedPartValidationBuilder.AssignToRegion valueOf(String name)
public static MWMoldedPartValidationBuilder.AssignToRegion[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.