public interface PortConnectionCollection extends TaggedObjectCollection
PortConnection
objects. RouteManager
Modifier and Type | Interface and Description |
---|---|
static class |
PortConnectionCollection.PortsStatus
Option to check if two ports can be connected by creating
a
PortConnection object. |
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
PortConnectionCollection.PortsStatus |
canPortsConnect(Port port1,
Port port2)
Determines if the two ports can be connected using a
PortConnection object. |
PortConnection |
createPortConnection(Port port1,
Port port2)
Creates a
PortConnection object. |
PortConnection |
getConnectionFromPort(Port port)
Returns the
PortConnection the given part participates in, if any. |
_find_next, iterator
PortConnection createPortConnection(Port port1, Port port2) throws NXException, RemoteException
PortConnection
object.
port1
- first Port to be connected by the Port Connection objectport2
- second Port to be connected by the Port Connection objectNXException
RemoteException
PortConnectionCollection.PortsStatus canPortsConnect(Port port1, Port port2) throws NXException, RemoteException
PortConnection
object.
port1
- first Port to be connected by the Port Connection objectport2
- second Port to be connected by the Port Connection objectNXException
RemoteException
PortConnection getConnectionFromPort(Port port) throws NXException, RemoteException
PortConnection
the given part participates in, if any.
port
- NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.