public static class PortConnectionCollection.PortsStatus extends Enum
PortConnection
object.Modifier and Type | Field and Description |
---|---|
static int |
_CAN_CONNECT
The Ports can be connected
using Port Connection object.
|
static int |
_CANNOT_CONNECT
The Ports cannot be connected
using Port Connection object.
|
static PortConnectionCollection.PortsStatus |
CAN_CONNECT
The Ports can be connected
using Port Connection object.
|
static PortConnectionCollection.PortsStatus |
CANNOT_CONNECT
The Ports cannot be connected
using Port Connection object.
|
Modifier and Type | Method and Description |
---|---|
static PortConnectionCollection.PortsStatus |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PortConnectionCollection.PortsStatus |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PortConnectionCollection.PortsStatus[] |
values()
Returns an array that contains the values for this enum.
|
public static final PortConnectionCollection.PortsStatus CAN_CONNECT
public static final PortConnectionCollection.PortsStatus CANNOT_CONNECT
public static final int _CAN_CONNECT
public static final int _CANNOT_CONNECT
public static PortConnectionCollection.PortsStatus valueOf(int value)
public static PortConnectionCollection.PortsStatus valueOf(String name)
public static PortConnectionCollection.PortsStatus[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.