Modifier and Type | Interface and Description |
---|---|
static class |
Division.SplitDirectionType
The direction in which the cross-section is to be split
|
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
void |
createSplitterCurve()
Creates splitting Curve.
|
void |
deleteAllChildren()
Deletes all children divisions of the input division and the splitter curves
that were used to create the children divisions.
|
void |
setSplitDirection(Division.SplitDirectionType splitDirection)
License requirements: routing_hvac ("Routing HVAC") . |
Division.SplitDirectionType |
splitDirection()
Returns the direction of split, either vertical or horizontal
License requirements: routing_hvac ("Routing HVAC") . |
void |
updateFlow(double leftChildFlow,
double rightChildFlow,
boolean isAbsoluteFlow)
Update the Flow.
|
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
Division.SplitDirectionType splitDirection() throws NXException, RemoteException
NXException
RemoteException
void setSplitDirection(Division.SplitDirectionType splitDirection) throws NXException, RemoteException
splitDirection
- NXException
RemoteException
void createSplitterCurve() throws NXException, RemoteException
NXException
RemoteException
void updateFlow(double leftChildFlow, double rightChildFlow, boolean isAbsoluteFlow) throws NXException, RemoteException
leftChildFlow
- percentage absolute or relative flow in the left child divisionrightChildFlow
- percentage absolute or relative flow in the right child divisionisAbsoluteFlow
- if TRUE: displays absolute flow percentage for each
division, else displays relative flow percentageNXException
RemoteException
void deleteAllChildren() throws NXException, RemoteException
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.