public interface DiscontinuityCornerCollection extends TaggedObjectCollection
DiscontinuityCorner
objects. RouteManager
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
boolean |
areSegmentsDisconnected(SplineSegment segment1,
SplineSegment segment2,
ControlPoint rcp)
Checks whether segment1 and segment2 are disconnected at a control point
due to a discontinuity corner.
|
DiscontinuityCorner |
create(ControlPoint rcp,
ISegment firstSegment,
ISegment secondSegment)
Creates a discontinuity corner object at the given
ControlPoint . |
DiscontinuityCorner[] |
getDiscontinuityCorners(ControlPoint rcp)
Return the discontinuity corners assigned to the input control point.
|
_find_next, iterator
DiscontinuityCorner create(ControlPoint rcp, ISegment firstSegment, ISegment secondSegment) throws NXException, RemoteException
ControlPoint
. There must be two input
ISegment
objects, and they both must
reference the input ControlPoint
object.
rcp
- firstSegment
- first segment to form discontinuity on,
must be attached to the input RCP.secondSegment
- second segment to form discontinuity on,
must be attached to the input RCP.NXException
RemoteException
DiscontinuityCorner[] getDiscontinuityCorners(ControlPoint rcp) throws NXException, RemoteException
rcp
- The control pointNXException
RemoteException
boolean areSegmentsDisconnected(SplineSegment segment1, SplineSegment segment2, ControlPoint rcp) throws NXException, RemoteException
segment1
- First segment associated with the corner.segment2
- The 2nd segment associated with the corner.rcp
- Control point.NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.