See: Description
Interface | Description |
---|---|
AssignCornerBuilder |
Builder class for Assign Corner which creates corner
To create a new instance of this class, use nxopen.MechanicalRouting.BuilderFactory#createAssignCornerBuilder Default values. |
BaseCornerTypeBuilder |
Builder class for Base Corner Types .
|
BendCornerTypeBuilder |
Contains setting for corner creation.
|
BuilderFactory |
Represents an
BuilderFactory object. |
ConnectBuilder |
the Builder for Connect Path
To create a new instance of this class, use nxopen.MechanicalRouting.BuilderFactory#createConnectBuilder Created in NX11.0.0 |
ConnectivityService |
Represents a
ConnectivityService object. |
CreatePathBuilder |
Represents
CreatePathBuilder . |
EditPointBuilder |
Represents
EditPointBuilder . |
InsulationBuilder |
Represents
InsulationBuilder . |
LogicalDesignService |
Represents a
LogicalDesignService object. |
ManageInlineBehaviorBuilder |
Represents
ManageInlineBehaviorBuilder . |
MergeBuilder |
the Builder to Merge Component
To create a new instance of this class, use nxopen.MechanicalRouting.BuilderFactory#createMergeBuilder Created in NX11.0.0 |
MovePathBuilder |
Represents
MovePathBuilder . |
PartPlacementBuilder |
Represents
PartPlacementBuilder . |
PathStockPreferenceBuilder |
Assigns stocks to segments based on user's criteria and the current default stock.
|
PathTransitionBuilder |
Represents
PathTransitionBuilder . |
PathTransitionBuilderList |
Represents a list of objects.
|
PathTransitionListManagerBuilder |
Represents
PathTransitionListManagerBuilder . |
RoutingManager |
Represents an
RoutingManager object. |
SplitBuilder |
the Builder to Assign Discontinuity for the stocks
To create a new instance of this class, use nxopen.MechanicalRouting.BuilderFactory#createSplitBuilder Created in NX11.0.0 |
StockBuilder |
Builder for creating/editing stocks.
|
TransformBlockBuilder |
Represents
TransformBlockBuilder . |
Class | Description |
---|---|
AssignCornerBuilder.CornerType |
Defines the corner types.
|
BendCornerTypeBuilder.BendMethod |
Methods available for bend creation.
|
ConnectivityService.ConnectedPortsData |
This class holds the data returned from
ConnectivityService.getConnectedPorts(nxopen.Part) |
EditPointBuilder.Editsegmenttype |
Specifies the options available for Edit Segment motion.
|
EditPointBuilder.Motiontype |
Specifies the options available for motion.
|
InsulationBuilder.WrapType |
The application type for wrapped Insulation
|
LogicalDesignService.MappingStatus |
The status returned from checking the logical design mapping to physical design.
|
MovePathBuilder.DetachTypes |
Specifies the options that will allow the user to enforce the transformation by detaching
the routing objects (if necessary) from objects that stop the selected object from moving.
|
PartPlacementBuilder.PlacementValidationStatus |
The placement validation status .
|
PartPlacementBuilder.PositionAsType |
The positioning types .
|
PathStockPreferenceBuilder.AssignMethod |
Determines how to choose which stock to assign.
|
PathStockPreferenceBuilder.AssignStockSubType |
Determines the type of sub stock being assigned.
|
PathStockPreferenceBuilder.AssignStockType |
Determines the type of stock being assigned.
|
PathTransitionBuilder.HealOrientation |
The box orientation for heal transition traversal order.
|
PathTransitionBuilder.TraversalOrder |
The heal transition traversal order the path takes to reach the transition end point.
|
PathTransitionBuilder.Type |
The type of transition the path takes to reach the transition end point.
|
RoutingManagerFactory | |
TransformBlockBuilder.Transformtype |
Specifies the options available for transform.
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.