public static class PartPlacementBuilder.PlacementValidationStatus extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_PART_NOT_CONNECTED_TO_ROUT
after placement connection should have been built with routing system but it was not
|
static int |
_SUCCESS
part placement is successful as expected
|
static PartPlacementBuilder.PlacementValidationStatus |
PART_NOT_CONNECTED_TO_ROUT
after placement connection should have been built with routing system but it was not
|
static PartPlacementBuilder.PlacementValidationStatus |
SUCCESS
part placement is successful as expected
|
Modifier and Type | Method and Description |
---|---|
static PartPlacementBuilder.PlacementValidationStatus |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartPlacementBuilder.PlacementValidationStatus |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartPlacementBuilder.PlacementValidationStatus[] |
values()
Returns an array that contains the values for this enum.
|
public static final PartPlacementBuilder.PlacementValidationStatus SUCCESS
public static final PartPlacementBuilder.PlacementValidationStatus PART_NOT_CONNECTED_TO_ROUT
public static final int _SUCCESS
public static final int _PART_NOT_CONNECTED_TO_ROUT
public static PartPlacementBuilder.PlacementValidationStatus valueOf(int value)
public static PartPlacementBuilder.PlacementValidationStatus valueOf(String name)
public static PartPlacementBuilder.PlacementValidationStatus[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.