public static class EndCutBuilder.SelectionTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FACE_AND_EDGE
If this Selection Type is set, then a single pair of a Face (Placement Face) and an edge(Placement Edge) needs to be specified.
|
static int |
_FACES_WITH_ATTRIBUTES
If this Selection Type is set, just faces need to be specifed and placement edges will be inferred automatically.
|
static EndCutBuilder.SelectionTypes |
FACE_AND_EDGE
If this Selection Type is set, then a single pair of a Face (Placement Face) and an edge(Placement Edge) needs to be specified.
|
static EndCutBuilder.SelectionTypes |
FACES_WITH_ATTRIBUTES
If this Selection Type is set, just faces need to be specifed and placement edges will be inferred automatically.
|
Modifier and Type | Method and Description |
---|---|
static EndCutBuilder.SelectionTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EndCutBuilder.SelectionTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EndCutBuilder.SelectionTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final EndCutBuilder.SelectionTypes FACES_WITH_ATTRIBUTES
public static final EndCutBuilder.SelectionTypes FACE_AND_EDGE
public static final int _FACES_WITH_ATTRIBUTES
public static final int _FACE_AND_EDGE
public static EndCutBuilder.SelectionTypes valueOf(int value)
public static EndCutBuilder.SelectionTypes valueOf(String name)
public static EndCutBuilder.SelectionTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.