public static class EndCutBuilder.LimitTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NEAT_TRIM
If this Limit Type is set, a datum plane feature, a face or a profile/plate body needs to be selected and the endcut will be trimmed to the selected geometry.
|
static int |
_PLANE
If this Limit Type is set, a Plane needs to be specified and the Tilt and Shear angles will be inferred from the intersection of Datum Plane with the body on which EndCut will be applied.
|
static int |
_VALUE
If this Limit Type is set, the values of Tilt Angle and Shear Angle expressions will be used.
|
static EndCutBuilder.LimitTypes |
NEAT_TRIM
If this Limit Type is set, a datum plane feature, a face or a profile/plate body needs to be selected and the endcut will be trimmed to the selected geometry.
|
static EndCutBuilder.LimitTypes |
PLANE
If this Limit Type is set, a Plane needs to be specified and the Tilt and Shear angles will be inferred from the intersection of Datum Plane with the body on which EndCut will be applied.
|
static EndCutBuilder.LimitTypes |
VALUE
If this Limit Type is set, the values of Tilt Angle and Shear Angle expressions will be used.
|
Modifier and Type | Method and Description |
---|---|
static EndCutBuilder.LimitTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EndCutBuilder.LimitTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EndCutBuilder.LimitTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final EndCutBuilder.LimitTypes VALUE
public static final EndCutBuilder.LimitTypes PLANE
public static final EndCutBuilder.LimitTypes NEAT_TRIM
public static final int _VALUE
public static final int _PLANE
public static final int _NEAT_TRIM
public static EndCutBuilder.LimitTypes valueOf(int value)
public static EndCutBuilder.LimitTypes valueOf(String name)
public static EndCutBuilder.LimitTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.