public static class BridgeTransitionBuilder.InsetOptions extends Enum
Features.SheetMetal.BridgeTransitionBuilder.InsetOptions#MATERIAL_INSIDE
then the transtion and start edge flow will be on the same logical side
of the plane. If they are on opposite sides then use Features.SheetMetal.BridgeTransitionBuilder.InsetOptions#MATERIAL_OUTSIDE
.Modifier and Type | Field and Description |
---|---|
static int |
_MATERIAL_INSIDE
Bridge Transition body near tangential plane and start will be on same side of the tangential plane selected.
|
static int |
_MATERIAL_OUTSIDE
Bridge Transition body near tangential plane and start will be on opposite sides of the tangential plane selected.
|
static BridgeTransitionBuilder.InsetOptions |
MATERIAL_INSIDE
Bridge Transition body near tangential plane and start will be on same side of the tangential plane selected.
|
static BridgeTransitionBuilder.InsetOptions |
MATERIAL_OUTSIDE
Bridge Transition body near tangential plane and start will be on opposite sides of the tangential plane selected.
|
Modifier and Type | Method and Description |
---|---|
static BridgeTransitionBuilder.InsetOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeTransitionBuilder.InsetOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeTransitionBuilder.InsetOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final BridgeTransitionBuilder.InsetOptions MATERIAL_INSIDE
public static final BridgeTransitionBuilder.InsetOptions MATERIAL_OUTSIDE
public static final int _MATERIAL_INSIDE
public static final int _MATERIAL_OUTSIDE
public static BridgeTransitionBuilder.InsetOptions valueOf(int value)
public static BridgeTransitionBuilder.InsetOptions valueOf(String name)
public static BridgeTransitionBuilder.InsetOptions[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.