public static class BridgeTransitionBuilder.FoldTransitionTypeOptions extends Enum
Features.SheetMetal.BridgeTransitionBuilder.TypeOptions#FOLD
.
Features.SheetMetal.BridgeTransitionBuilder.TypeOptions#FOLD
can be defined by Length or Bend.Modifier and Type | Field and Description |
---|---|
static int |
_BEND
Fold Transition type is Bend.
|
static int |
_LENGTH
Fold Transition type is Length.
|
static BridgeTransitionBuilder.FoldTransitionTypeOptions |
BEND
Fold Transition type is Bend.
|
static BridgeTransitionBuilder.FoldTransitionTypeOptions |
LENGTH
Fold Transition type is Length.
|
Modifier and Type | Method and Description |
---|---|
static BridgeTransitionBuilder.FoldTransitionTypeOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeTransitionBuilder.FoldTransitionTypeOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeTransitionBuilder.FoldTransitionTypeOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final BridgeTransitionBuilder.FoldTransitionTypeOptions LENGTH
public static final BridgeTransitionBuilder.FoldTransitionTypeOptions BEND
public static final int _LENGTH
public static final int _BEND
public static BridgeTransitionBuilder.FoldTransitionTypeOptions valueOf(int value)
public static BridgeTransitionBuilder.FoldTransitionTypeOptions valueOf(String name)
public static BridgeTransitionBuilder.FoldTransitionTypeOptions[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.