Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StepBuilder.StepFaceMethods |
StepBuilder.StepFaceMethods.ALIGNWITH_REFERENCE_FACE
Aligns the step face with the reference face
|
static StepBuilder.StepFaceMethods |
StepBuilder.StepFaceMethods.BLEND
Blends the step face
|
static StepBuilder.StepFaceMethods |
StepBuilder.StepFaceMethods.NORMAL
Orients the step face normal to the stationary face
|
static StepBuilder.StepFaceMethods |
StepBuilder.StepFaceMethods.RULED_RAMP
Replaces the step face with a ruled ramp face
|
static StepBuilder.StepFaceMethods |
StepBuilder.StepFaceMethods.VARIABLE_OFFSET_RAMP
Replaces the step face with a variable offset ramp face
|
Modifier and Type | Method and Description |
---|---|
StepBuilder.StepFaceMethods |
StepBuilder.stepFaceMethod1()
Returns the step face method 1
License requirements: None. |
StepBuilder.StepFaceMethods |
StepBuilder.stepFaceMethod2()
Returns the step face method 2
License requirements: None. |
static StepBuilder.StepFaceMethods |
StepBuilder.StepFaceMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StepBuilder.StepFaceMethods |
StepBuilder.StepFaceMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StepBuilder.StepFaceMethods[] |
StepBuilder.StepFaceMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StepBuilder.setStepFaceMethod1(StepBuilder.StepFaceMethods stepFaceMethod1)
License requirements: nx_aero_design (" NX Aero Design") . |
void |
StepBuilder.setStepFaceMethod2(StepBuilder.StepFaceMethods stepFaceMethod2)
License requirements: nx_aero_design (" NX Aero Design") . |
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.