public static class TubeBuilder.Output extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MULTIPLE_SEGMENTS
multiple segments output
|
static int |
_SINGLE_SEGMENT
single segment output
|
static TubeBuilder.Output |
MULTIPLE_SEGMENTS
multiple segments output
|
static TubeBuilder.Output |
SINGLE_SEGMENT
single segment output
|
Modifier and Type | Method and Description |
---|---|
static TubeBuilder.Output |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TubeBuilder.Output |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TubeBuilder.Output[] |
values()
Returns an array that contains the values for this enum.
|
public static final TubeBuilder.Output MULTIPLE_SEGMENTS
public static final TubeBuilder.Output SINGLE_SEGMENT
public static final int _MULTIPLE_SEGMENTS
public static final int _SINGLE_SEGMENT
public static TubeBuilder.Output valueOf(int value)
public static TubeBuilder.Output valueOf(String name)
public static TubeBuilder.Output[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.