public static class ThroughCurveMeshBuilder.ConstructionMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NORMAL
Use the standard procedures.
|
static int |
_SIMPLE
Build the simplest curve mesh surface possible.
|
static int |
_SPLINE_POINTS
Use the points and tangent values at the points for reparameterizing curves.
|
static ThroughCurveMeshBuilder.ConstructionMethod |
NORMAL
Use the standard procedures.
|
static ThroughCurveMeshBuilder.ConstructionMethod |
SIMPLE
Build the simplest curve mesh surface possible.
|
static ThroughCurveMeshBuilder.ConstructionMethod |
SPLINE_POINTS
Use the points and tangent values at the points for reparameterizing curves.
|
Modifier and Type | Method and Description |
---|---|
static ThroughCurveMeshBuilder.ConstructionMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ThroughCurveMeshBuilder.ConstructionMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ThroughCurveMeshBuilder.ConstructionMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final ThroughCurveMeshBuilder.ConstructionMethod NORMAL
public static final ThroughCurveMeshBuilder.ConstructionMethod SPLINE_POINTS
public static final ThroughCurveMeshBuilder.ConstructionMethod SIMPLE
public static final int _NORMAL
public static final int _SPLINE_POINTS
public static final int _SIMPLE
public static ThroughCurveMeshBuilder.ConstructionMethod valueOf(int value)
public static ThroughCurveMeshBuilder.ConstructionMethod valueOf(String name)
public static ThroughCurveMeshBuilder.ConstructionMethod[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.