public interface TangentBuilder extends FeatureBuilder
Tangent
builder
FeatureCollection.createTangentBuilder(nxopen.features.Tangent)
Property | Value |
---|---|
MoveAlongFace.CoaxialEnabled | 0 |
MoveAlongFace.CoplanarAxesEnabled | 0 |
MoveAlongFace.CoplanarEnabled | 0 |
MoveAlongFace.EqualDiameterEnabled | 0 |
MoveAlongFace.OffsetEnabled | 0 |
MoveAlongFace.ParallelEnabled | 0 |
MoveAlongFace.PerpendicularEnabled | 0 |
MoveAlongFace.SymmetricEnabled | 0 |
MoveAlongFace.TangentEnabled | 0 |
MoveAlongFace.ThicknessChainEnabled | 0 |
MoveAlongFace.UseFaceBrowse | 1 |
Modifier and Type | Method and Description |
---|---|
FaceChangeOverflowBehavior |
faceChangeOverflowBehavior()
Returns the face change overflow behavior.
|
SelectFace |
motionFace()
Returns the motion face
License requirements: None. |
FaceRecognitionBuilder |
moveAlongFace()
Returns the move along faces
License requirements: None. |
void |
setThroughPoint(Point throughPoint)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
SelectISurface |
stationaryFace()
Returns the stationary face
License requirements: None. |
Point |
throughPoint()
Returns the through point
License requirements: None. |
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
SelectFace motionFace() throws NXException, RemoteException
NXException
RemoteException
Point throughPoint() throws NXException, RemoteException
NXException
RemoteException
void setThroughPoint(Point throughPoint) throws NXException, RemoteException
throughPoint
- NXException
RemoteException
SelectISurface stationaryFace() throws NXException, RemoteException
NXException
RemoteException
FaceRecognitionBuilder moveAlongFace() throws NXException, RemoteException
NXException
RemoteException
FaceChangeOverflowBehavior faceChangeOverflowBehavior() throws NXException, RemoteException
FaceChangeOverflowBehavior
for details.
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.