public interface SphereBuilder extends FeatureBuilder
Sphere
builder.
FeatureCollection.createSphereBuilder(nxopen.features.Sphere)
Property | Value |
---|---|
Diameter.Value | 100 (millimeters part), 4 (inches part) |
Modifier and Type | Interface and Description |
---|---|
static class |
SphereBuilder.Types
Represents the sphere types.
|
Modifier and Type | Method and Description |
---|---|
SelectICurve |
arc()
Returns the selected arc associated with the Sphere.
|
BooleanOperation |
booleanOption()
Returns the boolean operation associated with the Sphere.
|
Point |
centerPoint()
Returns the center point of the Sphere.
|
Expression |
diameter()
Returns the diameter of the Sphere.
|
boolean |
parentAssociativity()
Returns the option to keep associativity of the sphere center point
License requirements: None. |
void |
setCenterPoint(Point centerPoint)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
setParentAssociativity(boolean parentAssociativity)
License requirements: features_modeling ("FEATURES MODELING"), solid_modeling ("SOLIDS MODELING") . |
void |
setType(SphereBuilder.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
SphereBuilder.Types |
type()
Returns the sphere type represented by
SphereBuilder.Types
License requirements: None. |
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
Point centerPoint() throws NXException, RemoteException
NXException
RemoteException
void setCenterPoint(Point centerPoint) throws NXException, RemoteException
centerPoint
- NXException
RemoteException
Expression diameter() throws NXException, RemoteException
NXException
RemoteException
SelectICurve arc() throws NXException, RemoteException
NXException
RemoteException
BooleanOperation booleanOption() throws NXException, RemoteException
NXException
RemoteException
SphereBuilder.Types type() throws NXException, RemoteException
SphereBuilder.Types
NXException
RemoteException
void setType(SphereBuilder.Types type) throws NXException, RemoteException
type
- NXException
RemoteException
boolean parentAssociativity() throws NXException, RemoteException
NXException
RemoteException
void setParentAssociativity(boolean parentAssociativity) throws NXException, RemoteException
parentAssociativity
- NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.