public static class SilhouetteFlangeBuilder.OutputSurfaceOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BLEND_FLANGE
Output blend and flange surfaces
|
static int |
_FLANGE_ONLY
Output flange surface
|
static int |
_PIPE_ONLY
Output pipe
|
static SilhouetteFlangeBuilder.OutputSurfaceOptions |
BLEND_FLANGE
Output blend and flange surfaces
|
static SilhouetteFlangeBuilder.OutputSurfaceOptions |
FLANGE_ONLY
Output flange surface
|
static SilhouetteFlangeBuilder.OutputSurfaceOptions |
PIPE_ONLY
Output pipe
|
Modifier and Type | Method and Description |
---|---|
static SilhouetteFlangeBuilder.OutputSurfaceOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SilhouetteFlangeBuilder.OutputSurfaceOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SilhouetteFlangeBuilder.OutputSurfaceOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final SilhouetteFlangeBuilder.OutputSurfaceOptions BLEND_FLANGE
public static final SilhouetteFlangeBuilder.OutputSurfaceOptions PIPE_ONLY
public static final SilhouetteFlangeBuilder.OutputSurfaceOptions FLANGE_ONLY
public static final int _BLEND_FLANGE
public static final int _PIPE_ONLY
public static final int _FLANGE_ONLY
public static SilhouetteFlangeBuilder.OutputSurfaceOptions valueOf(int value)
public static SilhouetteFlangeBuilder.OutputSurfaceOptions valueOf(String name)
public static SilhouetteFlangeBuilder.OutputSurfaceOptions[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.